<a id="displaying-images"></a>

# Displaying Images

<a id="the-setup-view"></a>

## The Setup View

![](assets/images/easy_studio2_common/displaying_images_1.webp)
* Its `Setup View` opens

* One or more images may show.
* If there are multiple images, click on the blue check boxes to show or hide these images.

* Use the zoom and adjustment buttons.

* Click on the ![](assets/images/easy_studio2_common/_icon_save.webp) button.

<a id="the-image-pane"></a>

## The Image Pane(s)

* You can display the result image of any tool in separate image panes:
  * An image pane always displays the result image of the corresponding tool.
  * The result image may be different from the image displayed in the `Setup View`.
  * You cannot configure a result image.
  * You can display the result image from multiple tools at the same time.
  * The images stay displayed independently of the currently selected tool.

  #### HINT
  When you adjust a tool, use these image panes to easily keep an eye on the effect of your changes on the other tools of your graph.

  ![](assets/images/easy_studio2_common/displaying_images_2.webp)

* Will open its result image.
* This additional view pane stays open even when you select another tool.

* One or more images may show.
* If there are multiple images, click on the blue check boxes to show or hide these images.

* Use the zoom and adjustment buttons.

* Click on the ![](assets/images/easy_studio2_common/_icon_save.webp) button.

#### SEE ALSO
By default, image panes are displayed in the right part of the window. To move and organize them on your screen, see [The Main Interface](navigating_the_interface/index.html.md).

<a id="the-zoom-buttons"></a>

## The Zoom Buttons

* In 2D image viewers, you can control the zoom of the image:
  * ![](assets/images/easy_studio2_common/_icon_view_parent.webp) : view parent.
  * ![](assets/images/easy_studio2_common/_icon_zoom_in.webp) : zoom in (up to the 1:1 size).
  * ![](assets/images/easy_studio2_common/_icon_zoom_out.webp) : zoom out.
  * ![](assets/images/easy_studio2_common/_icon_zoom_all.webp) : resize to display the whole graph (up to the 1:1 size).
  * ![](assets/images/easy_studio2_common/_icon_zoom_1-1.webp) : zoom the 1:1 size.

<a id="the-3d-adjustment-buttons"></a>

## The 3D Adjustment Buttons

* In 3D image viewers, you can control the display of the 3D image rendering:
  ![image](assets/images/easy_studio2_common/displaying_images_3.webp)
  * ![](assets/images/easy_studio2_common/_icon_3d_color_scale.webp) : select the color scale reference.
  * ![](assets/images/easy_studio2_common/_icon_3d_view.webp) : point the camera towards an axis (Z by default).
  * ![](assets/images/easy_studio2_common/_icon_3d_lock_view.webp) : point the camera towards an axis (Z by default).
  * ![](assets/images/easy_studio2_common/_icon_3d_axis.webp) : show or hide the axis.
  * ![](assets/images/easy_studio2_common/_icon_3d_edl.webp) : enable or disable the Eye-Dome-Lighting (EDL) shading.
  * ![](assets/images/easy_studio2_common/_icon_3d_wireframe.webp) : enable or disable the display of the wire frame triangles.
  * ![](assets/images/easy_studio2_common/_icon_3d_point_size.webp) : increase or decrease the size of the points.
  * ![](assets/images/easy_studio2_common/_icon_3d_parameters.webp) : open the 3D Viewer settings window to further configure the 3D image rendering.

  ![image](assets/images/easy_studio2_common/displaying_images_4.webp)