# Neo Licensing System FAQ

## How do I use a Neo License?

* After ordering a **Neo License**, you will receive a document (typically a shipping note) containing a unique **Ticket ID**.
* With this **Ticket ID**, use the new **Neo License Manager** to activate your in the container of your choice (a **Neo USB Dongle** (PC6514) or a **Neo Software Container**).
* Once the **Neo License** is activated, you are able to use **eVision**.

## What should I do with my Ticket ID after activation?

* Very carefully store your **Ticket IDs** where you can retrieve them easily. In addition, we recommend that you keep track of which **Ticket ID** is activated on each dongle, system or machine.
* If you ever experience a licensing issue, this **Ticket ID** is required when you contact your distributor or **Allied Vision** support.

## On which device can I activate my Neo License?

* You can activate your **Neo License** either on a **Neo USB Dongle** (PC6514) or on the hard drive of a compatible computer system via **Neo Software Container**.

## Do I have to choose where I want to activate my **Neo License** when I order it?

* No, you just have to order a **Neo License** for the product you want to use.
  * **Neo License** of **eVision** libraries have product codes starting with 43.
  * These licenses are valid for activation on a **Neo USB Dongle** (PC6514) or on a **Neo Software Container**.

## Can I use a Neo License with an older legacy dongle?

* No, **Neo Licenses** can only be activated on a **Neo USB Dongle** (PC6514).
* The old USB Dongle (PC6512) and the PAR Dongle (PC6513) cannot be used with **Neo Licenses**.

## Can I use a Neo License with a dongle from another company?

No, you can only activate a **Neo License** on the **Neo USB Dongle** (PC6514) purchased from **Allied Vision** or from an **Allied Vision** distributor.

## When should I use a Neo Software Container instead of a dongle?

* We recommend that you only use a **Neo Software Container** if your system cannot handle a USB dongle.
* **Neo Software Container** are locked to a computer system and computers are more fragile than USB dongles. USB dongles can easily be moved to a replacement computer in case of a failure of the computer or in case of an upgrade.

## I have activated a Neo License on Neo Software Container a on my computer. Can I move it to a new computer?

* No, once you have activated a **Neo License** on a **Neo Software Container** on a computer, it is locked to that computer and it cannot be moved to another computer or to a **Neo USB Dongle**.

## I have activated a Neo License on a Neo Software Container on my computer. My computer no longer worked and had to be repaired. What can I do?

* If your computer has been repaired by replacing the defective parts, try to reactivate your license(s) from the **Neo License Manager** using the same **Ticket ID** as originally used on this computer. If your computer is still recognized by the **Neo License Manager**, the license(s) will be restored.
* If this process fails, or if your computer cannot be repaired and you wish to use a new computer, please contact your distributor or **Allied Vision** support to request the reactivation of the license(s). You will have to provide the original **Ticket ID** used for that computer. When that reactivation is granted, you can activate the corresponding license(s) again on a new **Neo Software Container**.

## Where can I find the new Neo License Manager?

* The **Neo License Manager** application is available both as a stand-alone installer and within the **eVision** installation package (starting with release 2.13).

## Can I use Neo License Manager the via command line?

* Yes, the **Neo License Manager** is available both as a Graphical User Interface application and as a command line executable.
* The command line executable is less user friendly, but allows to automate the management of **Neo Licenses**.

## Can I use a legacy activation key with the Neo Licensing System ?

* No, legacy activation keys only work with the legacy licensing system.

## Can the new Neo License Manager activate legacy licenses?

* No, the **Neo License Manager** application only manages **Neo Licenses**.
* The previous (legacy) License Manager, however, remains available in the package to manage legacy licenses.

## I have (legacy) non-Neo USB Dongles can I still use them with 2.13 and higher?

* Yes, the legacy dongle licensing system used before **eVision** 2.13 is still active and supported. It will remain active and supported for the foreseeable future.
* However, for new projects, we highly recommend using the **Neo Licensing System**.

## Can I restrict the choice of licensing system (Neo Licensing System or legacy) in my application?

* Yes. A new `Preconfiguration` object is available in **eVision** (as of 2.13) to allow users to restrict the use to a particular licensing system.
* Note that using this feature is optional.

## Are emergency licenses available with the Neo Licensing System ? Are the emergency licenses of the and the legacy licensing system independent?

* Yes, emergency licenses are available with the **Neo Licensing System**, they are independent of the legacy emergency licenses.
* Each of these licensing systems provides three time-limited emergency licenses.

## Are all libraries and bundles available with the new Neo Licensing System ?

* All current libraries and bundles are available with the new **Neo Licensing System**.
* However, some old legacy bundles may not be available with the new **Neo Licensing System**. They remain available with the old licensing systems only.

## What can I do if I have lost a Ticket ID?

* The **Ticket ID** is the unique identifier of a license. It is very important and must be securely stored. If you ever experience a licensing issue, this **Ticket ID** is required when contacting your distributor or **Allied Vision** support.
* **Ticket IDs** that have been activated on a **Neo USB Dongle** can be retrieved by the **Allied Vision** technical support from the dongle serial number.
* However, support for licenses stored in a **Neo Software Container** will not be possible if the **Ticket ID** has been lost.

## Is an Internet connection required to activate a Neo License?

* Yes, an Internet connection is required to activate a **Neo License** on a **Neo USB Dongle** or on a  **Neo Software Container**.
* However, an Internet connection is not required to run **eVision** after the **Neo License** has been activated.

## Do I have to provide the serial number of a Neo USB Dongle when ordering a Neo License?

* No, you do not have to provide the serial number of a **Neo USB Dongle** when ordering a **Neo License**.
* You can activate a **Neo License** either on a **Neo USB Dongle** (PC6514) or on the hard drive of a compatible computer system via a **Neo Software Container**.
* The link between the **Neo USB Dongle** and the **Neo License** is recorded during the activation.

## Is it possible to add licenses for additional eVision libraries to Neo Containers that are already in the field?

* Yes. Just order the additional **Neo Licenses** and activate the new **Ticket ID** on the existing **Neo Container** as usual.
* The activation process is additive. It will add the new licenses to the licenses already activated on the container. The existing licenses will not be lost.
* Please note that this operation requires an Internet connection.

## Can I use a Neo License with older versions of eVision ?

* No, **Neo Licensing System** the is only available as of **eVision** 2.13.
* However, the existing licensing systems remain available with the earlier releases of **eVision**.

## Is the 30-day evaluation license available with the Neo Licensing System ?

* Yes. The Product Code is 4300.
* The time-limited 30-day evaluation license can be activated a single time either on a **Neo USB Dongle** (PC6514) or on a **Neo Software Container**.

## Why is my system start slower after installing the Neo Licensing System ?

* Under **Windows 7**, there is a known issue concerning the **Neo Licensing System** where the associated service can take a long time to start.
* For more information on that issue and steps to solve it, please refer to the FAQ of the service provider: [https://www.wibu.com/support/faq/codemeter-miscellaneous.html](https://www.wibu.com/support/faq/codemeter-miscellaneous.html)

## Why can’t I see my license container in the Neo License Manager ?

* The licensing service might not be started in your system. Check that the `CodeMeter Runtime Service` is running and/or configured to start automatically.
* If you can’t see your dongle, make sure that this dongle was provided by **Allied Vision**. The **Neo Licensing System** is only compatible with **Allied Vision**-provided dongles.

## The Neo License Manager seems to have trouble to contact the Neo Licensing Server when activating. What can I do?

* During activation, the **Neo License Manager** requires an access to the internet through the HTTP and HTTPS protocols. These protocols usually use the ports 80 and 443 or, alternatively, 8080 and 8443. Check that those ports are open and available.

## Why can’t I activate a license on my Neo Software Container?

* First check your internet connection and the open state of the HTTP and HTTPS ports (see previous question).
* If your connection is operational, be sure that your software container is not an emergency container.
* On embedded systems, you might lack a required hardware resource. We cannot guarantee compatibility of **Neo Software Containers** on all embedded systems. If none of the troubleshooting steps in this FAQ helps, you might need to use a dongle instead.

## What should I do if the runtime service is not running?

In rare cases, the **Neo Licensing System** runtime service may not be started automatically.

In such a case:

### On Linux

* To check that the service is not running, run the command:

```bash
> sudo systemctl status codemeter.service
```

* To start the service, run the command:

```bash
> sudo systemctl start codemeter.service
```

### On Windows

* Check that the status of the service `CodeMeterRuntimeServer` is running and that the startup type is automatic.

## I have trouble with licenses and the led on my dongle gives a red light. What can I do ?

* This indicates an issue with the communication between the dongle and the system. Here are common sources of this issue:
  1. The USB port has an issue or is underpowered. Try using another USB port. Don’t use non-powered USB ports.
  2. The CodeMeter service is stopped or badly installed. See above on how to check it.
* If nothing works, your dongle might be defective. Contact Allied Vision for a potential replacement.

## What else can I check if I still have issues with the Neo Licensing System ?

* Check that you use the latest version of the **Neo License Manager** and **Neo Licensing System**. Those tools are regularly updated to improve the compatibility and the user feedback.
* Check that your OS is supported by the **Neo Licensing System**. The compatibility list for a given version is available in the Release Notes of your version.