# Using the Online Command Line

* When you order a **Neo License**, **Allied Vision** sends you a **Ticket ID** required to activate the license on your system.
  * A **Ticket ID** is made of 5 groups of 5 alphanumeric characters separated by a dash. For example: `TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ`
  * You can activate your license either directly on the computer, as a software license, or on a **Neo USB Dongle**, that you can buy from **Allied Vision**.

  ![](assets/images/neo/RN213_Neo_License_Manager_Dongle.webp)
* In the case of the software container, the license is strongly linked to a single computer system, while with a dongle you can move it easily from computer to computer.

## Select a container

1. To select a license container, use the `list-containers` command of the **Neo License Manager**.
   All the containers compatible with **Neo Licenses** are listed:
   ```bash
   > NeoLicenseManagerCL.exe list-containers

   Container list:
     130-3613949292 (software)
   ```

   * A *software container* appears in the list with a serial number starting with `130-`.
   * A *dongle* appears in the list with a serial number starting with `3-`. This serial number is also written on the dongle itself.
2. To create a software container, use the `create-software-container` command of the **Neo License Manager**.
   ```bash
   > NeoLicenseManagerCL.exe create-software-container

   Software container 130-3245488904 has been created.
   ```

   If you already have a software container on your system:
   * We highly recommend you to use that one.
   * Create a new software container only if the old one is broken for any reason. The old license container will become unavailable for activation purposes.
3. Copy the serial number of the container you want to use for the next step.

## Activate the license

1. To activate the license, use the `activate` command of the **Neo License Manager** with the serial number of the container.
   ```bash
   > NeoLicenseManagerCL.exe activate -t TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ -s 130-3245488904

   Activation of ticket TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ has been done successfully.
   ```

   The command associates the **Ticket ID** to the container and activates the license.

## Check the Neo License presence

* To check the presence of the license, use the `list-licenses` command of the **Neo License Manager**.

  The new license appears under the serial number of the license container.
  ```bash
  > NeoLicenseManagerCL.exe list-licenses

  Licenses on container 130-3613949292 (software):
       Open eVision EasyOCR
  ```

## Activating the OEM key feature

By default, the dongles come with the OEM key feature activated. Nevertheless, older dongles may have to be activated.

* To check if this feature is activated use the `check-dongle-OEM-key-readiness` command:
  ```bash
  > NeoLicenseManagerCL.exe check-dongle-OEM-key-readiness –s 3-3613949292
  ```
* If the feature is not activated on the dongle, use the `prepare-dongle-for-OEM-key` command to activate it:
  ```bash
  > NeoLicenseManagerCL.exe prepare-dongle-for-OEM-key –s 3-3613949292
  ```

## Forcing more than one copy of the same license

* By default, the license manager protects you against multiple activations of the same license in a container, refusing the subsequent activations:
* If you want to bypass that protection, use the `--force` argument:
  ```bash
  > NeoLicenseManagerCL.exe activate --force -t TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ -s 130-3245488904
  ```

## Troubleshooting

### Command line help

* To get help about the syntax and the usage of the command line, use the `--help` argument:
  ```bash
  > NeoLicenseManagerCL.exe --help

  Neo License Manager 2
  Usage: C:\Program Files\Euresys\NeoLicenseManager\NeoLicenseManagerCL.exe [OPTIONS] SUBCOMMAND

  Options:
  --console-log               Activates console log
  --file-log TEXT             Activates file log; a path to the desired log file must be specified as argument
  -h,--help

  Subcommands:
  list-containers
  Returns the list of containers
  Options:
      --filter TEXT:{dongle,software}
                                  Type of containers to be checked (dongle/software)
      -e,--expert                 Enables expert mode

  list-licenses
  Returns the list of licenses
  Options:
      -s,--serial-number TEXT     Serial number of a specific container to be checked
      -l,--list-empty-containers  List containers even if they contain no license
      -e,--expert                 Enables expert mode

  apply-license-file
  Applies the given activation file to the software container of your computer
  Options:
      -p,--path TEXT REQUIRED     Path of the license activation file

  create-software-container
  Creates a new software container on the computer. It will only work if none were present
  Options:
      -f,--force                  Additional argument to enforce container creation. For expert users only

  delete-software-container
  Deletes a software container on the computer, given its serial number
  Options:
      -s,--serial-number TEXT REQUIRED
                                  Serial number of the software container to be deleted

  get-container-fingerprint
  Saves the fingerprint file of the given container at the specified location
  Options:
      -s,--serial-number TEXT REQUIRED
                                  Serial number of the software container we want to retrieve the fingerprint from
      -p,--path TEXT REQUIRED     File path for the creation of fingerprint

  check-dongle-OEM-key-readiness
  Checks if the OEM key feature is available in the given container
  Options:
      -s,--serial-number TEXT REQUIRED
                                  Serial number of the dongle on which we want to check OEM key readiness

  prepare-dongle-for-OEM-key
  Prepares a given dongle for OEM key
  Options:
      -s,--serial-number TEXT REQUIRED
                                  Serial number of the dongle we want to prepare for OEM key

  check-neo-status
  Performs a global check-up of the Neo licensing system and print it
  Options:
      -p,--path TEXT              File path for the creation of report

  activity-log
  Prints the content of the log file

  activate
  Activates a Neo ticket ID on the given container
  Options:
      -t,--ticket TEXT REQUIRED   Id of the Neo ticket to be activated
      -s,--serial-number TEXT REQUIRED
                                  Serial number of the container on which ticket will be activated
      -f,--force                  Additional argument to enforce activation. For expert users only

  reactivate
  Reactivates a Neo ticket ID on the given container
  Options:
      -t,--ticket TEXT REQUIRED   Id of the Neo ticket to be reactivated
      -s,--serial-number TEXT REQUIRED
                                  Serial number of the container on which ticket will be reactivated
      -f,--force                  Additional argument to enforce reactivation. For expert users only

  request-activation-file
  Generates an activation file using the given Neo ticket ID and container fingerprint file. This file can then be used to proceed to an offline activation.
  Options:
      -f,--fingerprint-path TEXT REQUIRED
                                  Path to the fingerprint of a container
      -p,--output-path TEXT REQUIRED
                                  Path for the generated activation file
      -t,--ticket TEXT REQUIRED   Neo ticket Id

  request-reactivation-file
  Generates a reactivation file using the given Neo ticket ID and container fingerprint file. This file can then be used to proceed to an offline reactivation.
  Options:
      -f,--fingerprint-path TEXT REQUIRED
                                  Path to the fingerprint of a container
      -p,--output-path TEXT REQUIRED
                                  Path for the generated reactivation file
      -t,--ticket TEXT REQUIRED   Neo ticket Id

  apply-emergency-license
  Activates one of the three emergency licenses packages. It has a 8 days duration.

  version
  Prints the version of Neo License Manager


  End message of Neo License Manager CL
  ```

### Emergency licenses

If you need a license for a limited time (for instance while waiting for some support), use an emergency license.

1. To activate an emergency license , use the `apply-emergency-license` command:
   * These licenses activate all **eVision** products.
   * They are valid for 8 days.
   * You can repeat this a maximum of 3 times.
   * For security reasons, you cannot activate emergency licenses on virtual machines.

   ```bash
   > NeoLicenseManagerCL.exe apply-emergency-license
   ```

### License recovery with a software container

If you have to reinstall the system and lost your licenses:

1. Create a software container.
2. Activate the license with the old **Ticket ID** to try to recover all the licenses associated to the container where you first activated this **Ticket ID**.

   This only works if:
   * It is done in a new, empty container.
   * The system is recognizable (the hardware is more or less the same).
3. If this does not work, perform a reactivation.

### Reactivation

If the recovery does not work or if you lost your licenses and the system has changed significantly (for instance after the failure and replacement of a hardware component), you need to perform a reactivation.

* This transfers your lost license on a container on the new system.
* By default, the reactivation is disabled.

1. Contact the support to obtain a reactivation authorization for the corresponding **Ticket ID**.
2. Once the reactivation is authorized, follow the license activation procedure described above but use the `reactivate` command instead of `activate`.

### Error reporting

If anything fails, the **Neo License Manager** returns an error and information about it in `stderr`.

1. To recover the `stderr` log from the command line, you can use `-–file-log` argument, followed by the path to a log file, as follows:
   ```bash
   NeoLicenseManagerCL.exe --file-log c:\tmp\error.log activate -t TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ -s 130-3245488904
   ```
2. If you need more information, use the **Memento** tool from **Euresys**.
3. To check the status of the licensing system on your computer at any time, use the `check-neo-status` command of the **Neo License Manager**.
   ```bash
   > NeoLicenseManagerCL.exe check-neo-status

   ** Starting List Product Item for box 130-3613949292 and firm code 6001261 **
   Found Productcode (Dependency: 0x7): 4305
       Text (#=20, Dependency 0x00):  "Open eVision EasyOCR"
       Extended Protected Data (#=16, Type 136, Dependency 0x07): 6c 63 64 63 00 01
   9b 05 00 00 00 00 00 00 01 00
   ** List Product Item finished without errors **
   ```
4. To check the log of the licensing system on your computer at any time, use the `activity-log` command of the **Neo License Manager**.
   ```bash
   > NeoLicenseManagerCL.exe activity-log
   ** L.M version 23.08.0 09/07/23 14:25:02 : Emergency activation was requested.
   L.M version 23.08.0 09/07/23 14:25:03 : Emergency activation was successful. There is (are) 2 emergency license(s) remaining. **
   ```