# Image Stitching with Learning

This code snippet shows how to stitch multiple images.

## C++

```cpp
#include <eVision/EasyImage/EImageStitcher.h>
```

```cpp
using namespace eVision;
// Create the stitcher class
EImageStitcher stitcher;

std::vector<EImageBW8> learningImages;
std::vector<EImageBW8> subjectImages;
EImageBW8 output;

stitcher.LearnBW8(learningImages);
// Learn has been done, stitching will be faster as the transformation to apply
// to the different patches are already computed
stitcher.Stitch(subjectImages, output);
```

## C#

```cs
using eVision;
using System.Collections.Generic;
```

```cs
// Create the stitcher class
EImageStitcher stitcher = new EImageStitcher();

List<EImageBW8> learningImages = new List<EImageBW8>();
List<EImageBW8> subjectImages = new List<EImageBW8>();
EImageBW8 output = new EImageBW8();

stitcher.LearnBW8(learningImages.ToArray());
// Learn has been done, stitching will be faster as the transformation to apply
// to the different patches are already computed
stitcher.Stitch(subjectImages.ToArray(), output);
```

## Python

```py
import eVision
# Create the stitcher class
stitcher = eVision.EImageStitcher()

# EImageC24 can be used instead of EImageBW8
# Patchs is a vector of image where each image is calibrated
learningImages = [eVision.EImageBW8(), eVision.EImageBW8(), eVision.EImageBW8()]
subjectImages = []
output = eVision.EImageBW8()

stitcher.LearnBW8(learningImages)
# Learn has been done, stitching will be faster as the transformation to apply
# to the different patches are already computed
stitcher.Stitch(subjectImages, output)
```