<a id="easydeeplearning-dlstudio"></a>

# Deep Learning Studio

**Deep Learning Studio** is a graphical user interface that you can use to create datasets and train your deep learning tools.

**Deep Learning Studio** is organized around the concept of projects.

A project consists in:

* A tool type.
* A dataset (images and their annotations).
* Several dataset splits.
* The data augmentation settings.
* The tools that you can train on the dataset.
* The results and metrics for each tool to analyze their performance.

The project is stored as a folder containing:

* The project file with the `.edlproject` extension.
* The `Images` folder with the imported images.
* A dedicated folder for each tool.

By default, the projects are stored in the folder named `Deep Learning Studio Projects` located in your `Documents` folder. After loading a project, the project file is automatically locked when it is used. This means that when a program opens a **Deep Learning** project file, this project file is inaccessible by other programs as long as the initial program doesn’t explicitly close the project.

Here are the various file extensions used within a project:

* `.edlproject`: the project file containing the dataset, the splits, the list of tools and the data augmentation settings.
* `.edlsettings`: the settings for a tool.
* `.edlmodel`: a deep learning model for the tool.
  * The training model is the model obtained after the last training iteration.
  * The inference model is the model that is applied to images. It is the model that gave the best performances during the training.
* `.edltool`: a complete usable tool (obtained by exporting the tool from **Deep Learning Studio**).
* `.edlmetrics`: the metrics for the tools.
* `.edlresult`: a result for a given image and tool.
* `.edldataset`: a dataset (obtained by exporting the dataset from the project).
* In older versions of **eVision**, the settings, model and tool had the extension `.ecl`, the metrics `.edl`, and the dataset `.eds`.

#### NOTE
**Deep Learning Studio** never sends or shares resources over the internet. All images, annotations, models and results always remain on your local computer.

<a id="easydeeplearning-dlstudio-workflow"></a>

## Deep Learning Studio Workflow Illustration

This illustrates the typical [workflow](easydeeplearning/index.html.md#easydeeplearning-workflow) to create a Deep Learning tool for your application.

1. Load or create a project.
   * Quickly go back to your work with the recent project lists.
     * Open existing projects or create new projects.

     ![image](assets/images/easydeeplearning/easydeeplearning_studio_step1a.webp)
   * Create a new project.
     * Specify the name and the type of the project.
     * If necessary, change the path to save the project.
     * See [Choose Your Tool](easydeeplearning/choose_your_tool.html.md#easydeeplearning-choose-your-tool).

     ![image](assets/images/easydeeplearning/easydeeplearning_studio_step1b.webp)
2. Import images in the project dataset and annotate the images. See [Managing the Dataset and the Annotations](easydeeplearning/managing_the_dataset_and_the_annotations.html.md#easydeeplearning-dataset).
   ![image](assets/images/easydeeplearning/easydeeplearning_studio_step2.webp)
3. Split your dataset into training, validation, and test images. See [Managing the Dataset Splits](easydeeplearning/managing_the_dataset_splits.html.md#easydeeplearning-splits).
   ![image](assets/images/easydeeplearning/easydeeplearning_studio_step3.webp)
4. Configure and view the data augmentation settings. See [Using Data Augmentation](easydeeplearning/using_data_augmentation.html.md#easydeeplearning-data-augmentation).
   ![image](assets/images/easydeeplearning/easydeeplearning_studio_step4.webp)
5. Create, configure, and train your tools. See [Training a Deep Learning Tool](easydeeplearning/training_a_deep_learning_tool.html.md#easydeeplearning-training).
   ![image](assets/images/easydeeplearning/easydeeplearning_studio_step5.webp)
6. Analyze the performance and the results of the trained tools. Make predictions on new images. See [Using a Deep Learning Tool](easydeeplearning/using_a_deep_learning_tool.html.md#easydeeplearning-using).
   ![image](assets/images/easydeeplearning/easydeeplearning_studio_step6.webp)
7. Benchmark your tools to optimize the execution settings and maximize the inference speed on your hardware. See [Benchmarking a Deep Learning Tool](easydeeplearning/benchmarking_a_deep_learning_tool.html.md#easydeeplearning-benchmark).
   ![](assets/images/easydeeplearning/benchmarking.webp)

<a id="easydeeplearning-dlstudio-additional-resources"></a>

## Additional Resources

* The **Deep Learning Additional Resources** package, separate from the **eVision** installer, provide several sample datasets as well as **Deep Learning Studio** projects containing a trained tool for these datasets:
  * For **EasyClassify**: the `MiniWaffle`, `Stone Tiles` and `CopperSilverTape` datasets.
  * For **EasySegment Unsupervised**: the `Fabric` dataset.
  * For **EasySegment Supervised**: the `Coffee` dataset.
  * For **EasyLocate Axis Aligned Bounding Box**: the `ElectronicComponentsBag` dataset.
  * For **EasyLocate Interest Point**: the `CeramicCapacitor` dataset.