<a id="easydeeplearning-easylocate"></a>

# EasyLocate - Locating Objects and Defects

To create an **EasyLocate** tool:

* API:
  * **EasyLocate - Axis aligned bounding box**: [`ELocator`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocator.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocator.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocator.html)
  * **EasyLocate - Interest Point**: [`EInterestPointLocator`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html)
* To create an **EasyLocate** project in **Deep Learning Studio**:
  1. Start **Deep Learning Studio**.
  2. Create a new project and select `EasyLocate Axis Aligned Bounding Box` or `EasyLocate Interest Point` in the `New deep learning project` dialog.
     ![](assets/images/easydeeplearning/easylocate_1.webp)

<a id="easydeeplearning-easylocate-properties"></a>

## Properties

<a id="easydeeplearning-easylocate-properties-common"></a>

### Common Properties

![image](assets/images/easydeeplearning/easylocate_2.webp)

The `EasyLocate` tool has 3 main parameters:

1. The `Capacity` of the neural network (default: `Normal`) represents the quantity of information it is capable of learning. A larger capacity makes the tool slower.

   In the API:
   * The capacity is represented by the enumerate type [`ELocatorCapacity`](../../../doxygen_cpp/namespaceeVision_1_1EasyDeepLearning.html#a347cb8b689c40f5ffd1cb400800acf8b) [<sub>.NET</sub>](../../../doxygen_cs/namespaceeVision_1_1EasyDeepLearning.html#a295054325fe5dbca3595afdf471658ce) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorCapacity.html).
   * [`ELocatorBase::SetCapacity`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a0f5f3a021bb7a5f19aec91f867a20b36) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a456786be90610de03489ba3c22e76c6c) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#abef2463cd49d9074fca74c518cefe2db) sets the capacity of the tool.
2. The `Image type` (default: `Monochrome (1 channel)` if the dataset contains only grayscale images, otherwise `color (3 channels)`):

   In the API:
   * To use monochrome (grayscale, 1 channel) images, set [`ELocatorBase::SetChannels`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#af894bc01f3d27c122c9e8717ac632fe6) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a779181e4557f2043a7b22da5f931f575) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a2900b5431941aa25504b5b0c8f97dbfb) to `1`.
   * To use color (3 channels) images, set [`ELocatorBase::SetChannels`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#af894bc01f3d27c122c9e8717ac632fe6) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a779181e4557f2043a7b22da5f931f575) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a2900b5431941aa25504b5b0c8f97dbfb) to `3`.
3. The size of the images (`Width` and `Height`). You must configure **EasyLocate** for a specific image size.
   * The image must contain less than 500 000 pixels (about 707 × 707 pixels for a square image).
   * The width and the height must be at least 128 pixels.
   * The images are automatically resized to the specified size before **EasyLocate** processes them.
   * The lower the image size, the faster **EasyLocate** is.
   * **EasyLocate** works best with objects equal to or bigger than 16 × 16 pixels.

   In **Deep Learning Studio**:
   * Use the `Width` and `Height` controls to change the size of the images.
   * Uncheck `Keep aspect ratio` if you want to control the width and height independently of each other.
   * By default, the width and height are set to the size of the images in the dataset. or, when they are bigger than 500 000 pixels, to the maximum possible size so that the aspect ratio of the image is kept and it contains at most 500 000 pixels.
   * A warning is displayed when the selected size makes the ground truth objects smaller than 16 × 16 pixels.
     ![image](assets/images/easydeeplearning/easylocate_3.webp)

   In the API:
   * Use [`ELocatorBase::SetWidth`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a3b66020b7ac570fcebd691d20652efee) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a0b0ca0b107c559aa6df1f8c6fbe6a022) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a89ae62d10106f1cd1fb39536f7a1ec6e) and [`ELocatorBase::SetHeight`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a27192744809322fc97def3e84120aa5a) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a2d00bccf1433c30838eefe4795af8ad4) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#af8e96e40b841096d0fa21b7cab9e86ee) to specify the image size.

<a id="easydeeplearning-easylocate-properties-advanced"></a>

### Advanced Parameters

<a id="easydeeplearning-easylocate-properties-advanced-bbox"></a>

#### Axis Aligned Bounding Box

![image](assets/images/easydeeplearning/easylocate_2a.webp)

The **EasyLocate Axis Aligned Bounding Box** tool has 4 advanced parameters linked to **EasyLocate** neural network design.

* The **EasyLocate** neural network works as an image pyramid where the size of the input image is halved at each level. **EasyLocate** attempts to detect objects using one or more pyramid levels depending on the size of the objects to detect.
* To do so, **EasyLocate** uses a set of typical object size, called  ***anchors***, that are assigned to pyramid levels according to their surface. Then, for each pixel and anchor of a pyramid level, **EasyLocate** predicts whether there is an object or not located around that pixel and whose size approximately matches the anchor.
* **EasyLocate** then performs a post-processing on the prediction of the neural network. Indeed, the neural network can predict the same object several times using different levels of the pyramid, different anchors or neighboring positions in the image. **EasyLocate** keeps only the prediction with the highest probability and removes duplicates based on the overlap between objects.

The advanced parameters are:

1. The `Anchors`. By default, the anchors are determined automatically from the objects in your dataset. The set of anchors must reflect the variety of object sizes that must be detected.

   To check or manually edit the anchors, click on `See/edit anchors` to open the following dialog:
   ![image](assets/images/easydeeplearning/easylocate_4.webp)

   The dialog lists the current anchors and enables the following operations:
   * To edit an existing anchor, double-click on its width or on its height in the list.
   * To add or remove an anchor, click on the corresponding button.
   * To generate a new set of anchors, specify the number of subscales, the minimum and the maximum dimensions of the anchors and one or more aspect ratios.
   * The dimension of an anchor is the square root of its surface and determines the pyramid level assigned to the anchor. The number of subscales represent the number of dimensions to generate for each pyramid level. For each of those dimensions, the anchors with the specified aspect ratios are generated.

   #### NOTE
   The anchors must be defined with respect to the width and height of the current tool. Thus, when specifying the anchors manually, the width and height parameters are locked.

   In the API:
   * Use [`SetPredictionAnchors`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#af55356312f6106bf95a036a43ff6f693) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a0f703a3aa859fe9e7d13aa2ad854f9ea) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a732ca38599205adad64df48940a1c3f0) and [`GenerateAnchors`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocator.html#a8d09fd693156cb027e4b8d1918e2fe51) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocator.html#a567d177f86b01778804bc19ce6dbe120) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocator.html#ac48aff8fe49ad70a4474f8ee57df4aed).
2. The `Maximum number of objects in an image`. By default the value is 100. A lower value can speed up the post-processing of the results.

   In the API:
   * Use [`SetMaxNumberOfObjects`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a7c7054f47056b8c0a44fdacf5b0c8f46) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#ab62de16d144046528b593344b5db6213) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a8fbc5ab313399b930a45068e1b28d3d8).
3. The `Same label maximum overlap` is the maximum overlap between objects with the same label. By default the value is 0.5.

   In the API:
   * Use [`SetSameLabelMaxOverlap`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocator.html#a48c9cd0b0efcdad7a59a61f09eb1d32a) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocator.html#ae3cbb9dc42e31161504c75460db25f8a) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocator.html#a8f70550fa2feac25538c880109a56914).
4. The `Absolute maximum overlap` is the maximum overlap between objects, regardless of their label. By default the value is 1 and it means that the tool can predict two objects with different labels but with the exact same bounding box.

   In the API:
   * Use [`SetSameLabelMaxOverlap`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocator.html#a48c9cd0b0efcdad7a59a61f09eb1d32a) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocator.html#ae3cbb9dc42e31161504c75460db25f8a) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocator.html#a8f70550fa2feac25538c880109a56914).

The overlap between two objects is their intersection over union (IoU), defined as the ratio between the surface of the intersection of their bounding boxes and the surface of the union of their bounding boxes.

<a id="easydeeplearning-easylocate-properties-advanced-ip"></a>

#### Interest Point

![image](assets/images/easydeeplearning/easylocate_5.webp)

The **EasyLocate Interest Point** tool has 4 advanced parameters.

1. The `Object size` is the size of the objects that you want to detect in the image.
   * By default, the value of this parameter is the object size specified for the dataset.
   * The object size has the same role as the anchors for **Easy Locate Axis Aligned Bounding Box**.
   * The object size is defined with respect to the size of the images in the dataset. When training a tool with a different input resolution, the object size parameters should not change (they are internally adapted according to the resolution of the training images and the width and height set for the tool).

   In the API:
   * Use [`SetObjectSize`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a99ef65d3d549fdcb4bb09f9d861570fb) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a695de95790a322c6e7811d5a6b5fcc13) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a91e6404fde4ef043b9f64d2ffb655a48)
2. The `Maximum number of objects` in an image.
   * By default the value is 100.
   * A lower value can speed up the post-processing of the results.

   In the API:
   * Use [`SetMaxNumberOfObjects`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a7c7054f47056b8c0a44fdacf5b0c8f46) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#ab62de16d144046528b593344b5db6213) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a8fbc5ab313399b930a45068e1b28d3d8).
3. The `Same label minimum distance` is the minimum distance between objects with the same label.
   * By default the value is a third of the object size.

   In the API:
   * Use [`SetSameLabelMinDistance`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#afedbae6ba82bc49466a07dc2e3dc3c96) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a6b9ab6f77359632cf5e0e6680d5b7133) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a3ad1a2e5f9075ff8b70c8f6ab8da72db)
4. The `Absolute minimum distance` is the minimum distance between objects, regardless of their label.
   * By default the value is 0 and it means that the tool can predict two objects with different labels but with the exact same position.

   In the API:
   * Use [`SetAbsoluteMinDistance`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a396065e011b2fc4d7d9d61f5b83d4ecd) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#a3b6d7d79fdd4da54f8da2d6587214743) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EInterestPointLocator.html#aa9b18f6080217b570f7a26eeca0ad73f)

<a id="easydeeplearning-easylocate-training"></a>

## Training

To train your tool, see [Training a Deep Learning Tool](../easydeeplearning/training_a_deep_learning_tool.html.md).

<a id="easydeeplearning-easylocate-validation"></a>

## Validating the Results

* The **EasyLocate** tool exposes 2 types of metrics. These object-based metrics quantify the performance of the tool :
  * At the object level.
  * At the image level. These metrics are related to the tool ability to correctly detect images without object and images with objects.
* In **Deep Learning Studio**
  * The metrics are available in the `Validation and results` tab.
  * Most metrics depends on the value of the `Detection threshold`.

  ![image](assets/images/easydeeplearning/easylocate_validating_1.webp)
* In the API:
  * The metrics are represented by an [`ELocatorMetrics`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorMetrics.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorMetrics.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorMetrics.html) object.

<a id="easydeeplearning-easylocate-validation-object"></a>

### The Object-Based Metrics

The object-based metrics are computed by matching actual, ground truth objects to detected objects.

A ground truth object and a detected object are matched together if:

* They have the same label.
* With **EasyLocate Axis Aligned Bounding Box**:
  * Their overlap (“Intersection over Union”) is higher or equal to the `Same label maximum overlap` parameter of the tool.
  * There is no other ground truth that has a higher overlap with the detected object and there is no other detected object that has a higher overlap with the ground truth object.
* With **EasyLocate Interest Point**:
  * Their distance is lower than the `Same label minimum overlap` parameter of the tool
  * There is no other ground truth that has a smaller distance with the detected object and there is no other detected object that has a smaller distance with the ground truth object.

The object-based metrics are:

* The `Average precision` (AP) is the average of the precision (proportion of detected objects that are matched to a ground truth objects) for different values of recall (true positive rate, proportion of ground truth objects that are matched to detected objects) obtained by varying the `Detection threshold`.
  * Its value is between 0 (bad detector) and 1 (good detector).
  * It is a standard metric for evaluating object detector.
* The `recall`, also called the “true positive rate”, is the proportion of ground truth objects matched with a predicted object.
* The `weighted recall` is the weighted average of the `recall` for each label.
* The `precision`, also called the “positive predicted value”, is the proportion of predicted objects matched with a ground truth object.
* The `weighted precision` is the weighted average of the `precision` for each label.
* The `F-Score` is the harmonic mean of the recall and the `precision`.
* The `weighted F-Score` is the weighted average of the `F-Score` for each label.
* The `Per label metrics` table shows various metrics of the objects of each label. The columns starting with a “#” indicate the number of objects in the corresponding category.
  * Selecting one or more cells from these columns filters the image list to show only the images that have objects falling in the corresponding categories.
  * If there is no selection, all the images are listed.
  * Use `CTRL`+`LeftClick` to add cells to the current selection.

<a id="easydeeplearning-easylocate-validation-image"></a>

### The Image-Based Metrics

![image](assets/images/easydeeplearning/easylocate_validating_2.webp)

The metrics related to the correct detection of the class of the images (background / with object or good / defective in the context of defect detection) are:

* The `image detection accuracy` is the proportion of images correctly predicted to have objects or not.
* A `Confusion matrix` listing the number of images in each category.
  * Selecting one or more cells of the confusion matrix filters the image list to show only the images in the corresponding categories.

<a id="easylocate-inference"></a>

## Applying the Tool to New Images

#### SEE ALSO
Some **eVision Studio** samples illustrate inference with **EasyLocate**:

* `EasyLocate (bounding boxes)`: inference on the `ElectronicComponentsBag` dataset.
* `EasLocate (interest points)`: inference on the `CeramicCapa` dataset.

See [Additional Resources](../deep_learning_studio.html.md#easydeeplearning-dlstudio-additional-resources) for details about the datasets and how to get them.

<a id="easylocate-inference-dlstudio"></a>

### Deep Learning Studio

* To apply **EasyLocate** to new images:
  * Include the new images in the test set
    1. Add new images to the dataset from the `Dataset and annotations` tab.
    2. In the `Validation and results` tab, refresh the results

    ![image](assets/images/easydeeplearning/easysegment_8.webp)
  * Open the `Inference tests` tab to apply the segmenter to new images and display detailed results for these images.
* To visualize the predicted objects of an image:
  1. Open the `Results` menu (`ALT`+`R`) of the image viewer.
  2. Check the `Predicted` objects option (`CTRL`+`P`).

  ![](assets/images/easydeeplearning/easylocate_locating_1.webp)
* If the image has a ground truth, check the `Missing ground truth object` option (`CTRL`+`G`) to display missing objects. They appear with a yellow pattern drawn over it.
* In the `Results` tab on the right side:
  * The list of detected objects shows their label, their score, whether they are matched to a ground truth object and their predicted bounding box or position.
  * To see how close a predicted object is to a ground truth object, select the object in the list on the right side of the image.

    For **EasyLocate Axis Aligned Bounding Box**, the ground truth object is displayed on top of the predicted object with the following color code:
    ![image](assets/images/easydeeplearning/easylocate_locating_2.webp)
* To accept all the predicted objects as ground truth:
  * Click on the `Use prediction as ground truth` button (`CTRL`+`U`).
  * Note that it removes any previous ground truth object already present in the image.
* To accept a single predicted object as ground truth:
  1. Right click on the object.
  2. Select `Accept into ground truth` in the menu.

  ![](assets/images/easydeeplearning/easylocate_locating_3.webp)

<a id="easylocate-inference-api"></a>

### API

* To apply **EasyLocate** to an image, use [`ELocatorBase::Apply`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a5637cb94b57423da5dbf56dd19101768) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#aebd89f38cfcfdacc02df07e20a6646a4) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorBase.html#a197f14726ea6f7de45e6d5a300f8bf1f).

  This method returns an object [`ELocatorResult`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html).
* Use [`GetDetectedObjects`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a5bec702bb6d5adbc662844d0db916668) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a88264f974ed4df96bec0de2c3919b94a) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#ab5b9a82d09e9f4d4f2aa228e418331d9) to retrieve the predicted objects as an array of [`ELocatorPredictedObject`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html).
* Use [`Draw`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a34ff1a57ed7417fe8dbecb73b868b3ad) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a1a37b44948e7f53cce2caeef8743be66) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a13e9b72def330eb976a13fb0e96f087d) to draw all the predicted objects.
* With **EasyLocate Axis Aligned Bounding Box**, for each predicted object, use:
  * [`GetPositionX`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#ab62f19eb86ca7a24b82a7fc52a817e53) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a1bab4b5dbe81f9cd0955fec5a3909658) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a8da8bcaede0b0173e35cca09d4a0e393) to get the X coordinate of the center of the bounding box.
  * [`GetPositionY`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a35aa55a82eb927f4e17d83e18de23da8) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a1d4a85115fc0ef85ab57051b89bcfd7a) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a2bbc0132323ae8cdea075d1eb1bf7a88) to get the Y coordinate of the center of the bounding box.
  * [`GetOrgX`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a2892e257cefe8f091104bbdf4499864c) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#aae10fefbc24161ee0aea62df4b330834) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#aa918b2b1119c27752c13f8d56d2931e3) to get the X coordinate of the top left origin of the bounding box.
  * [`GetOrgY`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#aa846e405dae00406c442c4d8dc3d5d55) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#ad4a7aa51938e292fae8ff564ac2aa487) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a28a03819e00872af700de07a9b872e33) to get the Y coordinate of the top left origin of the bounding box.
  * [`GetWidth`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#ab1cbfa5e8c4f7341abf55003a20b9df6) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#aab7b0011b00fc9efffb248e1f8412e55) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#ac3a1dc7956306da4cd08af9d239bf59a) to get its width.
  * [`GetHeight`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a387a7817f70635216938e694b96da0e3) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a7afb29e0cdd8e93ab2b3d5b742943f51) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#abcf2cc53fe5ec996f0bf505f0a635236) to get its height.
  * [`GetLabel`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#aab5eae91d1d8bdfbb14f1e82d1cf9661) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a8b47e221e2a81760b58719d109ebe9b7) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a92d5fca51870043add9218dae6e45a43) to get its label.
  * [`GetProbability`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html#a927bc42e002346c7a9738c58aa895989) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html#a90d96403a51583bb2b0b314e950c5ff2) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html#abd4c6a40d29e27fd65778464bd41598a) to get its predicted probability.
* With **EasyLocate Interest Point**, for each predicted object, use:
  * [`GetPositionX`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#ab62f19eb86ca7a24b82a7fc52a817e53) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a1bab4b5dbe81f9cd0955fec5a3909658) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a8da8bcaede0b0173e35cca09d4a0e393) to get the X coordinate of the object.
  * [`GetPositionY`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a35aa55a82eb927f4e17d83e18de23da8) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a1d4a85115fc0ef85ab57051b89bcfd7a) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a2bbc0132323ae8cdea075d1eb1bf7a88) to get the Y coordinate of the object.
  * [`GetLabel`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#aab5eae91d1d8bdfbb14f1e82d1cf9661) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a8b47e221e2a81760b58719d109ebe9b7) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorObject.html#a92d5fca51870043add9218dae6e45a43) to get its label.
  * [`GetProbability`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html#a927bc42e002346c7a9738c58aa895989) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html#a90d96403a51583bb2b0b314e950c5ff2) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorPredictedObject.html#abd4c6a40d29e27fd65778464bd41598a) to get its predicted probability.

#### NOTE
Use [`GetLocatorFeatures`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#abfac51f6e785005e6ecd80990b56a02f) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a2dcb44925b5394c2f71bfde8c0abc666) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a288aea39397438ccd06de419636fb2d1) to check if the result was computed by **EasyLocate Axis Aligned Bounding Box** or **EasyLocate Interest Point**.

The value of [`GetLocatorFeatures`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#abfac51f6e785005e6ecd80990b56a02f) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a2dcb44925b5394c2f71bfde8c0abc666) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorResult.html#a288aea39397438ccd06de419636fb2d1) is a combination (using the binary OR (|) operator) of one or more [`ELocatorFeature`](../../../doxygen_cpp/namespaceeVision_1_1EasyDeepLearning.html#a6b2c2ea7a028842503847f7850e4bd1a) [<sub>.NET</sub>](../../../doxygen_cs/namespaceeVision_1_1EasyDeepLearning.html#aee0d2bd65f88bc4cb92c07c8e4996659) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1ELocatorFeature.html) values. It indicates the type of information predicted by the tool:

* For **EasyLocate Interest Point**: `ELocatorFeature_Position`.
* For **EasyLocate Axis Aligned Bounding Box**: `ELocatorFeature_Position | ELocatorFeature_Size`.