# Calibration and Transformation

## Field-of-view Calibration

| Calibration establishes the relationship between real-world point coordinates and image pixels. A simple calibration model computes faster, a repeatable part position is easier to locate.                                                                          | ![](assets/images/easygauge/fieldofviewcalibration.webp)          |
|----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------|-------------------------------------------------------------------|
| **The Raw sensor** coordinate system starts from upper left and extends rightwards and downwards.<br /><br/>\\\\<br/>The range of abscissas is 0 to width-1 and the range of ordinates is 0 to height-1 where integer coordinate values correspond to pixel centers. | ![](assets/images/easygauge/rawsensorcoordinatessystem.webp)      |
| **The Centered sensor** coordinate system starts at the center ([width-1]/2, [height-1]/2 in the Raw system) and extends rightwards and upwards.                                                                                                                     | ![](assets/images/easygauge/centeredsensorcoordinatessystem.webp) |
| The real world 3D coordinates are defined in a 2D reference frame tied to a reference plane. The origin and direction of the axis are normally aligned with major features of the inspected parts.                                                                   | ![](assets/images/easygauge/18150.webp)                           |

## Before World-to-Sensor Transform

Before converting from world to sensor coordinates, sources of distortion should be eliminated:

* adjust sweep frequency or scanning speed to avoid non-square pixels.
* adjust optical alignment to minimize perspective effect. The field of view should be parallel to the sensor plane.
* use long focal distances and good quality lenses to minimize Optical distortion.
* use appropriate scale factor based on lens magnification, observation distance and focusing.
* minimize skew and translation effects by secure fixtures, and part-movement / acquisition-triggering synchronization.

## Effects of World-to-Sensor Transform

| **No calibration**. World and sensor coordinates are identical.                                                                                                                                                       | ![](assets/images/easygauge/worldtosensortransformuncalibrated.webp)          |
|-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------|-------------------------------------------------------------------------------|
| **Translated calibration**: The coordinate origin can be moved. World coordinates correspond to pixel units.                                                                                                          | ![](assets/images/easygauge/worldtosensortransformtranslated.webp)            |
| **Isotropic scaling** (square pixels).   A scale factor converts pixel values  to physical measurements.                                                                                                              | ![](assets/images/easygauge/worldtosensortransformscaledsquare.webp)          |
| **Anisotropic scaling** (non-square pixels). Uses two scale factors with pixel aspect ratio (X /Y ) in the range [-4/3, -3/4] (or [3/4, 4/3]). Pixels are always displayed as square, so the image appears stretched. | ![](assets/images/easygauge/worldtosensortransformscalednonsquare.webp)       |
| **Scaled and skewed** (square pixels). Real-world axis aligns with rotated inspected part using translation, rotation and scaling.                                                                                    | ![](assets/images/easygauge/worldtosensortransformscaledskewedsquare.webp)    |
| **Scaled and skewed** (non-square pixels). Distortion is apparent. Occurs when camera scan speed does not match pixel spacing.                                                                                        | ![](assets/images/easygauge/worldtosensortransformscaledskewednonsquare.webp) |
| **Perspective distortion** causes further away objects to look smaller; lines remain straight but angles are not preserved.                                                                                           | ![](assets/images/easygauge/worldtosensortransformperspective.webp)           |
| **Optical distortion** causes cushion or barrel appearance of rectangles.                                                                                                                                             | ![](assets/images/easygauge/worldtosensortransformoptical.webp)               |
| **Combined distortions** result in a complex, non linear, transform from real-world to sensor spaces.                                                                                                                 | ![](assets/images/easygauge/worldtosensortransformcombined.webp)              |