<a id="easydeepocr-maintitle"></a>

# EasyDeepOCR - Reading Texts with Deep Learning

<a id="edo-purpose"></a>

## Purpose

**EasyDeepOCR** is a new generation OCR library that relies on deep learning technologies to tackle modern text reading challenges.

**EasyDeepOCR** features:

* Zero-configuration text location and recognition
* Text filtering through [topologies](detailed_usage.html.md#edo-specifying-topology)
* Improved speed on x86_64 CPUs with **OpenVINO** and **NVIDIA** GPUs with **TensorRT**
* Optional further speed optimization using only a few labeled samples
* A simple and comprehensive C++, C# and Python API
* A fully featured **eVision Studio** tool and samples showcasing the entire workflow of **EasyDeepOCR**.

**EasyDeepOCR** is a major improvement over the **EasyOCR** and **EasyOCR2** libraries, combining ease of use and enhanced capabilities.

<a id="edo-scope"></a>

### Scope

**EasyDeepOCR** is able to locate and read all texts in a given image, provided they adhere to the following specifications:

* Printable ASCII characters: `!"#$%&\'()*+,-./0123456789:;<=>?@ABCDEFGHIJKLMNOPQRSTUVWXYZ[\]^_`abcdefghijklmnopqrstuvwxyz{|}~`
* Industrial fonts
* Minimum line height: 12 pixels
* Line aspect ratio between 1:1 and 40:1
* Maximum characters per line: 50
* Gray scale (8-bit) or color (24-bit) images
* Near planar images (limited perspective)

<a id="edo-structuredtexts"></a>

### Structured Texts

When you specify a topology, the lines are gathered into texts that satisfy the following requirements:

* The texts match the topology.
* The texts are structured.

#### HINT
See [Specifying the Execution Settings](setting_the_parameters.html.md#edo-specifying-execution-settings).

**EasyDeepOCR** only returns ‘structured texts’ (a concept specific to this tool: see [`eVision::EasyDeepOCR::ETextLine`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextLine.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextLine.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextLine.html)) where the geometric arrangement of lines and words meets a particular definition:

1. All the lines of a ‘structured text’:
   * Must be parallel.
   * Must have the same height.
   * Must be horizontally aligned:<br />
     \\\\
     Two lines l₀ and l₁ are horizontally aligned if:

   $$
   l₀^{begin} \le l₁^{begin}

   and

   l₁^{end} \le l₀^{end}
   $$
2. All the pairs of consecutive lines:
   * Must not overlap vertically.
   * Must not be separated by a vertical distance greater than the line height.
3. All the words of a line:

* Must not be separated by a horizontal distance greater than the line height.

|                      | ![](assets/images/global/g_icon_ok.webp)                           | ![](assets/images/global/g_icon_nok.webp)                           |
|----------------------|--------------------------------------------------------------------|---------------------------------------------------------------------|
| Parallelism          | ![](assets/images/easydeepocr/structured_text_parallelism_ok.webp) | ![](assets/images/easydeepocr/structured_text_parallelism_nok.webp) |
| Line height          | ![](assets/images/easydeepocr/structured_text_line_ok.webp)        | ![](assets/images/easydeepocr/structured_text_line_nok.webp)        |
| Horizontal alignment | ![](assets/images/easydeepocr/structured_text_hor_ok.webp)         | ![](assets/images/easydeepocr/structured_text_hor_nok.webp)         |
| Vertical alignment   | ![](assets/images/easydeepocr/structured_text_ver_ok.webp)         | ![](assets/images/easydeepocr/structured_text_ver_nok.webp)         |
| Word spacing         | ![](assets/images/easydeepocr/structured_text_word_ok.webp)        | ![](assets/images/easydeepocr/structured_text_word_nok.webp)        |

<a id="edo-customusecases"></a>

### Optimization for Custom Use Cases

**EasyDeepOCR** also offers the possibility to optimize the reader for a custom use case.

* When doing so, an additional constraint is added to the list:
  * The texts must belong to the same custom use case as the one used for the optimization.
  * This optimization offers two potential benefits:
    * Increasing the processing speed.
    * Improving the detection of challenging texts.
* In the context of **EasyDeepOCR**, a *custom use case* is defined as follows:
  * It is a batch of images captured in the same conditions that depict a different instance of the same object.
  * For every image, you must designate a ‘text of interest’.
  * This ‘text of interest’ is the text that the `ETextReader` should retrieve.
  * From one image to another, all the ‘texts of interest’ must share some geometrical properties.<br />
    \\\\
    Specifically, they must have:
    * The same line height (in pixels).
    * The same font.
    * The same appearance (such as printed, embossed, dotted).

  #### NOTE
  There can be several ‘texts of interest’ in a given image, but all texts must share the above-mentioned geometrical properties.

<a id="edo-basic-workflow"></a>

## Basic Workflow

The full-featured **EasyDeepOCR** workflow consists of the following steps:

1. Instantiate an [`ETextReader`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html)
2. (Optional) Set the [`EDeepLearningExecutionSettings`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepLearningExecutionSettings.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepLearningExecutionSettings.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepLearningExecutionSettings.html)
3. Initialize
4. (Optional) Set the [`ETopology`](../../../doxygen_cpp/classeVision_1_1ETopology.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1ETopology.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1ETopology.html)
5. (Optional) Optimize
6. Read
7. Extract the [`EasyDeepOCR::EText`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1EText.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1EText.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1EText.html) results

![](assets/images/easydeepocr/workflow.svg)

This complete workflow is broken down and explained in the following sections:

* The section [Reading a Text](detailed_usage.html.md#edo-reading-a-text) goes through the minimal working example, without any optional steps.
* The section [Specifying a Topology](detailed_usage.html.md#edo-specifying-topology) explains how to create the appropriate topology for your use case.
* The section [Performing an Optimization](detailed_usage.html.md#edo-performing-optimization) demonstrates how to optimize the reader for a given use case.
* Finally, the section [Specifying the Execution Settings](setting_the_parameters.html.md#edo-specifying-execution-settings) explains how to properly set the deep learning execution settings.

<a id="edo-inputs"></a>

### Inputs

The reading method of an [`ETextReader`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html), namely [`ETextReader::Read()`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a89af65e87d9b4bcb08c67ccb6144bef6), accepts 2 input arguments:

* An ROI ([`EROIBW8`](../../../doxygen_cpp/classeVision_1_1EROIBW8.html) or [`EROIC24`](../../../doxygen_cpp/classeVision_1_1EROIC24.html)): the image to be searched for texts.
* An [`ERegion`](../../../doxygen_cpp/classeVision_1_1ERegion.html) (optionally) that defines a geometrical filter: any text whose 4 corners are not included in the region is filtered out.

<a id="edo-outputs"></a>

### Outputs

The method [`ETextReader::Read()`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a89af65e87d9b4bcb08c67ccb6144bef6) returns a vector of [`EText`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1EText.html) that contains the following information:

* An [`ERectangle`](../../../doxygen_cpp/classeVision_1_1ERectangle.html) representing the text position in the image
* A text string
* A vector of [`ETextLine`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextLine.html)

This vector of [`ETextLine`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextLine.html) represents the lines of the text and contains 2 pieces of information:

* An [`ERectangle`](../../../doxygen_cpp/classeVision_1_1ERectangle.html) representing the line position in the image
* A line string