<a id="edo-retraining-a-model"></a>

# Retraining a Model

<a id="edo-retraining-flowchart"></a>

## Flowchart

**EasyDeepOCR** uses several neural networks to locate, orient and recognize the texts.

In **Deep Learning Studio**, you can:

* Retrain some neural networks on a few images.
* Export these retrained models.
* Use them in an [`ETextReader`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html).

![](assets/images/easydeepocr/userretraining_flowchart.svg)

<a id="edo-trainable-models"></a>

## Trainable Models

There are 3 neural network models that you can retrain:

<a id="edo-trainable-location"></a>

### Location Model

* Properties:
  * Scale (value between 0 and 1): the downscaling is applied to the image before the inference.<br />
    \\\\
    By default, in **Deep Learning Studio**, the scale is set so that the minimum height of any ground truth text is 64 pixels.
  * Threshold (value between 0 and 1): the score under which the located texts are rejected.<br />
    \\\\
    By default, in **Deep Learning Studio**, the threshold is set after the training to maximize the recall (true positive rate).
* When to retrain:
  * When no text is located at all.
  * When the text is badly detected.
  * When the text of interest is printed on top of an unimportant text.

  ![](assets/images/easydeepocr/userretraining_locationretraining_badpred.jpg)![](assets/images/easydeepocr/userretraining_locationretraining_badpred2.jpg)![](assets/images/easydeepocr/userretraining_locationretraining_ignoretext.jpg)

<a id="edo-trainable-orientation"></a>

### Orientation Model

* Properties:
  * None.
* When to retrain:
  * When the direction of the text is wrong.

  ![](assets/images/easydeepocr/userretraining_orientationretraining_beforeafter.jpg)

<a id="edo-trainable-recognition"></a>

### Recognition Model

* Properties:
  * None.
* When to retrain:
  * When the predicted text has mistakes in it (missing character, character mistaken for another one…).

  ![](assets/images/easydeepocr/userretraining_recogntionretraining_wrongpred.jpg)
  * To identify new characters: annotate the new character using one of the characters in [the supported dictionary](index.html.md#edo-scope).

#### NOTE
In simple cases, retraining these models can work with as few as 3 or 4 images containing a single text. However, the actual requirements depend on various factors and may be much greater than this.

<a id="edo-training-custom-model"></a>

## Training a Custom Model

<a id="edo-training-custom-model-in-dlstudio"></a>

### In Deep Learning Studio

No license is needed to train a custom model with **Deep Learning Studio**.

1. Create a new project **EasyDeepOCR** in **Deep Learning Studio**

   ![](assets/images/easydeepocr/userretraining_dlstudio_step1.jpg)
2. Add your images and annotate them

   ![](assets/images/easydeepocr/userretraining_dlstudio_step2.jpg)
   1. Click on the button `Add images` (1) and select the images that you want to train and test with.
   2. Click on the thumbnail of an image (2) to edit its annotation (3).<br />
      \\\\
      To edit annotations:
      * Click on `Propose annotations` (4) to automatically propose annotations (that you must accept or reject). The proposed annotations are displayed in purple.

        ![](assets/images/easydeepocr/userretraining_dlstudio_step2_proposeannotations.jpg)
      * To accept or reject the proposed annotations:
        * Use the button `Accept all` (5) or `Reject all` (6) to accept or reject all the proposed annotations in one step.
        * To only accept some annotations or fix these, click on an annotation to edit its geometry, its text (8), accept it (9) or reject it (10).

        ![](assets/images/easydeepocr/userretraining_dlstudio_step2_proposeannotationsedit.jpg)
      * Add new annotations:
        * To draw the top line of the text in the direction of reading, click on the top left corner of the text and, while continuing to click on the mouse, drag it to the top right corner of the text.
        * Release the mouse and drag it to set the height of the text.
        * Write the ground truth text and press `ENTER` to validate the annotation.

        ![](assets/images/easydeepocr/userretraining_manualannotations.gif)
      * Valid annotations appear in the table (7)

        ![](assets/images/easydeepocr/userretraining_dlstudio_step2_annotationtable.jpg)

   #### HINT
   To copy/paste annotations within the same image or between images, use the standard shortcuts or right-click on an annotation (image or table).

   #### NOTE
   If the spacing separating two texts is much bigger than a character, do not annotate this as a single text separated by a space (’ ‘) character.
3. Create a dataset split
   * By default, we recommend to use the default proportion for the split.
   * For very small datasets, as the validation metrics may not be accurate due to a lack of samples, do not use any validation images. However, keep a few test images to make sure that your model does not overfit.
4. Create data augmentation settings for your use case

   #### NOTE
   Shear data augmentation is not supported for the location training.

   #### NOTE
   Rotation and flip data augmentation are automatically disabled when training an orientation or a recognition network.
5. Train your tool

   ![](assets/images/easydeepocr/userretraining_dlstudiotool.jpg)
   1. Create a new tool (1).
   2. Select the type of model that you want to train: location, orientation or recognition (2).
   3. Select the split (3) and data augmentation settings (4).
   4. Train your model (5).
6. Evaluate your results
   1. Location results

      ![](assets/images/easydeepocr/userretraining_dlstudio_validationlocation.jpg)
      * The left panel (1) displays the F-Score, the recall and the precision metrics and the score histogram of all the located texts.
        * The red curve in the histogram corresponds to the wrong predictions.
        * The green curve corresponds to the correct predictions.
        * The blue vertical line corresponds to the threshold.
      * For each image, the predictions are drawn atop the image and a list of all predictions is available in the right panel (2).
        * The predictions whose score are below the threshold are displayed in gray.
   2. Orientation results

      ![](assets/images/easydeepocr/userretraining_dlstudio_validationorientation.jpg)
      * The left panel (1) displays the error, the accuracy and the confusion matrix.
      * For each ground truth annotation, the predicted orientation is drawn atop the image:
        * The correct predictions are green.
        * The wrong predictions are red.
        * The selected elements are blue.
      * For each ground truth annotation, the list of predictions is available in the right panel (2).
        * All ground truths, by definition, are always Upright.
        * An Upright prediction is good while a Flipped prediction is wrong.
   3. Recognition results

      ![](assets/images/easydeepocr/userretraining_dlstudio_validationrecognition.jpg)
      * The left panel (1) displays the image-wise and word-wise accuracies.
        * The image-wise accuracy refers to the ratio of images in which all texts are correctly recognized.
        * The word-wise accuracy refers to the ratio of texts that are correctly recognized in all images.
      * For each ground truth annotation, the predicted text is drawn below the box of each ground truth text.
        * The correct predictions are green.
        * The wrong predictions are red.
        * The selected elements are blue.
      * For each ground truth annotation, the list of predicted texts is available in the right panel (2).
7. Export the tool

   ![](assets/images/easydeepocr/userretraining_dlstudio_export.jpg)
   1. Go to the tab `Tools` (1).
   2. Select the tool you want to export.
   3. Click on Export > For Inference Only (2).

   #### HINT
   For more information about the advanced training parameters, see [Deep Learning Inspection Tools](../../deep_learning/index.html.md).

<a id="edo-training-custom-model-in-api"></a>

### In the API

* You can train an **EasyDeepOCR** model with the API.
* You need an **EasyDeepOCR** license to train a custom model with the API.

1. Create the dataset

   Use the class [`EClassificationDataset`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EClassificationDataset.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EClassificationDataset.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EClassificationDataset.html) to create and annotate your image to train the **EasyDeepOCR** models.
2. Train the models
   * To train an **EasyDeepOCR** model, use the class [`EDeepOCRTool`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html).
     * To control the type of model that is trained, set [`EDeepOCRTool::SetModel`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html#ad6636db107a0979f4e4be79db764359c) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html#a042748f7656878e71bb71d3ed2bdca3b) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html#a70d66a5e70fabcbc41c17f72e1e68724) as [`EDeepOCRModel_Location`](../../../doxygen_cpp/namespaceeVision_1_1EasyDeepLearning.html#a554948333ddeddfe56b3eb55eb88b01d) [<sub>.NET</sub>](../../../doxygen_cs/namespaceeVision_1_1EasyDeepLearning.html#a2660103d208ef3df6d13e44ff29bb539) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRModel.html), [`EDeepOCRModel_Orientation`](../../../doxygen_cpp/namespaceeVision_1_1EasyDeepLearning.html#a554948333ddeddfe56b3eb55eb88b01d) [<sub>.NET</sub>](../../../doxygen_cs/namespaceeVision_1_1EasyDeepLearning.html#a2660103d208ef3df6d13e44ff29bb539) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRModel.html) or [`EDeepOCRModel_Recognition`](../../../doxygen_cpp/namespaceeVision_1_1EasyDeepLearning.html#a554948333ddeddfe56b3eb55eb88b01d) [<sub>.NET</sub>](../../../doxygen_cs/namespaceeVision_1_1EasyDeepLearning.html#a2660103d208ef3df6d13e44ff29bb539) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRModel.html).
     * Each model has its own set of parameters: [`EDeepOCRTool::SetParameters`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html#a3ca6be796aa941d047dca7bc6ed63207) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html#ad5c9524e29c30eca4aa3bca723fb5f07) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html#ab19b50f79a02dc01a0b561a9205cc06a).
     * Currently, only the location model has parameters (in the class [`EDeepOCRModelParametersTextLocation`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRModelParametersTextLocation.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRModelParametersTextLocation.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRModelParametersTextLocation.html)).

   #### WARNING
   An object [`EDeepOCRTool`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) is not capable of performing an inference. Use the tool with [`ETextReader`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html) to perform inference.

#### SEE ALSO
[Code snippet](../../../resources/code_snippets/text_and_code_reading/easydeepocr/trainingandusingcustommodel.html.md)

<a id="edo-using-custom-model"></a>

## Using a Custom Model

#### WARNING
In **EasyDeepOCR**, the results can be different from those in **Deep Learning Studio**.<br />
\\\\
This is due to several reasons:

* **Deep Learning Studio** uses the ground truth text box as input for the orientation and the recognition models while **EasyDeepOCR** uses the output of the location model.
* Various additional rules to handle small texts, text height and orientation hints can affect the final results.

<a id="edo-using-custom-model-in-evision-studio"></a>

### In eVision Studio

![](assets/images/easydeepocr/userretraining_locationretraining_studio.jpg)![](assets/images/easydeepocr/userretraining_locationretraining_studiocustom.jpg)

You can load the models you exported from **Deep Learning Studio** directly in the text reader tool of **eVision Studio**.

* When the custom models are set to Default, it means that the default models of **EasyDeepOCR** are used.
* Otherwise, it indicates the filename (1) that you selected when clicking on Browse (2). Use the cross button (3) to remove the custom model and use the default model again.

<a id="edo-using-custom-model-in-api"></a>

### In the API

For each type of model, the API has:

* A setter that takes the path to a saved [`EDeepOCRTool`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) (for ex. [`ETextReader::SetLocationCustomModelPath`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a6e6bf6c075d4a44da4dba0a957f59a55) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#aac25cc31e69f87220126e9aaec9f33bb) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a107ead3e95f02bef36b01acb70f9c55e)).
* A setter that takes an object [`EDeepOCRTool`](../../../doxygen_cpp/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepLearning_1_1EDeepOCRTool.html) (for ex. [`ETextReader::SetRecognitionCustomModel`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#adb9e0204fc84fb94d008828965df8219) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#ab2697e722edefaaa4dd7760409024294) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a5b1f95e854a8b5262750803dda20b4e2)).
* A method to check if a custom model is set (for ex. [`ETextReader::HasOrientationCustomModel`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#ada2472aea01164a633c154b23016e95c) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a13ac0e71145929cc8c65273578c586d7) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a24b9652bdcc7b1ec06daa0857e182d35)).
* A method to remove the custom model and use the default model (for ex. [`ETextReader::ResetLocationCustomModel`](../../../doxygen_cpp/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#ae140099cf45a696d96d451bb6658cdaa) [<sub>.NET</sub>](../../../doxygen_cs/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a71588e95e2891388976c5644eef57fd7) [<sub>Python</sub>](../../../doxygen_python/classeVision_1_1EasyDeepOCR_1_1ETextReader.html#a8edf0eec781446db01d891a839cb6e06)).

#### SEE ALSO
[Code snippet](../../../resources/code_snippets/text_and_code_reading/easydeepocr/trainingandusingcustommodel.html.md)