<a id="easyocr2"></a>

# EasyOCR2 - Reading Complex Texts

<a id="easyocr2-purpose"></a>

## Purpose and Principles

**EasyOCR2** is an optical recognition tool designed to read short texts such as serial numbers, expiry dates or lot codes printed on labels or on parts.

![](assets/images/easyocr2/functional_step_1.jpg)

It segments pixels then detects text blobs and sets textboxes over the detected blobs following a user-defined topology.

![](assets/images/easyocr2/functional_step_2.jpg)![](assets/images/easyocr2/functional_step_3.jpg)

The topology specifies the number of lines, words and characters in the text. You can also specify a character type (letter, digit and/or symbol) for each character in the text, to improve the recognition rate and speed.

**EasyOCR2** supports up-to-360-degree rotated texts, non-uniform illumination and textured backgrounds as well as dot-printed or fragmented characters.

To recognize characters, **EasyOCR2** uses a pretrained classifier, powered by deep learning technologies, or a classifier that was trained on your character database.

For each input character:

* The classifier calculates a score for all candidate outputs.
* It returns the candidate with the highest score as the recognition result.

![](assets/images/easyocr2/functional_step_4.jpg)

<a id="easyocr2-workflow"></a>

## Workflow

<a id="easyocr2-learning"></a>

### Learning Mode

![](assets/images/easyocr2/workflow_learn.svg)

<a id="easyocr2-production"></a>

### Production Mode

![image](assets/images/easyocr2/workflow_production.svg)

<a id="easyocr2-contents"></a>

## Contents

Learn how to use **EasyOCR2**.

Learn how to correctly setup the parameters of **EasyOCR2**.

<a id="easyocr2-quick-links"></a>

## Quick Links

List of all Classes, Structs and Enumerations of the **EasyOCR2** library.

Code snippets for the **EasyOCR2** library.

#### SEE ALSO
Some **eVision Studio** samples illustrate several aspects of the **EasyOCR2** library:

* `EasyOCR2 text reading with a database classifier`: Uses **EasyOCR2** to loads an image and uses a character database to read it.
* `EasyOCR2 text reading with a deep learning recognizer`: Uses **EasyOCR2** to loads an image and uses the deep learning recognizer ‘Industrial’ to read it.