eVision Python API
Loading...
Searching...
No Matches
Class List
Here are the classes, structs, unions and interfaces with brief descriptions:
 NeVision
 NEasy3D
 CE3DAttributeThis enumeration contains the possible attributes of the eVision.Easy3D.EPointCloud in addition to the eVision.Easy3D.E3DPoint
 CE3DObjectFeatureThe list of possible extracted features for eVision.Easy3D.E3DObject
 CE3DPlaneNormalOrientationOrient the normal of the plane such that normal.X/Y/Z is positive/negative
 CEAlignmentPolarityPolarity of an alignment, used in eVision.Easy3D.EFeaturesAligner
 CEAlignmentTypeType of alignment to perform by eVision.Easy3D.EFeaturesAligner
 CEAttributeTypeThis enumeration contains the possible types for the eVision.Easy3D.E3DAttribute
 CEAxisOriginModeThis enumeration contains the possible values for the parameter of eVision.Easy3D.E3DViewer.AxisOrigin method
 CEAxisSystemTypeAxis type used in a eVision.Easy3D.EZMap or eVision.Easy3D.EDepthMap
 CECalibrationTypeThe Easy3D calibration type
 CEColorRampModeThis enumeration contains the possible values for the parameter of eVision.Easy3D.E3DViewer.GenerateColors method
 CEComparisonDistanceModeThis enumeration specifies the distance mode for the 3D comparison
 CEFillUndefinedPixelsDirectionDirection in which the undefined pixels are filled in a depthmap
 CEFillUndefinedPixelsMethodMethod to fill the undefined pixels in a depthmap
 CEMapConversionModeConversion modes to use in eVision.Easy3D.EConverter
 CEMaximumAnalysisModeThis enumeration contains the possible values for the analysis mode of the eVision.Easy3D.ELaserLineExtractor object
 CENoiseRemovalMethodType of filter used in method eVision.Easy3D.EFilters.RemoveNoise
 CEObjectBasedCalibrationPrecisionVsSpeedTradeOffThe precision vs speed trade-off
 CEObjectBasedCalibrationTypeThe type of the calibration object
 CEPhotometricStereoContrastThis enumeration contains the possible ways to handle the contrast when retrieving Albedos, Gaussian curvatures or Mean curvatures
 CEPlaneCropperTypeType of crop to use in eVision.Easy3D.EPlaneCropper
 CEPointCloudFilteringMethodType of filtering method to use in eVision.Easy3D.EPointCloudFilter
 CEPreservationModeEnum defining what quantities related to the X, Y and Z axes are preserved by eVision.Easy3D.EZMapLeveler
 CEProjectionTypeThis enumeration contains the possible values for the parameter of eVision.Easy3D.E3DViewer.ProjectionType method
 CESourceColorModeThis enumeration contains the modes for the display of the point cloud colors
 CETextLabelAlignmentThis enumeration contains the alignment of the text labels
 CEUIAPIThis enumeration contains the various User Interface API supported by eVision.Easy3D.E3DViewer
 CEViewDirectionThis enumeration contains the axis aligned view directions
 CEZMapGeneratorResolutionXYModeMode used to specify the resolution of the ZMap generated on the x and y axes
 CEZMapGeneratorZResolutionFailureHandlerMode used to specify what to do when the Z Resolution set is too small to represent all the data
 CEZMapImageToWorldKernelRepresents the kernel to use to compute the Z coordinate of the worldPoint in eVision.Easy3D.EZMap.ImageToWorld
 CEZMapOrientationVectorModeThe eVision.Easy3D.EZMap orientation, it's the direction of the X (width) axis of the ZMap
 CEZMapReferencePlaneModeThe 3D reference plane used to build the eVision.Easy3D.EZMap
 CE3DAlignerAligns an eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap on a reference eVision.Easy3D.EMesh, eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap
 CE3DAlignmentRepresents a 3D Alignment returned by eVision.Easy3D.E3DAligner
 CE3DAnomalyRepresents a detected 3D anomaly
 CE3DAxisDisplayRepresents the axis and the grid to display in the eVision.Easy3D.E3DViewer
 CE3DAxisSystemRepresent a 3D base axis system
 CE3DBoxA 3D box, used as bounding volume for eVision.Easy3D.E3DObject class
 CE3DComparerRepresents a 3D comparison context
 CE3DLineRepresents a 3D line
 CE3DMatchRepresents a 3D match returned by eVision.Easy3D.E3DMatcher
 CE3DMatcherAligns an eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap on and compares it with a reference eVision.Easy3D.EMesh, eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap
 CE3DObjectA eVision.Easy3D.E3DObject is a geometric description of a set of 3D points, produced by E3DObjectExtractor
 CE3DObjectExtractoreVision.Easy3D.E3DObjectExtractor is used to extract 3D objects from a ZMap
 CE3DOrthonormalAxisSystemE3DOrthonormalAxisSystem is a subassembly of eVision.Easy3D.E3DAxisSystem with properties Orthogonal and Normed
 CE3DPlaneRepresents a 3D plane
 CE3DRightOrthonormalAxisSystemE3DRightOrthonormalAxisSystem is a subassembly of eVision.Easy3D.E3DAxisSystem with properties Orthogonal and Normed and Right
 CE3DSphereRepresents a 3D sphere
 CE3DTransformMatrixRepresents a 3D transformation [4x4] matrix
 CE3DViewerManages a viewer window for eVision.Easy3D.EPointCloud
 CEAffineTransformerManages a 3D coordinates transformation context
 CECalibrationGeneratorRepresents a 3D calibration model generator, a class made to compute calibration models
 CECalibrationModelRepresents a 3D calibration model
 CEConverterConversion functions between bit depth formats of various 3D classes
 CEDecimatorDecimation of a point cloud/ZMap/DepthMap
 CEDepthMapRepresents a generic DepthMap type interface
 CEDepthMap16Represents a eVision.Easy3D.EDepthMap with an 16-bit pixel internal representation
 CEDepthMap32fRepresents a eVision.Easy3D.EDepthMap with an 32-bit pixel internal representation
 CEDepthMap8Represents a eVision.Easy3D.EDepthMap with an internal 8-bit pixel representation
 CEDepthMapToMeshConverterPerforms the conversion from a eVision.Easy3D.EDepthMap to a eVision.Easy3D.EMesh, using the given calibration model
 CEDepthMapToPointCloudConverterPerforms the conversion from a eVision.Easy3D.EDepthMap to a eVision.Easy3D.EPointCloud, using the given calibration model
 CEErrorStatisticsThis object contains the error statistics (deviation between model and aligned points)
 CEExplicitGeometricCalibrationModeleVision.Easy3D.EExplicitGeometricCalibrationModel is used to calibrate a depth map from a minimal set of explicit geometric values
 CEFeaturesAlignerAlignment class, used to calculate the best transformation between matching pairs of points
 CEFiltersFiltering functions used to remove noise on 3D containers
 CEGridDecimatorDecimation of an eVision.Easy3D.EPointCloud
 CELaserLineExtractorManages a laser line extraction context
 CEMeshRepresents a 3D meshed object
 CEMeshToZMapConverterComputes an eVision.Easy3D.EZMap from an eVision.Easy3D.EMesh
 CEObjectBasedCalibrationGeneratorRepresents an object-based 3D calibration generator
 CEObjectBasedCalibrationModeleVision.Easy3D.EObjectBasedCalibrationModel is an Easy3D calibration model built from a scan of a reference object
 CEPhotometricStereoImagerManages photometric stereo reconstruction
 CEPlaneCropperA eVision.Easy3D.EPlaneCropper object is used to crop some points of a eVision.Easy3D.EPointCloud object
 CEPlaneFinderA eVision.Easy3D.EPlaneFinder object is used to search an eVision.Easy3D.E3DPlane in an eVision.Easy3D.EPointCloud
 CEPlaneFitterA eVision.Easy3D.EPlaneFitter object is used to fit an eVision.Easy3D.E3DPlane on an eVision.Easy3D.EPointCloud
 CEPointCloudRepresents a 3D point cloud
 CEPointCloudFactoryManages a context for creating point clouds of specific shapes
 CEPointCloudFilterAn eVision.Easy3D.EPointCloudFilter is used to filter some points out of an eVision.Easy3D.EPointCloud
 CEPointCloudMergerMerges several eVision.Easy3D.EPointCloud of the same scene from different sensors after having performed a calibration
 CEPointCloudStatisticsManages a context for retrieving statistics on an eVision.Easy3D.EPointCloud
 CEPointCloudToMeshConverterPerforms the conversion from an eVision.Easy3D.EPointCloud to an eVision.Easy3D.EMesh
 CEPointCloudToZMapConverterComputes an eVision.Easy3D.EZMap from an eVision.Easy3D.EPointCloud
 CEPrincipalAxisExtractorA eVision.Easy3D.EPrincipalAxisExtractor object computes the principal axis analysis (PCA) on an eVision.Easy3D.EPointCloud and produces a eVision.Easy3D.E3DTransformMatrix as a result
 CERandomDecimatorDecimation of an eVision.Easy3D.EPointCloud
 CERectangularCropperManages a point cloud cropper in the shape of a rectangular parallelepiped
 CEScaleCalibrationModeleVision.Easy3D.EScaleCalibrationModel is used to convert depth map 2.5D point to 3D world position, only by applying a scale factor
 CESimpleCropperManages a point cloud cropper based on X/Y/Z value ranges
 CESphereFitterA eVision.Easy3D.ESphereFitter object is used to fit an eVision.Easy3D.E3DSphere on an eVision.Easy3D.EPointCloud
 CESphericalCropperManages a spherical point cloud cropper
 CEStatisticsCalculates various statistics on the pixels values of an eVision.Easy3D.EDepthMap or eVision.Easy3D.EZMap
 CEUtils3D Utilitarian Functions
 CEZMapRepresents a generic ZMap type interface
 CEZMap16A ZMap16 is a 16bits corrected 2.5D image
 CEZMap32fA ZMap32f is a 32bits corrected 2.5D image
 CEZMap8A ZMap8 is a 8bits corrected 2.5D image
 CEZMapLevelerClass performing the leveling of an eVision.Easy3D.EZMap
 CEZMapToMeshConverterPerforms the conversion from an eVision.Easy3D.EZMap to an eVision.Easy3D.EMesh
 CEZMapToPointCloudConverterGenerates an eVision.Easy3D.EPointCloud from a ZMap
 CTextLabelA class representing a text label that can be displayed using eVision.Easy3D.E3DViewer
 CE3DClosestPointStruct containing the eVision.Easy3D.E3DPoint of an eVision.Easy3D.EPointCloud that is closest to a line or segment with its index in the cloud and its distance to the line or segment
 CE3DPointRepresents a 3D point with floating point coordinates
 CEAnomalyThresholdsThresholds used to define an anomaly in Easy3DMatch
 CEAzimuthElevationAnglesAzimuth and Elevation Angles
 CEEdgeCroppingParametersParameters used to defined edge cropping in Easy3DMatch
 CERenderStyleRepresents how to visualize 3D Objects in a E3DViewer
 CEStatistics16Statistics on the pixels values of an eVision.Easy3D.EDepthMap16 or eVision.Easy3D.EZMap16 computed by eVision.Easy3D.EStatistics
 CEStatistics32fStatistics on the pixels values of an eVision.Easy3D.EDepthMap or eVision.Easy3D.EZMap computed by eVision.Easy3D.EStatistics
 CEStatistics8Statistics on the pixels values of an eVision.Easy3D.EDepthMap8 or eVision.Easy3D.EZMap8 computed by eVision.Easy3D.EStatistics
 NEasyBarCode2
 CEBarCodeSymbologiesEnum representing the different symbologies of barcodes that can be read by an eVision.EasyBarCode2.EBarCodeReader
 CEReadingOrientationRepresents the orientation to assume when decoding a barcode without start/stop patterns, for example those of eVision.EasyBarCode2.EBarCodeSymbologies.PharmacodeOneTrack
 CEBarCodeRepresents a 1D Bar Code
 CEBarCodeGridRepresents a grid of Data Barcodes
 CEBarCodeReaderRepresents a 1D Bar Code Reading Context
 CEBarCodeGradingParametersRepresents the grading Parameters associated with an eVision.EasyBarCode2.EBarCode as defined by ISO15416
 CEBarCodeGridDrawOptionsList of options to customize the drawing of the bar codes
 NEasyDeepLearning
 CEClassifierCapacityThe capacity of the classifier network
 CEConfusionMatrixElementThe various elements representing the cases of the 2x2 confusion matrix used in eVision.EasyDeepLearning.EDeepLearningDefectDetectionMetrics
 CEDatasetTypeType of dataset split
 CEDeepLearningDeviceTypeDifferent types of Deep Learning device
 CEDeepLearningInferencePrecisionPrecisions supported by a Deep Learning device
 CEDeepLearningLearningRateTypeThe type of learning rate indicates how the learning rate changes during training
 CEDeepLearningToolTypeType of EasyDeepLearning tool
 CEDeepOCRModelEasyDeepOCR models that are trainable with eVision.EasyDeepLearning.EDeepOCRTool
 CEDLDataAugmentationTypeThis enum represents how the data augmentation transformation are generated
 CEHeatmapColormapColor maps for visualizing the heatmap
 CEImageAnnotationFormatSupported formats of annotation files for image file
 CELocatorCapacityThe capacity of the locator deep learning network
 CELocatorFeatureFeatures supported by the eVision.EasyDeepLearning.ELocator or eVision.EasyDeepLearning.ELocatorObject
 CESupervisedSegmenterCapacityThe capacity of the supervised segmentation network
 CEUnsupervisedSegmenterCapacityThe capacity of the unsupervised network
 CEClassificationDataseteVision.EasyDeepLearning.EClassificationDataset manages a dataset of images
 CEClassificationMetricsCollection of metrics used to evaluate the state of an eVision.EasyDeepLearning.EClassifier
 CEClassificationResultAn eVision.EasyDeepLearning.EClassificationResult object represents the result of a classification
 CEClassifiereVision.EasyDeepLearning.EClassifier allows to train a classifier using an eVision.EasyDeepLearning.EDataset object and classify new images
 CEDataAugmentationAn eVision.EasyDeepLearning.EDataAugmentation object is responsible for storing the data augmentation parameters and generating new transformed images from existing ones
 CEDataseteVision.EasyDeepLearning.EDataset manages a dataset of images
 CEDatasetSplitThe eVision.EasyDeepLearning.EDatasetSplit maps the image indexes of a eVision.EasyDeepLearning.EDataset to a dataset split type (eVision.EasyDeepLearning.EDatasetType)
 CEDeepLearningBenchmarkDeep Learning benchmark results
 CEDeepLearningBenchmarkSettingsClass representing the settings of a Deep Learning benchmark
 CEDeepLearningDefectDetectionMetricsCollection of metrics used to evaluate a defect detection problem where the detection is based on the thresholding of a score produced by the underlying deep learning tool, e.g
 CEDeepLearningDeviceClass representing a device that can run a neural network
 CEDeepLearningExecutionSettingsExecution settings for a Deep Learning tool
 CEDeepLearningProjectDeep learning project
 CEDeepLearningTooleVision.EasyDeepLearning.EDeepLearningTool represents the common operations of deep learning tools
 CEDeepOCRModelParametersBase class for the parameters of EasyDeepOCR models for user retraining
 CEDeepOCRModelParametersTextLocationParameters for the user retraining of the text location model of EasyDeepOCR
 CEDeepOCRToolTrains the EasyDeepOCR Deep Learning models
 CEDeepOCRToolMetricsMetrics for eVision.EasyDeepLearning.EDeepOCRTool
 CEDeepOCRToolResultResult for eVision.EasyDeepLearning.EDeepOCRTool
 CEInterestPointLocatorEasyLocate tool - interest point version
 CELocatorEasyLocate tool - axis aligned bounding box version
 CELocatorBaseBase class for EasyLocate tool
 CELocatorMetricsCollection of metrics used to evaluate the results of a eVision.EasyDeepLearning.ELocator tool
 CELocatorMetricsGeneratorLocator metric generator
 CELocatorObjectObject for a eVision.EasyDeepLearning.ELocator tool
 CELocatorPredictedObjectObject predicted by a eVision.EasyDeepLearning.ELocator tool
 CELocatorResultResult of a eVision.EasyDeepLearning.ELocator tool
 CESupervisedSegmenterSupervised segmentation tool
 CESupervisedSegmenterBlobA blob detected by a supervised segmentation tool (see eVision.EasyDeepLearning.ESupervisedSegmenter and eVision.EasyDeepLearning.ESupervisedSegmenterResult)
 CESupervisedSegmenterMetricsCollection of metrics used to evaluate the state of a eVision.EasyDeepLearning.ESupervisedSegmenter tool
 CESupervisedSegmenterResultAn eVision.EasyDeepLearning.ESupervisedSegmenterResult object represents the result of a supervised segmenter
 CEUnsupervisedSegmenterUnsupervised segmentation tool
 CEUnsupervisedSegmenterMetricsCollection of metrics used to evaluate the state of an eVision.EasyDeepLearning.EUnsupervisedSegmenter
 CEUnsupervisedSegmenterResultAn eVision.EasyDeepLearning.EUnsupervisedSegmenterResult object represents the result of a eVision.EasyDeepLearning.EUnsupervisedSegmenter tool
 CEROCPointThe structure representing a point on the ROC (Receiver Operating Characteristic) curve
 CEWeightedPrecisionRecallPointWeighted precision and recall for a given threshold
 NEasyDeepOCR
 CEOptimizationReportAn eVision.EasyDeepOCR.EOptimizationReport stores information about the optimization of an eVision.EasyDeepOCR.ETextReader (eVision.EasyDeepOCR.ETextReader.Optimize)
 CESampleA sample is composed of an image, and optionally a region, together with one or several texts, which are visible in the image
 CESampleListHolds a list of samples
 CETextRepresents a text detected by a eVision.EasyDeepOCR.ETextReader
 CETextDrawingParametersRepresents the drawing parameters needed by eVision.EasyDeepOCR.ETextLine.Draw and eVision.EasyDeepOCR.EText.Draw
 CETextLineRepresents a text line detected by a eVision.EasyDeepOCR.ETextReader
 CETextReaderA eVision.EasyDeepOCR.ETextReader aims to find and read texts inside a given ROI, through eVision.EasyDeepOCR.ETextReader.Read
 NEasyMatrixCode2
 CECC000FamilyFamily of error corrections used
 CEReadModeThis enumeration contains the possible operation modes for the eVision.EasyMatrixCode2.EMatrixCodeReader.Read method
 CEMatrixCodeHolds all the information regarding a single Data Matrix code: its decoded string, its grading, its errors and more
 CEMatrixCodeGridRepresents a grid of Data Matrix Codes
 CEMatrixCodeReaderAn eVision.EasyMatrixCode2.EMatrixCodeReader instance can detect, decode and grade matrixcodes in an ROI, it returns a vector of eVision.EasyMatrixCode2.EMatrixCode instances
 CEMatrixCodeGridDrawOptionsList of options to customize the drawing of the matrix codes
 NLegacy
 CEFiducialMatchingModeAllowed values for the fiducial finder mode in EChecker
 CEPolygonMeasurementModePolygonGauge measurement mode
 CECheckerManages a complete context for the inspection tool based on image comparison in EasyOCV
 CEChecker2Manages a complete context for the EChecker2 golden template inspection tool
 CECircleRepresents a model of a circle (or arc) in EasyGauge
 CECircleGaugeManages a circle fitting gauge
 CECircleShapeManages a circle shape
 CEFrameRepresents a geometrical frame of reference as well as the parameters needed to transform from/to local and global coordinates
 CEFrameShapeManages a complete context for measuring frame shapes
 CELineRepresents a model of a line segment
 CELineGaugeManages a line fitting gauge
 CELineShapeManages a line shape
 CEPointGaugeManages a point location gauge
 CEPointShapeManages a point shape context
 CEPolygonRepresents a polygon
 CEPolygonGaugeManages a polygon fitting gauge
 CEPolygonShapeManages a polygonal shape
 CERectangleRepresents a model of a rectangle
 CERectangleGaugeManages a rectangle fitting gauge
 CERectangleShapeManages a rectangle shape
 CESamplePointA point sampled by a gauge
 CEShapeAbstract class to federate the classes that can be hierarchically attached together (from a geometrical point of view)
 CEWedgeRepresents a model of a wedge (disk, ring, sector or curvilinear quadrilateral)
 CEWedgeGaugeManages a wedge fitting gauge
 CEWedgeShapeManages a wedge shape
 CEWorldShapeManages a complete context for calibrating a field of view
 NLicenseFeatures
 CFeaturesEVision Features
 NSegmenters
 CEColorRangeThresholdSegmenterSegments an image using a double threshold on a color image
 CEColorSingleThresholdSegmenterSegments an image using a single threshold on a color image
 CEGrayscaleDoubleThresholdSegmenterSegments an image using a double threshold on a grayscale image
 CEGrayscaleSingleThresholdSegmenterSegments an image using a single threshold on a grayscale image
 CEImageRangeSegmenterSegments an image using a pixel-by-pixel double threshold given as two images
 CEImageSegmenterBase class from which all the segmenters derive
 CELabeledImageSegmenterSegments an image by mapping the value of the pixels directly to a layer index
 CEReferenceImageSegmenterSegments an image using a pixel-by-pixel single threshold given as an image
 CEThreeLayersImageSegmenterThe base class from which all the segmenters that produce three layers derive
 CETwoLayersImageSegmenterThe base class from which all the segmenters that produce two layers derive
 CEAdaptiveThresholdMethodAdaptive thresholding modes
 CEAngleUnitThe angle units that are supported by eVision
 CEArithmeticLogicOperationSupported arithmetic or logic pixel-wise operators
 CEasyOCR2CharacterFilterThis enumeration contains the possible filters for loading fonts in eVision.EOCR2
 CEasyOCR2CharacterType
 CEasyOCR2CharSpacingBiasThis enumeration contains the possible biases for the optimized character spacing in the detection phase of eVision.EOCR2
 CEasyOCR2CharWidthBiasThis enumeration contains the possible biases for the optimized character width in the detection phase of eVision.EOCR2
 CEasyOCR2DrawDetectionStyleThis enumeration contains the possible drawing styles for the detection results in eVision.EOCR2
 CEasyOCR2DrawRecognitionStyleThis enumeration contains the possible drawing styles for the recognition results in eVision.EOCR2
 CEasyOCR2DrawSegmentationStyleThis enumeration contains the possible drawing styles for the segmentation results in eVision.EOCR2
 CEasyOCR2TextPolarityThis enumeration contains the possible polarities of text searched during segmentation in eVision.EOCR2
 CEBayerConfigurationThe Bayer image color configuration of the first two pixels
 CEByteInterpretationModeThis enumeration contains the available modes to interpret bytes values of a decoded string
 CECalibrationModeAllowed values for the calibration mode
 CECannyThresholdingModeThe thresholding modes for the Canny edge detector
 CECellColorAllowed values for a cell color (Black or White)
 CECharCreationModeAllowed values for the character creation mode in EasyOCV
 CEClippingModeAllows to choose how the fitted segment length and centre are computed
 CECodeTypeRepresents a type of Code
 CEColorQuantizationAllowed values for the quantization mode in EasyColor
 CEColorSystemThe color systems that are supported by eVision
 CEConnexityPossible values for the connexity of a contour
 CEContourModePossible modes for contour traversal
 CEContourThresholdAllowed thresholding modes for contour traversal
 CECorrelationModeAllowed values for the EasyMatch correlation mode
 CEDataSizePossible data sizes for an object feature
 CEDataTypePossible data types for an object feature
 CEDegreesOfFreedomAllowed values for the degrees of freedom in eVision.EChecker
 CEDiagnosticPossible defect codes in EasyOCV
 CEDongleTypeDongle types
 CEDoubleThresholdModeThe double threshold mode for the selection of coded elements with respect to a given feature
 CEDraggingModeDefines how the shape could be dragged
 CEDragHandleAllowed values for a handle identifier in the context of handle dragging
 CEDrawableFeatureThe various features that can be drawn for coded elements
 CEDrawingModeAllowed modes to draw the bounding box of a symbol
 CEDrawRegionEnum specifying how to draw the eVision.ERegion that may be associated with an eVision.EFoundPattern
 CEEditionModeThis enumeration is used to select which graphical interactions are allowed
 CEEncodingConnexityThe connexity mode for the encoding process
 CEErrorPossible eVision error codes
 CEFamilyAllowed values for the ECC symbol family in EasyMatrixCode
 CEFeatureThe various features that can be measured on the coded elements of a selection
 CEFilteringModeAllowed values for the filtering mode of EasyMatch
 CEFindContrastModeAllowed values for the contrast mode of EasyFind
 CEFlipAxisAxis for flipping
 CEFlippingAllowed values for the symbol flipping type in EasyMatrixCode
 CEFontStyleFont style
 CEFramePositionThis enumeration contains the possible values for the placement of the overlay frame edges that are drawn to highlight the position of an ROI
 CEFrameScalingScaling used to construct an eVision.EFrame from other objects
 CEFrequentialDomainFormatThis enumeration represents the supported data formats for frequential domain images
 CEGrayscaleSingleThresholdThe modes that are available to segment a grayscale image using a single threshold
 CEHarrisThresholdingModeThe thresholding modes for the Harris corner detector
 CEHistogramFeatureThe various parameters that can be extracted from a histogram
 CEHitAndMissValueThe allowed values for the elements of a hit-and-miss kernel
 CEImageFileTypeEnum representing the file types supported by eVision
 CEImageTypeImage type
 CEInterpolationModeEstimation function to apply when resizing an image
 CEKernelRectifierPossible values for the rectification mode of a kernel
 CEKernelRotationPossible values for rotating a convolution kernel
 CEKernelTypeThe types of convolution kernels that are supported by eVision
 CELearningModeAllowed values for the learning mode in EasyOCV
 CELearnParamAllowed values for the kind of parameters that can be learnt by EasyMatrixCode
 CELegacyFeatureThe various parameters that can be extracted from a histogram
 CELineSpacingModeAllowed values for the line spacing mode of EasyOCR
 CELocalSearchModeAllowed values for the local search mode of EasyFind
 CELocationModeAllowed values for the kind of pre-processing to be applied to the sample image in EasyOCV
 CELogicalSizeAllowed values for the logical size of Data Matrix codes in EasyMatrixCode
 CEMailBarcodeOrientationThe orientations supported by EMailBarcode
 CEMailBarcodeSymbologiesThe symbologies supported by EMailBarcode
 CEMatchContrastModeAllowed values for the contrast mode of EasyMatch
 CEMatchingModeAllowed values for the matching mode of EasyOCR
 CEMatrixCodeContrastModeEnum representing the contrast mode of an EMatrixCode
 CEMergerTypeType of merger algorithm to use
 CENormalizationModeAllowed values for the gray-level normalization mode in EChecker and EasyOCV
 CEObjectTemplateMatcherAlignmentThe type of alignment perform by eVision.EObjectTemplateMatcher priori to matching the objects
 CEOCR2ClassifierThis enumeration contains the different types of classifier for character recognition in eVision.EOCR2
 CEOCR2DetectionMethodThis enumeration contains the possible methods for text detection in eVision.EOCR2
 CEOCR2SegmentationMethodThis enumeration contains the possible methods for image segmentation in eVision.EOCR2
 CEOCRClassAllowed values for the class of pattern in EasyOCR
 CEOCRColorAllowed values for the text color in EasyOCR
 CEPathVectorDrawOptionEnum representing the drawing options of an eVision.EPathVector
 CEPatternStyleAllowed values for the nature of the pattern in EasyFind
 CEPatternTypeAllowed values for the type of patterns in EasyFind
 CEPenStylePen style
 CEPlotItemDefines how the profile is drawed across a gauge
 CEPolygonMeasurementModePolygonGauge measurement mode
 CEQRCodeCodingModeThis enumeration contains the possible values for the coding mode of a QR code
 CEQRCodeEncodingThis enumeration contains the possible values for the encoding used for parts of the bit stream of a QR code, contained by the eVision.EQRCodeDecodedStreamPart object
 CEQRCodeLevelThis enumeration contains the possible values for the level of error correction of a QR code
 CEQRCodeModelThis enumeration contains the possible values for a QR code model
 CEQRCodePerspectiveModeThis enumeration contains the possible values for the scanning precision of an eVision.EQRCodeReader object
 CEQRCodeScanPrecisionThis enumeration contains the possible values for the scanning precision used by an eVision.EQRCodeReader object
 CEQRDetectionMethodThis enumeration contains the possible detection methods the eVision.EQRCodeReader can use to detect QR codes
 CEQRDetectionTradeOffThis enumeration contains several settings for the trade-off between detection speed and reliability of the EasyQRCode methods
 CEQualityIndicatorAllowed values for the quality indicators in EasyOCV
 CERectangleGaugeEdgeEdges that can be measured by a eVision.ERectangleGauge
 CERectangleModeThe modes that specify how the selection of coded elements with a rectangle behaves
 CEReductionModeThe reduction mode to be used when learning a Consistent Edges model
 CEReferenceNoiseEnumeration for specifying how a reference image is affected by noise in EasyImage
 CERgbStandardAllowed values for the RGB standard in EasyColor
 CERoiHitDescribes the ROI that was hit by the mouse cursor
 CERotationRightAnglesClockwise Right angles for rotation
 CESegmentationMethodThe segmentation methods that are available to the image encoder
 CESegmentationModeAllowed values for the segmentation mode in EasyOCR
 CESelectionFlagSpecifies to which subset of a selection an operation should be applied in EasyObject and EasyOCV
 CESerializerFileWriterModeCreation mode of the file
 CESerializerModeThe mode of an eVision.ESerializer object
 CEShapeBehaviorAllowed values for conditions on the behavior of a shape
 CEShapeTypeShape type
 CEShiftingModeAllowed values for the shifting mode of EasyOCR
 CESingleThresholdModeThe single threshold mode for the selection of coded elements with respect to a given feature
 CESortDirectionThe sorting mode for selections of coded elements based on their features
 CESpotPolarityThe possible polarities of an eVision.ESpot
 CESpotTypeThe possible types of an eVision.ESpot
 CEStitchingAlgorithmAlgorithm used by the eVision.EImageStitcher
 CEStitchingGridStartingCornerDefines which corner of the grid is considered the starting corner for the traversal
 CEStitchingGridTraversalDefines how images are ordered (mapped) into a 2D grid when stitching in grid mode
 CESymbologiesThe symbologies supported by EasyBarCode
 CESymbolPolarityAllowed values for the polarity of a code
 CETextSizeConstraintModeDifferent modes to resize or modify texts before drawing them
 CEThinStructureModeAllowed values for the type of thin structures in EasyFind
 CEThresholdModeThe various modes for thresholding that are supported by eVision
 CEToneMapperTypeType of tone-mapper algorithm to use
 CETopologyFormatTypeFormat types supported for the specification of an eVision.ETopology
 CETrainingModeAllowed values for the training mode in EChecker
 CETransitionChoiceThe transition selection method applied by the gauge measurement
 CETransitionTypeThe type of transition to be retained by the gauge measurement
 CEVerbosityThe verbosity level of a Memento message
 CEWedgeGaugeEdgeEdges that can be measured by a eVision.EWedgeGauge
 CEExceptionThe exception type used in this library
 CAdvancedCalibrationParametersAdvanced calibration parameters
 CAdvancedDistortionParametersAdvanced distortion calibration parameters
 CEasyThis class contains static properties and methods specific to the eVision.Easy library
 CEasyColorThis class contains static properties and methods specific to the eVision.EasyColor library
 CEasyImageThis class contains static properties and methods specific to the eVision.EasyImage library
 CEasyObjectThis class contains static properties and methods specific to the eVision.EasyObject library
 CEBaseGaugeEasyGauge base class
 CEBaseROIThis represents the abstract base class for all ROI and image classes
 CEBW16PathVectorVector objects are used to store 1-dimensional data
 CEBW16VectorVector objects are used to store 1-dimensional data
 CEBW32VectorVector objects are used to store 1-dimensional data
 CEBW8PathVectorVector objects are used to store 1-dimensional data
 CEBW8VectorVector objects are used to store 1-dimensional data
 CEBWHistogramVectorVector objects are used to store 1-dimensional data
 CEC24PathVectorVector objects are used to store 1-dimensional data
 CEC24VectorVector objects are used to store 1-dimensional data
 CECallbackSerializerRemarks:
 CECameraCalibrationCamera calibration
 CECannyEdgeDetectorManages a complete context for the Canny edge detector
 CECheckerManages a complete context for the EChecker golden template inspection tool
 CECircleRepresents a model of a circle (or arc) in EasyGauge
 CECircleGaugeCircle gauge
 CECircleRegionManages a complete context for an eVision.ERegion shaped like a circle
 CECodeRepresents a Code
 CECodedElementThis class encapsulates either an object or a hole in an object, in a coded image
 CECodedImage2The main class of the EasyObject API that represents a coded image, as produced by the encoder
 CECodeGridRepresents a grid of Codes
 CECodeReaderAn eVision.ECodeReader instance can detect and decode various types of codes
 CEColorLookupDescribes a color lookup table, that is used to speed-up complex conversions between color systems
 CEColorVectorVector objects are used to store 1-dimensional data
 CEDebevecMergerParametersContainer holding the parameters for a Debevec merger algorithm
 CEDragoToneMapperParametersContainer holding the parameters for a Drago tone-mapper algorithm
 CEDrawableExtentDrawable surface extent
 CEDrawAdapterDraw adapter interface used for drawing eVision objects and results
 CEEllipseRepresents a model of an (arc of) ellipse
 CEEllipseRegionManages a complete context for an eVision.ERegion shaped like an ellipse
 CEFileSerializerA type of eVision.ESerializer suitable for serialization and deserialization to and from memory buffers
 CEFindFeaturePointRepresents a feature point obtained from learning a model using eVision.EPatternFinder
 CEFloatRangeRepresents a range of floating point values
 CEFontFont
 CEFoundPatternRepresents a single instance of the pattern in the search field, as returned by the EasyFind or EasyMatch finding process
 CEFourierImageThe eVision.EFourierImage class is used to represent rectangular regions of interest inside eVision.EBW32f gray-level images
 CEFourierTransformerUtility class to manage direct and inverse Fast Fourier Transforms
 CEFrameRepresents a geometrical frame of reference
 CEGDIPlusDrawAdapterDraw adapter using GDIPlus
 CEGenericDrawAdapterA type of draw adapter able to make rendering in images and yielding similar results on all platforms
 CEGridRepresents a rectangular grid, to be used by readers to read QRCodes, matrix codes, or bar codes
 CEGs1TranslatorAllows To retrieve human-readable GS1 code from machine-readable GS1 code
 CEHarrisCornerDetectorManages a complete context for the Harris corner detector
 CEHarrisInterestPointsContainer class for the results of the Harris corner detector
 CEHDRColorFuserA eVision.EHDRColorFuser.__init__ instance is a tool that flexibly fuses color images using HDR principles
 CEHDRFuserA eVision.EHDRFuser.__init__ instance is a tool that flexibly fuses grayscale images using HDR principles
 CEHDRFusionUtility class containing two configurable algorithms to display HDR images on standard display monitors while conserving details and visual quality of the input image
 CEHitAndMissKernelClass that defines a kernel for the morphological hit-and-miss operations
 CEImageBW16The eVision.EImageBW16 class is used to represent rectangular regions of interest inside eVision.EBW16 gray-level images
 CEImageBW32The eVision.EImageBW32 class is used to represent rectangular regions of interest inside eVision.EBW32 gray-level images
 CEImageBW32fThe eVision.EImageBW32f class is used to represent rectangular regions of interest inside eVision.EBW32f gray-level images
 CEImageBW8The eVision.EImageBW8 class is used to represent rectangular regions of interest inside eVision.EBW8 gray-level images
 CEImageC24The eVision.EImageC24 class is used to represent rectangular regions of interest inside eVision.EC24 color images
 CEImageC24AThe eVision.EImageC24A class is used to represent rectangular regions of interest inside eVision.EC24A color images
 CEImageC48The eVision.EImageC48 class is used to represent rectangular regions of interest inside eVision.EC48 color images
 CEImageEncoderThis class is responsible for the encoding of an image into an eVision.ECodedImage2 object
 CEImageStatisticsBW16Class storing the results of statistics computations on an eVision.EROIBW16
 CEImageStatisticsBW8Class storing the results of statistics computations on an eVision.EROIBW8
 CEImageStatisticsC24Class storing the results of statistics computations on an eVision.EROIC24
 CEImageStitcherStitch calibrated images together, forming a seamless panoramic image
 CEIntegerRangeRepresents a range of integer values
 CEKernelKernel for use in convolution operations
 CELandmarkThe landmark descriptor class
 CELineRepresents a model of a line segment
 CELinearToneMapperParametersContainer holding the parameters for a linear tone-mapper algorithm
 CELineGaugeLine gauge
 CEMailBarcodeManages a complete context for a Mail Barcode
 CEMailBarcodeReaderManages a complete context for a Mail Barcode Reader
 CEMantiukToneMapperParametersContainer holding the parameters for a Mantiuk tone-mapper algorithm
 CEMatcherManages a complete matching context in EasyMatch
 CEMatrixCodeHolds all the information regarding a single Data Matrix code: its decoded string, its grading, its errors,..
 CEMatrixCodeReaderA eVision.EMatrixCodeReader.__init__ instance is a tool that processes an ROI and returns a eVision.EMatrixCode instance
 CEMemorySerializerA type of eVision.ESerializer suitable for serialization and deserialization to and from memory buffers
 CEMergerParametersContainer holding the parameters for a merger algorithm
 CEMertensMergerParametersContainer holding the parameters for a Mertens merger algorithm
 CEMovingAverageTemporal integration of a number of images to reduce noise
 CEObjectRunsIteratorIterator to the runs of a coded element
 CEObjectSelectionThis container class handles the selection of a subset of coded elements taken from a coded image
 CEObjectTemplateMatcherThe EObjectTemplateMatcher class is a tool designed to align and match the output of EasyObject to a reference template
 CEOCRManages a complete context for the font-dependent printed character reader implemented in EasyOCR
 CEOCR2Manages a complete context for the font-dependent printed character reader implemented in EasyOCR2
 CEOCR2CharHolds all information related to a single detected character
 CEOCR2CharacterClusterHolds all information related to character cluster
 CEOCR2CharacterDatabaseHolds all information related to a character database
 CEOCR2DatabaseCharacterHolds all information related to a database character
 CEOCR2LineHolds a vector of eVision.EOCR2Word objects representing a line
 CEOCR2TextHolds a vector of eVision.EOCR2Line objects representing a text
 CEOCR2WordHolds a vector of eVision.EOCR2Char objects representing a word
 CEOCVManages a complete context for the optical character verification tool implemented in EasyOCV
 CEOCVCharHolds all information related to a single character, such as nominal and average position, reference quality indicators,... During the learning phases, it also keeps the list of its constituent blobs
 CEOCVTextHolds all information related to a single piece of text, such as nominal and average position, reference quality indicators,... It also keeps the list of its constituent characters
 CEPathVectorVector objects are used to store 1-dimensional data
 CEPatternFinderManages a complete finding context in EasyFind
 CEPeakVectorVector objects are used to store 1-dimensional data
 CEPixelViewBW16A class used to access the pixels of a ROI
 CEPixelViewBW32A class used to access the pixels of a ROI
 CEPixelViewBW8A class used to access the pixels of a ROI
 CEPixelViewC24A class used to access the pixels of a ROI
 CEPixelViewC24AA class used to access the pixels of a ROI
 CEPointGaugePoint gauge
 CEPointSetSet of points found by a eVision.EPointGauge
 CEPolygonRepresents a polygon
 CEPolygonGaugePolygon gauge
 CEPolygonRegionManages a complete context for an eVision.ERegion shaped like a polygon
 CEPseudoColorLookupDescribes a lookup table, that is used to for pseudo-coloring (i.e
 CEQRCodeRepresents a QR code found in the search field
 CEQRCodeDecodedStreamRepresents the complete decoded stream extracted from a QR code, eVision.EQRCode
 CEQRCodeDecodedStreamPartRepresents part of a decoded stream, eVision.EQRCodeDecodedStream, extracted from a QR code (eVision.EQRCode)
 CEQRCodeGeometryRepresents the geometry of a QR code
 CEQRCodeGridRepresents a grid of QR Codes
 CEQRCodeReaderRepresents the QR code reader, that is a context for the detection and decoding of QR codes, represented by eVision.EQRCode objects
 CERectangleRepresents a model of a rectangle
 CERectangleGaugeRectangle gauge
 CERectangleRegionManages a complete context for an eVision.ERegion shaped like a rectangle
 CERegionManages a complete context for a eVision.ERegion (Arbitrary Shaped ROI)
 CERegionFreeHandPainterManages a complete context for a eVision.ERegionFreeHandPainter
 CEReinhardToneMapperParametersContainer holding the parameters for a Reinhard tone-mapper algorithm
 CERobertsonMergerParametersContainer holding the parameters for a Robertson merger algorithm
 CEROIBW16The eVision.EROIBW16 class is used to represent rectangular regions of interest inside BW16 gray-level images
 CEROIBW32The eVision.EROIBW32 class is used to represent rectangular regions of interest inside BW32 gray-level images
 CEROIBW32fThe eVision.EROIBW32f class is used to represent rectangular regions of interest inside BW32f gray-level images
 CEROIBW8The eVision.EROIBW8 class is used to represent rectangular regions of interest inside BW8 gray-level images
 CEROIC24The eVision.EROIC24 class is used to represent rectangular regions of interest inside C24 color images
 CEROIC24AThe eVision.EROIC24A class is used to represent rectangular regions of interest inside C24A color images
 CEROIC48The eVision.EROIC48 class is used to represent rectangular regions of interest inside C48 color images
 CERotatedBoundingBoxThis class represents a rotated bounding box
 CESamplePathThe class represents a sample path (eVision.ELine on which we sample the pixel values to find the strong edge-crossings)
 CESamplePointA point sampled by a gauge
 CESearchParamsTypeThis class is instantiated once in each eVision.EMatrixCodeReader and represents the search parameters that are explored when reading a eVision.EMatrixCode
 CESerializerAbstract interface for file-like objects
 CESha1HasherObject for computing a SHA-1 hash
 CEShapeBase class for geometrical shapes
 CESpotThe eVision.ESpot store information about the detections produced by eVision.ESpotDetector
 CESpotDetectoreVision.ESpotDetector is dedicated to the detection of spots, particles and scratches on images
 CEStitchingGridOrderDefines the grid order when stitching in grid mode
 CEStringPairRepresent a Key/Value pair of strings
 CEToneMapperParametersContainer holding the parameters for a tone-mapper algorithm
 CETopologyeVision.ETopology aims to restrict the formats of the texts that will be returned by an eVision.EasyDeepOCR.ETextReader
 CETopologyLineeVision.ETopologyLine aims to restrict the formats of the textlines that will be returned by an eVision.EasyDeepOCR.ETextReader
 CEUnwarpingLutThis class is used only as a lookup table in the eVision.ECameraCalibration.Unwarp and eVision.ECameraCalibration.SetupUnwarp methods
 CEVectorBase class for all typed vectors
 CEVectorModelRepresents a eVision.Legacy.EShape hierarchy with a single root
 CEWedgeRepresents a model of a wedge (disk, ring, sector or curvilinear quadrilateral)
 CEWedgeGaugeWedge gauge
 CEWindowsDrawAdapterA draw adapter using the GDI+ native API on Windows
 CEBrushBrush
 CEBW16Gray-level pixel value, coded as an unsigned 16-bit integer
 CEBW16PathPath from a eVision.EBW16 image: image pixel coordinates, and associated gray-level pixel value
 CEBW32Gray-level pixel value, coded as an unsigned 32-bit integer
 CEBW32fGray-level pixel value, coded as a 32-bit floating-point number
 CEBW8Gray-level pixel value, coded as an unsigned 8-bit integer
 CEBW8PathPath from a eVision.EBW8 image: image pixel coordinates, and associated gray-level pixel value
 CEC24Color pixel value coded as 3 unsigned 8-bit integers (red, green and blue components)
 CEC24AColor pixel value coded as 4 unsigned 8-bit integers (red, green, blue and alpha components)
 CEC24PathPath from a eVision.EC24 image: image pixel coordinates, and associated color pixel value
 CEC48Color pixel value coded as 3 unsigned 16-bit integers (red, green, blue components)
 CECodeGridDrawOptionsList of options to customize the drawing of the codes
 CEColorTriple of floating-point numbers that encode a color in a given color system
 CEDepth16Depth value of the pixel, coded as an unsigned 16-bit integer
 CEDepth32fDepth value of the pixel, coded as a 32-bits floating point value
 CEDepth8Depth value of the pixel, coded as an unsigned 8-bit integer
 CEGridDrawOptionsList of options to customize the drawing of the grid
 CEGuardBandUsed to define a guard band around the processed ROI
 CEHistogramThresholdStructure containing the threshold of a histogram as well as the average value below/above the threshold
 CEIntPointEPoint whose coordinates are integers
 CEIntSizeSize composed of integer width and height
 CEISHIntensity, Saturation, Hue color system
 CELABCIE Lightness, a*, b* color system
 CELCHLightness, Chroma, Hue color system
 CELSHLightness, Saturation, Hue color system
 CELUVCIE Lightness, u*, v* color system
 CEMatchPositionRepresents a single instance of the pattern in the search field, as returned by the EasyMatch matching process
 CEMatrixCodeIso15415GradingParametersHolds all grading parameters pertaining to ISO/IEC 15415
 CEMatrixCodeIso29158CalibrationParametersHolds all grading inputs pertaining to ISO/IEC 29158
 CEMatrixCodeIso29158GradingParametersHolds all grading parameters pertaining to ISO/IEC 29158
 CEMatrixCodeSemiT10GradingParametersHolds all grading parameters pertaining to Semi T10-
 CEMatrixPositionRepresents a position in a 2D Matrix
 CEObjectBasicStatisticsBasic statistics about an object (area, gravity center, and first order moment of inertia)
 CEOCR2CharacterCandidateHolds a single recognition score for a detected character from the image
 CEParticleDetectionParametersUsed to store the particle detection parameters
 CEPathPath from an image: image pixel coordinates
 CEPeakRepresents a peak in a profile
 CEPenPen
 CEPlotDecorationOptionsOptions for drawing the decoration of a plot (axes, ticks, etc.)
 CEPointAn exact (floating-point) location in the 2D space
 CEQRCodeAdditionalParametersGradesHolds all grading inputs pertaining to ISO/IEC 29158
 CEQRCodeGridDrawOptionsList of options to customize the drawing of the QR codes
 CEQRCodeIso15415GradingParametersHolds all grading parameters pertaining to ISO/IEC 15415
 CEQRCodeIso29158CalibrationParametersHolds all grading inputs pertaining to ISO/IEC 29158
 CEQRCodeIso29158GradingParametersHolds all grading parameters pertaining to ISO/IEC 29158
 CEQuadrangleThis class represents a polygon with four corners (with sub-pixel accuracy)
 CERGBNTSC/PAL/SMPTE Red, Green, Blue color system
 CERGBColorNTSC/PAL/SMPTE Red, Green, Blue color system
 CERunGroup of pixels contiguous on a line
 CEScratchDetectionParametersUsed to store the scratch detection parameters
 CESizeSize composed of floating point width and height
 CETextSizeConstraintDetails how to resize or modify a text before drawing it
 CEThreeLevelsMinResidueThresholdStructure containing the min residue, its two corresponding thresholds as well as the average pixel below/above/between the thresholds
 CETwoLevelsMinResidueThresholdStructure containing the min residue, its corresponding threshold as well as the average pixel below/above the threshold
 CEVSHValue, Saturation, Hue color system
 CEXYZCIE XYZ color system
 CEYCbCrCCIR/ITU-R BT 601 Luma, U Chroma, V Chroma color system
 CEYIQCCIR Luma, Inphase, Quadrature color system
 CEYSHCCIR Luma, Saturation, Hue color system
 CEYUVPAL (CCIR/ITU-R BT 470-6) Luma, U Chroma, V Chroma color system