eVision Python API
Loading...
Searching...
No Matches
Class Hierarchy

Go to the graphical class hierarchy

This inheritance list is sorted roughly, but not completely, alphabetically:
 CeVision.AdvancedCalibrationParametersAdvanced calibration parameters
 CeVision.AdvancedDistortionParametersAdvanced distortion calibration parameters
 CeVision.Easy3D.E3DAlignerAligns an eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap on a reference eVision.Easy3D.EMesh, eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap
 CeVision.Easy3D.E3DMatcherAligns an eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap on and compares it with a reference eVision.Easy3D.EMesh, eVision.Easy3D.EPointCloud or eVision.Easy3D.EZMap
 CeVision.Easy3D.E3DAlignmentRepresents a 3D Alignment returned by eVision.Easy3D.E3DAligner
 CeVision.Easy3D.E3DMatchRepresents a 3D match returned by eVision.Easy3D.E3DMatcher
 CeVision.Easy3D.E3DAnomalyRepresents a detected 3D anomaly
 CeVision.Easy3D.E3DAxisDisplayRepresents the axis and the grid to display in the eVision.Easy3D.E3DViewer
 CeVision.Easy3D.E3DAxisSystemRepresent a 3D base axis system
 CeVision.Easy3D.E3DOrthonormalAxisSystemE3DOrthonormalAxisSystem is a subassembly of eVision.Easy3D.E3DAxisSystem with properties Orthogonal and Normed
 CeVision.Easy3D.E3DRightOrthonormalAxisSystemE3DRightOrthonormalAxisSystem is a subassembly of eVision.Easy3D.E3DAxisSystem with properties Orthogonal and Normed and Right
 CeVision.Easy3D.E3DBoxA 3D box, used as bounding volume for eVision.Easy3D.E3DObject class
 CeVision.Easy3D.E3DClosestPointStruct containing the eVision.Easy3D.E3DPoint of an eVision.Easy3D.EPointCloud that is closest to a line or segment with its index in the cloud and its distance to the line or segment
 CeVision.Easy3D.E3DComparerRepresents a 3D comparison context
 CeVision.Easy3D.E3DLineRepresents a 3D line
 CeVision.Easy3D.E3DObjectA eVision.Easy3D.E3DObject is a geometric description of a set of 3D points, produced by E3DObjectExtractor
 CeVision.Easy3D.E3DObjectExtractoreVision.Easy3D.E3DObjectExtractor is used to extract 3D objects from a ZMap
 CeVision.Easy3D.E3DPlaneRepresents a 3D plane
 CeVision.Easy3D.E3DPointRepresents a 3D point with floating point coordinates
 CeVision.Easy3D.E3DSphereRepresents a 3D sphere
 CeVision.Easy3D.E3DTransformMatrixRepresents a 3D transformation [4x4] matrix
 CeVision.Easy3D.E3DViewerManages a viewer window for eVision.Easy3D.EPointCloud
 CeVision.Easy3D.EAffineTransformerManages a 3D coordinates transformation context
 CeVision.Easy3D.EAnomalyThresholdsThresholds used to define an anomaly in Easy3DMatch
 CeVision.EasyThis class contains static properties and methods specific to the eVision.Easy library
 CeVision.EasyColorThis class contains static properties and methods specific to the eVision.EasyColor library
 CeVision.EasyImageThis class contains static properties and methods specific to the eVision.EasyImage library
 CeVision.EasyObjectThis class contains static properties and methods specific to the eVision.EasyObject library
 CeVision.Easy3D.EAzimuthElevationAnglesAzimuth and Elevation Angles
 CeVision.EasyBarCode2.EBarCodeRepresents a 1D Bar Code
 CeVision.EasyBarCode2.EBarCodeGradingParametersRepresents the grading Parameters associated with an eVision.EasyBarCode2.EBarCode as defined by ISO15416
 CeVision.EasyBarCode2.EBarCodeGridDrawOptionsList of options to customize the drawing of the bar codes
 CeVision.EasyBarCode2.EBarCodeReaderRepresents a 1D Bar Code Reading Context
 CeVision.EBaseGaugeEasyGauge base class
 CeVision.ECircleGaugeCircle gauge
 CeVision.ELineGaugeLine gauge
 CeVision.EPointGaugePoint gauge
 CeVision.EPolygonGaugePolygon gauge
 CeVision.ERectangleGaugeRectangle gauge
 CeVision.EWedgeGaugeWedge gauge
 CeVision.EBaseROIThis represents the abstract base class for all ROI and image classes
 CeVision.EROIBW16The eVision.EROIBW16 class is used to represent rectangular regions of interest inside BW16 gray-level images
 CeVision.EImageBW16The eVision.EImageBW16 class is used to represent rectangular regions of interest inside eVision.EBW16 gray-level images
 CeVision.EROIBW32The eVision.EROIBW32 class is used to represent rectangular regions of interest inside BW32 gray-level images
 CeVision.EImageBW32The eVision.EImageBW32 class is used to represent rectangular regions of interest inside eVision.EBW32 gray-level images
 CeVision.EROIBW32fThe eVision.EROIBW32f class is used to represent rectangular regions of interest inside BW32f gray-level images
 CeVision.EImageBW32fThe eVision.EImageBW32f class is used to represent rectangular regions of interest inside eVision.EBW32f gray-level images
 CeVision.EROIBW8The eVision.EROIBW8 class is used to represent rectangular regions of interest inside BW8 gray-level images
 CeVision.EImageBW8The eVision.EImageBW8 class is used to represent rectangular regions of interest inside eVision.EBW8 gray-level images
 CeVision.EROIC24The eVision.EROIC24 class is used to represent rectangular regions of interest inside C24 color images
 CeVision.EImageC24The eVision.EImageC24 class is used to represent rectangular regions of interest inside eVision.EC24 color images
 CeVision.EROIC24AThe eVision.EROIC24A class is used to represent rectangular regions of interest inside C24A color images
 CeVision.EImageC24AThe eVision.EImageC24A class is used to represent rectangular regions of interest inside eVision.EC24A color images
 CeVision.EROIC48The eVision.EROIC48 class is used to represent rectangular regions of interest inside C48 color images
 CeVision.EImageC48The eVision.EImageC48 class is used to represent rectangular regions of interest inside eVision.EC48 color images
 CeVision.EBrushBrush
 CeVision.EBW16Gray-level pixel value, coded as an unsigned 16-bit integer
 CeVision.EBW16PathPath from a eVision.EBW16 image: image pixel coordinates, and associated gray-level pixel value
 CeVision.EBW32Gray-level pixel value, coded as an unsigned 32-bit integer
 CeVision.EBW32fGray-level pixel value, coded as a 32-bit floating-point number
 CeVision.EBW8Gray-level pixel value, coded as an unsigned 8-bit integer
 CeVision.EBW8PathPath from a eVision.EBW8 image: image pixel coordinates, and associated gray-level pixel value
 CeVision.EC24Color pixel value coded as 3 unsigned 8-bit integers (red, green and blue components)
 CeVision.EC24AColor pixel value coded as 4 unsigned 8-bit integers (red, green, blue and alpha components)
 CeVision.EC24PathPath from a eVision.EC24 image: image pixel coordinates, and associated color pixel value
 CeVision.EC48Color pixel value coded as 3 unsigned 16-bit integers (red, green, blue components)
 CeVision.Easy3D.ECalibrationGeneratorRepresents a 3D calibration model generator, a class made to compute calibration models
 CeVision.Easy3D.EObjectBasedCalibrationGeneratorRepresents an object-based 3D calibration generator
 CeVision.Easy3D.ECalibrationModelRepresents a 3D calibration model
 CeVision.Easy3D.EExplicitGeometricCalibrationModeleVision.Easy3D.EExplicitGeometricCalibrationModel is used to calibrate a depth map from a minimal set of explicit geometric values
 CeVision.Easy3D.EObjectBasedCalibrationModeleVision.Easy3D.EObjectBasedCalibrationModel is an Easy3D calibration model built from a scan of a reference object
 CeVision.Easy3D.EScaleCalibrationModeleVision.Easy3D.EScaleCalibrationModel is used to convert depth map 2.5D point to 3D world position, only by applying a scale factor
 CeVision.ECameraCalibrationCamera calibration
 CeVision.ECannyEdgeDetectorManages a complete context for the Canny edge detector
 CeVision.ECheckerManages a complete context for the EChecker golden template inspection tool
 CeVision.Legacy.ECheckerManages a complete context for the inspection tool based on image comparison in EasyOCV
 CeVision.Legacy.EChecker2Manages a complete context for the EChecker2 golden template inspection tool
 CeVision.EasyDeepLearning.EClassificationMetricsCollection of metrics used to evaluate the state of an eVision.EasyDeepLearning.EClassifier
 CeVision.EasyDeepLearning.EClassificationResultAn eVision.EasyDeepLearning.EClassificationResult object represents the result of a classification
 CeVision.ECodeRepresents a Code
 CeVision.ECodedElementThis class encapsulates either an object or a hole in an object, in a coded image
 CeVision.ECodedImage2The main class of the EasyObject API that represents a coded image, as produced by the encoder
 CeVision.ECodeGridDrawOptionsList of options to customize the drawing of the codes
 CeVision.ECodeReaderAn eVision.ECodeReader instance can detect and decode various types of codes
 CeVision.EColorTriple of floating-point numbers that encode a color in a given color system
 CeVision.EColorLookupDescribes a color lookup table, that is used to speed-up complex conversions between color systems
 CeVision.Easy3D.EConverterConversion functions between bit depth formats of various 3D classes
 CeVision.EasyDeepLearning.EDataAugmentationAn eVision.EasyDeepLearning.EDataAugmentation object is responsible for storing the data augmentation parameters and generating new transformed images from existing ones
 CeVision.EasyDeepLearning.EDataseteVision.EasyDeepLearning.EDataset manages a dataset of images
 CeVision.EasyDeepLearning.EClassificationDataseteVision.EasyDeepLearning.EClassificationDataset manages a dataset of images
 CeVision.EasyDeepLearning.EDatasetSplitThe eVision.EasyDeepLearning.EDatasetSplit maps the image indexes of a eVision.EasyDeepLearning.EDataset to a dataset split type (eVision.EasyDeepLearning.EDatasetType)
 CeVision.Easy3D.EDecimatorDecimation of a point cloud/ZMap/DepthMap
 CeVision.Easy3D.EGridDecimatorDecimation of an eVision.Easy3D.EPointCloud
 CeVision.Easy3D.ERandomDecimatorDecimation of an eVision.Easy3D.EPointCloud
 CeVision.EasyDeepLearning.EDeepLearningBenchmarkDeep Learning benchmark results
 CeVision.EasyDeepLearning.EDeepLearningBenchmarkSettingsClass representing the settings of a Deep Learning benchmark
 CeVision.EasyDeepLearning.EDeepLearningDefectDetectionMetricsCollection of metrics used to evaluate a defect detection problem where the detection is based on the thresholding of a score produced by the underlying deep learning tool, e.g
 CeVision.EasyDeepLearning.ESupervisedSegmenterMetricsCollection of metrics used to evaluate the state of a eVision.EasyDeepLearning.ESupervisedSegmenter tool
 CeVision.EasyDeepLearning.EUnsupervisedSegmenterMetricsCollection of metrics used to evaluate the state of an eVision.EasyDeepLearning.EUnsupervisedSegmenter
 CeVision.EasyDeepLearning.EDeepLearningDeviceClass representing a device that can run a neural network
 CeVision.EasyDeepLearning.EDeepLearningExecutionSettingsExecution settings for a Deep Learning tool
 CeVision.EasyDeepLearning.EDeepLearningProjectDeep learning project
 CeVision.EasyDeepLearning.EDeepLearningTooleVision.EasyDeepLearning.EDeepLearningTool represents the common operations of deep learning tools
 CeVision.EasyDeepLearning.EClassifiereVision.EasyDeepLearning.EClassifier allows to train a classifier using an eVision.EasyDeepLearning.EDataset object and classify new images
 CeVision.EasyDeepLearning.EDeepOCRToolTrains the EasyDeepOCR Deep Learning models
 CeVision.EasyDeepLearning.ELocatorBaseBase class for EasyLocate tool
 CeVision.EasyDeepLearning.EInterestPointLocatorEasyLocate tool - interest point version
 CeVision.EasyDeepLearning.ELocatorEasyLocate tool - axis aligned bounding box version
 CeVision.EasyDeepLearning.ESupervisedSegmenterSupervised segmentation tool
 CeVision.EasyDeepLearning.EUnsupervisedSegmenterUnsupervised segmentation tool
 CeVision.EasyDeepLearning.EDeepOCRModelParametersBase class for the parameters of EasyDeepOCR models for user retraining
 CeVision.EasyDeepLearning.EDeepOCRModelParametersTextLocationParameters for the user retraining of the text location model of EasyDeepOCR
 CeVision.EasyDeepLearning.EDeepOCRToolMetricsMetrics for eVision.EasyDeepLearning.EDeepOCRTool
 CeVision.EasyDeepLearning.EDeepOCRToolResultResult for eVision.EasyDeepLearning.EDeepOCRTool
 CeVision.EDepth16Depth value of the pixel, coded as an unsigned 16-bit integer
 CeVision.EDepth32fDepth value of the pixel, coded as a 32-bits floating point value
 CeVision.EDepth8Depth value of the pixel, coded as an unsigned 8-bit integer
 CeVision.Easy3D.EDepthMapRepresents a generic DepthMap type interface
 CeVision.Easy3D.EDepthMap16Represents a eVision.Easy3D.EDepthMap with an 16-bit pixel internal representation
 CeVision.Easy3D.EDepthMap32fRepresents a eVision.Easy3D.EDepthMap with an 32-bit pixel internal representation
 CeVision.Easy3D.EDepthMap8Represents a eVision.Easy3D.EDepthMap with an internal 8-bit pixel representation
 CeVision.Easy3D.EDepthMapToMeshConverterPerforms the conversion from a eVision.Easy3D.EDepthMap to a eVision.Easy3D.EMesh, using the given calibration model
 CeVision.Easy3D.EDepthMapToPointCloudConverterPerforms the conversion from a eVision.Easy3D.EDepthMap to a eVision.Easy3D.EPointCloud, using the given calibration model
 CeVision.EDrawableExtentDrawable surface extent
 CeVision.EDrawAdapterDraw adapter interface used for drawing eVision objects and results
 CeVision.EGenericDrawAdapterA type of draw adapter able to make rendering in images and yielding similar results on all platforms
 CeVision.EWindowsDrawAdapterA draw adapter using the GDI+ native API on Windows
 CeVision.EGDIPlusDrawAdapterDraw adapter using GDIPlus
 CeVision.Easy3D.EEdgeCroppingParametersParameters used to defined edge cropping in Easy3DMatch
 CeVision.Easy3D.EErrorStatisticsThis object contains the error statistics (deviation between model and aligned points)
 CeVision.Easy3D.EFeaturesAlignerAlignment class, used to calculate the best transformation between matching pairs of points
 CeVision.Easy3D.EFiltersFiltering functions used to remove noise on 3D containers
 CeVision.EFindFeaturePointRepresents a feature point obtained from learning a model using eVision.EPatternFinder
 CeVision.EFloatRangeRepresents a range of floating point values
 CeVision.EFontFont
 CeVision.EFoundPatternRepresents a single instance of the pattern in the search field, as returned by the EasyFind or EasyMatch finding process
 CeVision.EFourierImageThe eVision.EFourierImage class is used to represent rectangular regions of interest inside eVision.EBW32f gray-level images
 CeVision.EFourierTransformerUtility class to manage direct and inverse Fast Fourier Transforms
 CeVision.EFrameRepresents a geometrical frame of reference
 CeVision.Legacy.EFrameRepresents a geometrical frame of reference as well as the parameters needed to transform from/to local and global coordinates
 CeVision.Legacy.ECircleRepresents a model of a circle (or arc) in EasyGauge
 CeVision.Legacy.ELineRepresents a model of a line segment
 CeVision.Legacy.EPolygonRepresents a polygon
 CeVision.Legacy.ERectangleRepresents a model of a rectangle
 CeVision.Legacy.EWedgeRepresents a model of a wedge (disk, ring, sector or curvilinear quadrilateral)
 CeVision.EGridRepresents a rectangular grid, to be used by readers to read QRCodes, matrix codes, or bar codes
 CeVision.ECodeGridRepresents a grid of Codes
 CeVision.EQRCodeGridRepresents a grid of QR Codes
 CeVision.EasyBarCode2.EBarCodeGridRepresents a grid of Data Barcodes
 CeVision.EasyMatrixCode2.EMatrixCodeGridRepresents a grid of Data Matrix Codes
 CeVision.EGridDrawOptionsList of options to customize the drawing of the grid
 CeVision.EGs1TranslatorAllows To retrieve human-readable GS1 code from machine-readable GS1 code
 CeVision.EGuardBandUsed to define a guard band around the processed ROI
 CeVision.EHarrisCornerDetectorManages a complete context for the Harris corner detector
 CeVision.EHarrisInterestPointsContainer class for the results of the Harris corner detector
 CeVision.EHDRColorFuserA eVision.EHDRColorFuser.__init__ instance is a tool that flexibly fuses color images using HDR principles
 CeVision.EHDRFuserA eVision.EHDRFuser.__init__ instance is a tool that flexibly fuses grayscale images using HDR principles
 CeVision.EHDRFusionUtility class containing two configurable algorithms to display HDR images on standard display monitors while conserving details and visual quality of the input image
 CeVision.EHistogramThresholdStructure containing the threshold of a histogram as well as the average value below/above the threshold
 CeVision.EHitAndMissKernelClass that defines a kernel for the morphological hit-and-miss operations
 CeVision.EImageEncoderThis class is responsible for the encoding of an image into an eVision.ECodedImage2 object
 CeVision.Segmenters.EImageSegmenterBase class from which all the segmenters derive
 CeVision.Segmenters.ELabeledImageSegmenterSegments an image by mapping the value of the pixels directly to a layer index
 CeVision.Segmenters.EThreeLayersImageSegmenterThe base class from which all the segmenters that produce three layers derive
 CeVision.Segmenters.EGrayscaleDoubleThresholdSegmenterSegments an image using a double threshold on a grayscale image
 CeVision.Segmenters.ETwoLayersImageSegmenterThe base class from which all the segmenters that produce two layers derive
 CeVision.Segmenters.EColorRangeThresholdSegmenterSegments an image using a double threshold on a color image
 CeVision.Segmenters.EColorSingleThresholdSegmenterSegments an image using a single threshold on a color image
 CeVision.Segmenters.EGrayscaleSingleThresholdSegmenterSegments an image using a single threshold on a grayscale image
 CeVision.Segmenters.EImageRangeSegmenterSegments an image using a pixel-by-pixel double threshold given as two images
 CeVision.Segmenters.EReferenceImageSegmenterSegments an image using a pixel-by-pixel single threshold given as an image
 CeVision.EImageStatisticsBW16Class storing the results of statistics computations on an eVision.EROIBW16
 CeVision.EImageStatisticsBW8Class storing the results of statistics computations on an eVision.EROIBW8
 CeVision.EImageStatisticsC24Class storing the results of statistics computations on an eVision.EROIC24
 CeVision.EImageStitcherStitch calibrated images together, forming a seamless panoramic image
 CeVision.EIntegerRangeRepresents a range of integer values
 CeVision.EIntPointEPoint whose coordinates are integers
 CeVision.EIntSizeSize composed of integer width and height
 CeVision.EISHIntensity, Saturation, Hue color system
 CeVision.EKernelKernel for use in convolution operations
 CeVision.ELABCIE Lightness, a*, b* color system
 CeVision.ELandmarkThe landmark descriptor class
 CeVision.Easy3D.ELaserLineExtractorManages a laser line extraction context
 CeVision.ELCHLightness, Chroma, Hue color system
 CeVision.EasyDeepLearning.ELocatorMetricsCollection of metrics used to evaluate the results of a eVision.EasyDeepLearning.ELocator tool
 CeVision.EasyDeepLearning.ELocatorMetricsGeneratorLocator metric generator
 CeVision.EasyDeepLearning.ELocatorObjectObject for a eVision.EasyDeepLearning.ELocator tool
 CeVision.EasyDeepLearning.ELocatorPredictedObjectObject predicted by a eVision.EasyDeepLearning.ELocator tool
 CeVision.EasyDeepLearning.ELocatorResultResult of a eVision.EasyDeepLearning.ELocator tool
 CeVision.ELSHLightness, Saturation, Hue color system
 CeVision.ELUVCIE Lightness, u*, v* color system
 CeVision.EMailBarcodeManages a complete context for a Mail Barcode
 CeVision.EMailBarcodeReaderManages a complete context for a Mail Barcode Reader
 CeVision.EMatcherManages a complete matching context in EasyMatch
 CeVision.EMatchPositionRepresents a single instance of the pattern in the search field, as returned by the EasyMatch matching process
 CeVision.EasyMatrixCode2.EMatrixCodeHolds all the information regarding a single Data Matrix code: its decoded string, its grading, its errors and more
 CeVision.EMatrixCodeHolds all the information regarding a single Data Matrix code: its decoded string, its grading, its errors,..
 CeVision.EasyMatrixCode2.EMatrixCodeGridDrawOptionsList of options to customize the drawing of the matrix codes
 CeVision.EMatrixCodeIso15415GradingParametersHolds all grading parameters pertaining to ISO/IEC 15415
 CeVision.EMatrixCodeIso29158CalibrationParametersHolds all grading inputs pertaining to ISO/IEC 29158
 CeVision.EMatrixCodeIso29158GradingParametersHolds all grading parameters pertaining to ISO/IEC 29158
 CeVision.EasyMatrixCode2.EMatrixCodeReaderAn eVision.EasyMatrixCode2.EMatrixCodeReader instance can detect, decode and grade matrixcodes in an ROI, it returns a vector of eVision.EasyMatrixCode2.EMatrixCode instances
 CeVision.EMatrixCodeReaderA eVision.EMatrixCodeReader.__init__ instance is a tool that processes an ROI and returns a eVision.EMatrixCode instance
 CeVision.EMatrixCodeSemiT10GradingParametersHolds all grading parameters pertaining to Semi T10-
 CeVision.EMatrixPositionRepresents a position in a 2D Matrix
 CeVision.EMergerParametersContainer holding the parameters for a merger algorithm
 CeVision.EDebevecMergerParametersContainer holding the parameters for a Debevec merger algorithm
 CeVision.EMertensMergerParametersContainer holding the parameters for a Mertens merger algorithm
 CeVision.ERobertsonMergerParametersContainer holding the parameters for a Robertson merger algorithm
 CeVision.Easy3D.EMeshRepresents a 3D meshed object
 CeVision.Easy3D.EMeshToZMapConverterComputes an eVision.Easy3D.EZMap from an eVision.Easy3D.EMesh
 CeVision.EMovingAverageTemporal integration of a number of images to reduce noise
 CeVision.EObjectBasicStatisticsBasic statistics about an object (area, gravity center, and first order moment of inertia)
 CeVision.EObjectRunsIteratorIterator to the runs of a coded element
 CeVision.EObjectSelectionThis container class handles the selection of a subset of coded elements taken from a coded image
 CeVision.EObjectTemplateMatcherThe EObjectTemplateMatcher class is a tool designed to align and match the output of EasyObject to a reference template
 CeVision.EOCRManages a complete context for the font-dependent printed character reader implemented in EasyOCR
 CeVision.EOCR2Manages a complete context for the font-dependent printed character reader implemented in EasyOCR2
 CeVision.EOCR2CharHolds all information related to a single detected character
 CeVision.EOCR2CharacterCandidateHolds a single recognition score for a detected character from the image
 CeVision.EOCR2CharacterClusterHolds all information related to character cluster
 CeVision.EOCR2CharacterDatabaseHolds all information related to a character database
 CeVision.EOCR2DatabaseCharacterHolds all information related to a database character
 CeVision.EOCR2LineHolds a vector of eVision.EOCR2Word objects representing a line
 CeVision.EOCR2TextHolds a vector of eVision.EOCR2Line objects representing a text
 CeVision.EOCR2WordHolds a vector of eVision.EOCR2Char objects representing a word
 CeVision.EOCVManages a complete context for the optical character verification tool implemented in EasyOCV
 CeVision.EOCVCharHolds all information related to a single character, such as nominal and average position, reference quality indicators,... During the learning phases, it also keeps the list of its constituent blobs
 CeVision.EOCVTextHolds all information related to a single piece of text, such as nominal and average position, reference quality indicators,... It also keeps the list of its constituent characters
 CeVision.EasyDeepOCR.EOptimizationReportAn eVision.EasyDeepOCR.EOptimizationReport stores information about the optimization of an eVision.EasyDeepOCR.ETextReader (eVision.EasyDeepOCR.ETextReader.Optimize)
 CeVision.EParticleDetectionParametersUsed to store the particle detection parameters
 CeVision.EPathPath from an image: image pixel coordinates
 CeVision.EPatternFinderManages a complete finding context in EasyFind
 CeVision.EPeakRepresents a peak in a profile
 CeVision.EPenPen
 CeVision.Easy3D.EPhotometricStereoImagerManages photometric stereo reconstruction
 CeVision.EPixelViewBW16A class used to access the pixels of a ROI
 CeVision.EPixelViewBW32A class used to access the pixels of a ROI
 CeVision.EPixelViewBW8A class used to access the pixels of a ROI
 CeVision.EPixelViewC24A class used to access the pixels of a ROI
 CeVision.EPixelViewC24AA class used to access the pixels of a ROI
 CeVision.Easy3D.EPlaneCropperA eVision.Easy3D.EPlaneCropper object is used to crop some points of a eVision.Easy3D.EPointCloud object
 CeVision.Easy3D.EPlaneFinderA eVision.Easy3D.EPlaneFinder object is used to search an eVision.Easy3D.E3DPlane in an eVision.Easy3D.EPointCloud
 CeVision.Easy3D.EPlaneFitterA eVision.Easy3D.EPlaneFitter object is used to fit an eVision.Easy3D.E3DPlane on an eVision.Easy3D.EPointCloud
 CeVision.EPlotDecorationOptionsOptions for drawing the decoration of a plot (axes, ticks, etc.)
 CeVision.EPointAn exact (floating-point) location in the 2D space
 CeVision.Easy3D.EPointCloudRepresents a 3D point cloud
 CeVision.Easy3D.EPointCloudFactoryManages a context for creating point clouds of specific shapes
 CeVision.Easy3D.EPointCloudFilterAn eVision.Easy3D.EPointCloudFilter is used to filter some points out of an eVision.Easy3D.EPointCloud
 CeVision.Easy3D.EPointCloudMergerMerges several eVision.Easy3D.EPointCloud of the same scene from different sensors after having performed a calibration
 CeVision.Easy3D.EPointCloudStatisticsManages a context for retrieving statistics on an eVision.Easy3D.EPointCloud
 CeVision.Easy3D.EPointCloudToMeshConverterPerforms the conversion from an eVision.Easy3D.EPointCloud to an eVision.Easy3D.EMesh
 CeVision.Easy3D.EPointCloudToZMapConverterComputes an eVision.Easy3D.EZMap from an eVision.Easy3D.EPointCloud
 CeVision.Easy3D.EPrincipalAxisExtractorA eVision.Easy3D.EPrincipalAxisExtractor object computes the principal axis analysis (PCA) on an eVision.Easy3D.EPointCloud and produces a eVision.Easy3D.E3DTransformMatrix as a result
 CeVision.EPseudoColorLookupDescribes a lookup table, that is used to for pseudo-coloring (i.e
 CeVision.EQRCodeRepresents a QR code found in the search field
 CeVision.EQRCodeAdditionalParametersGradesHolds all grading inputs pertaining to ISO/IEC 29158
 CeVision.EQRCodeDecodedStreamRepresents the complete decoded stream extracted from a QR code, eVision.EQRCode
 CeVision.EQRCodeDecodedStreamPartRepresents part of a decoded stream, eVision.EQRCodeDecodedStream, extracted from a QR code (eVision.EQRCode)
 CeVision.EQRCodeGeometryRepresents the geometry of a QR code
 CeVision.EQRCodeGridDrawOptionsList of options to customize the drawing of the QR codes
 CeVision.EQRCodeIso15415GradingParametersHolds all grading parameters pertaining to ISO/IEC 15415
 CeVision.EQRCodeIso29158CalibrationParametersHolds all grading inputs pertaining to ISO/IEC 29158
 CeVision.EQRCodeIso29158GradingParametersHolds all grading parameters pertaining to ISO/IEC 29158
 CeVision.EQRCodeReaderRepresents the QR code reader, that is a context for the detection and decoding of QR codes, represented by eVision.EQRCode objects
 CeVision.EQuadrangleThis class represents a polygon with four corners (with sub-pixel accuracy)
 CeVision.Easy3D.ERectangularCropperManages a point cloud cropper in the shape of a rectangular parallelepiped
 CeVision.ERegionManages a complete context for a eVision.ERegion (Arbitrary Shaped ROI)
 CeVision.ECircleRegionManages a complete context for an eVision.ERegion shaped like a circle
 CeVision.EEllipseRegionManages a complete context for an eVision.ERegion shaped like an ellipse
 CeVision.EPolygonRegionManages a complete context for an eVision.ERegion shaped like a polygon
 CeVision.ERectangleRegionManages a complete context for an eVision.ERegion shaped like a rectangle
 CeVision.ERegionFreeHandPainterManages a complete context for a eVision.ERegionFreeHandPainter
 CeVision.Easy3D.ERenderStyleRepresents how to visualize 3D Objects in a E3DViewer
 CeVision.ERGBNTSC/PAL/SMPTE Red, Green, Blue color system
 CeVision.ERGBColorNTSC/PAL/SMPTE Red, Green, Blue color system
 CeVision.EasyDeepLearning.EROCPointThe structure representing a point on the ROC (Receiver Operating Characteristic) curve
 CeVision.ERotatedBoundingBoxThis class represents a rotated bounding box
 CeVision.ERunGroup of pixels contiguous on a line
 CeVision.EasyDeepOCR.ESampleA sample is composed of an image, and optionally a region, together with one or several texts, which are visible in the image
 CeVision.EasyDeepOCR.ESampleListHolds a list of samples
 CeVision.ESamplePathThe class represents a sample path (eVision.ELine on which we sample the pixel values to find the strong edge-crossings)
 CeVision.ESamplePointA point sampled by a gauge
 CeVision.Legacy.ESamplePointA point sampled by a gauge
 CeVision.EScratchDetectionParametersUsed to store the scratch detection parameters
 CeVision.ESearchParamsTypeThis class is instantiated once in each eVision.EMatrixCodeReader and represents the search parameters that are explored when reading a eVision.EMatrixCode
 CeVision.ESerializerAbstract interface for file-like objects
 CeVision.ECallbackSerializerRemarks:
 CeVision.EFileSerializerA type of eVision.ESerializer suitable for serialization and deserialization to and from memory buffers
 CeVision.EMemorySerializerA type of eVision.ESerializer suitable for serialization and deserialization to and from memory buffers
 CeVision.ESha1HasherObject for computing a SHA-1 hash
 CeVision.EShapeBase class for geometrical shapes
 CeVision.ECircleRepresents a model of a circle (or arc) in EasyGauge
 CeVision.EEllipseRepresents a model of an (arc of) ellipse
 CeVision.ELineRepresents a model of a line segment
 CeVision.EPointSetSet of points found by a eVision.EPointGauge
 CeVision.EPolygonRepresents a polygon
 CeVision.ERectangleRepresents a model of a rectangle
 CeVision.EWedgeRepresents a model of a wedge (disk, ring, sector or curvilinear quadrilateral)
 CeVision.Legacy.EShapeAbstract class to federate the classes that can be hierarchically attached together (from a geometrical point of view)
 CeVision.Legacy.ECircleShapeManages a circle shape
 CeVision.Legacy.ECircleGaugeManages a circle fitting gauge
 CeVision.Legacy.EFrameShapeManages a complete context for measuring frame shapes
 CeVision.Legacy.ELineShapeManages a line shape
 CeVision.Legacy.ELineGaugeManages a line fitting gauge
 CeVision.Legacy.EPointShapeManages a point shape context
 CeVision.Legacy.EPointGaugeManages a point location gauge
 CeVision.Legacy.EPolygonShapeManages a polygonal shape
 CeVision.Legacy.EPolygonGaugeManages a polygon fitting gauge
 CeVision.Legacy.ERectangleShapeManages a rectangle shape
 CeVision.Legacy.ERectangleGaugeManages a rectangle fitting gauge
 CeVision.Legacy.EWedgeShapeManages a wedge shape
 CeVision.Legacy.EWedgeGaugeManages a wedge fitting gauge
 CeVision.Legacy.EWorldShapeManages a complete context for calibrating a field of view
 CeVision.Easy3D.ESimpleCropperManages a point cloud cropper based on X/Y/Z value ranges
 CeVision.ESizeSize composed of floating point width and height
 CeVision.Easy3D.ESphereFitterA eVision.Easy3D.ESphereFitter object is used to fit an eVision.Easy3D.E3DSphere on an eVision.Easy3D.EPointCloud
 CeVision.Easy3D.ESphericalCropperManages a spherical point cloud cropper
 CeVision.ESpotThe eVision.ESpot store information about the detections produced by eVision.ESpotDetector
 CeVision.ESpotDetectoreVision.ESpotDetector is dedicated to the detection of spots, particles and scratches on images
 CeVision.Easy3D.EStatisticsCalculates various statistics on the pixels values of an eVision.Easy3D.EDepthMap or eVision.Easy3D.EZMap
 CeVision.Easy3D.EStatistics16Statistics on the pixels values of an eVision.Easy3D.EDepthMap16 or eVision.Easy3D.EZMap16 computed by eVision.Easy3D.EStatistics
 CeVision.Easy3D.EStatistics32fStatistics on the pixels values of an eVision.Easy3D.EDepthMap or eVision.Easy3D.EZMap computed by eVision.Easy3D.EStatistics
 CeVision.Easy3D.EStatistics8Statistics on the pixels values of an eVision.Easy3D.EDepthMap8 or eVision.Easy3D.EZMap8 computed by eVision.Easy3D.EStatistics
 CeVision.EStitchingGridOrderDefines the grid order when stitching in grid mode
 CeVision.EStringPairRepresent a Key/Value pair of strings
 CeVision.EasyDeepLearning.ESupervisedSegmenterBlobA blob detected by a supervised segmentation tool (see eVision.EasyDeepLearning.ESupervisedSegmenter and eVision.EasyDeepLearning.ESupervisedSegmenterResult)
 CeVision.EasyDeepLearning.ESupervisedSegmenterResultAn eVision.EasyDeepLearning.ESupervisedSegmenterResult object represents the result of a supervised segmenter
 CeVision.EasyDeepOCR.ETextRepresents a text detected by a eVision.EasyDeepOCR.ETextReader
 CeVision.EasyDeepOCR.ETextDrawingParametersRepresents the drawing parameters needed by eVision.EasyDeepOCR.ETextLine.Draw and eVision.EasyDeepOCR.EText.Draw
 CeVision.EasyDeepOCR.ETextLineRepresents a text line detected by a eVision.EasyDeepOCR.ETextReader
 CeVision.EasyDeepOCR.ETextReaderA eVision.EasyDeepOCR.ETextReader aims to find and read texts inside a given ROI, through eVision.EasyDeepOCR.ETextReader.Read
 CeVision.ETextSizeConstraintDetails how to resize or modify a text before drawing it
 CeVision.EThreeLevelsMinResidueThresholdStructure containing the min residue, its two corresponding thresholds as well as the average pixel below/above/between the thresholds
 CeVision.EToneMapperParametersContainer holding the parameters for a tone-mapper algorithm
 CeVision.EDragoToneMapperParametersContainer holding the parameters for a Drago tone-mapper algorithm
 CeVision.ELinearToneMapperParametersContainer holding the parameters for a linear tone-mapper algorithm
 CeVision.EMantiukToneMapperParametersContainer holding the parameters for a Mantiuk tone-mapper algorithm
 CeVision.EReinhardToneMapperParametersContainer holding the parameters for a Reinhard tone-mapper algorithm
 CeVision.ETopologyeVision.ETopology aims to restrict the formats of the texts that will be returned by an eVision.EasyDeepOCR.ETextReader
 CeVision.ETopologyLineeVision.ETopologyLine aims to restrict the formats of the textlines that will be returned by an eVision.EasyDeepOCR.ETextReader
 CeVision.ETwoLevelsMinResidueThresholdStructure containing the min residue, its corresponding threshold as well as the average pixel below/above the threshold
 CeVision.EasyDeepLearning.EUnsupervisedSegmenterResultAn eVision.EasyDeepLearning.EUnsupervisedSegmenterResult object represents the result of a eVision.EasyDeepLearning.EUnsupervisedSegmenter tool
 CeVision.EUnwarpingLutThis class is used only as a lookup table in the eVision.ECameraCalibration.Unwarp and eVision.ECameraCalibration.SetupUnwarp methods
 CeVision.Easy3D.EUtils3D Utilitarian Functions
 CeVision.EVectorBase class for all typed vectors
 CeVision.EBW16PathVectorVector objects are used to store 1-dimensional data
 CeVision.EBW16VectorVector objects are used to store 1-dimensional data
 CeVision.EBW32VectorVector objects are used to store 1-dimensional data
 CeVision.EBW8PathVectorVector objects are used to store 1-dimensional data
 CeVision.EBW8VectorVector objects are used to store 1-dimensional data
 CeVision.EBWHistogramVectorVector objects are used to store 1-dimensional data
 CeVision.EC24PathVectorVector objects are used to store 1-dimensional data
 CeVision.EC24VectorVector objects are used to store 1-dimensional data
 CeVision.EColorVectorVector objects are used to store 1-dimensional data
 CeVision.EPathVectorVector objects are used to store 1-dimensional data
 CeVision.EPeakVectorVector objects are used to store 1-dimensional data
 CeVision.EVectorModelRepresents a eVision.Legacy.EShape hierarchy with a single root
 CeVision.EVSHValue, Saturation, Hue color system
 CeVision.EasyDeepLearning.EWeightedPrecisionRecallPointWeighted precision and recall for a given threshold
 CException
 CeVision.EExceptionThe exception type used in this library
 CeVision.EXYZCIE XYZ color system
 CeVision.EYCbCrCCIR/ITU-R BT 601 Luma, U Chroma, V Chroma color system
 CeVision.EYIQCCIR Luma, Inphase, Quadrature color system
 CeVision.EYSHCCIR Luma, Saturation, Hue color system
 CeVision.EYUVPAL (CCIR/ITU-R BT 470-6) Luma, U Chroma, V Chroma color system
 CeVision.Easy3D.EZMapRepresents a generic ZMap type interface
 CeVision.Easy3D.EZMap16A ZMap16 is a 16bits corrected 2.5D image
 CeVision.Easy3D.EZMap32fA ZMap32f is a 32bits corrected 2.5D image
 CeVision.Easy3D.EZMap8A ZMap8 is a 8bits corrected 2.5D image
 CeVision.Easy3D.EZMapLevelerClass performing the leveling of an eVision.Easy3D.EZMap
 CeVision.Easy3D.EZMapToMeshConverterPerforms the conversion from an eVision.Easy3D.EZMap to an eVision.Easy3D.EMesh
 CeVision.Easy3D.EZMapToPointCloudConverterGenerates an eVision.Easy3D.EPointCloud from a ZMap
 Cenum.IntFlag
 CeVision.EAdaptiveThresholdMethodAdaptive thresholding modes
 CeVision.EAngleUnitThe angle units that are supported by eVision
 CeVision.EArithmeticLogicOperationSupported arithmetic or logic pixel-wise operators
 CeVision.EBayerConfigurationThe Bayer image color configuration of the first two pixels
 CeVision.EByteInterpretationModeThis enumeration contains the available modes to interpret bytes values of a decoded string
 CeVision.ECalibrationModeAllowed values for the calibration mode
 CeVision.ECannyThresholdingModeThe thresholding modes for the Canny edge detector
 CeVision.ECellColorAllowed values for a cell color (Black or White)
 CeVision.ECharCreationModeAllowed values for the character creation mode in EasyOCV
 CeVision.EClippingModeAllows to choose how the fitted segment length and centre are computed
 CeVision.ECodeTypeRepresents a type of Code
 CeVision.EColorQuantizationAllowed values for the quantization mode in EasyColor
 CeVision.EColorSystemThe color systems that are supported by eVision
 CeVision.EConnexityPossible values for the connexity of a contour
 CeVision.EContourModePossible modes for contour traversal
 CeVision.EContourThresholdAllowed thresholding modes for contour traversal
 CeVision.ECorrelationModeAllowed values for the EasyMatch correlation mode
 CeVision.EDataSizePossible data sizes for an object feature
 CeVision.EDataTypePossible data types for an object feature
 CeVision.EDegreesOfFreedomAllowed values for the degrees of freedom in eVision.EChecker
 CeVision.EDiagnosticPossible defect codes in EasyOCV
 CeVision.EDongleTypeDongle types
 CeVision.EDoubleThresholdModeThe double threshold mode for the selection of coded elements with respect to a given feature
 CeVision.EDragHandleAllowed values for a handle identifier in the context of handle dragging
 CeVision.EDraggingModeDefines how the shape could be dragged
 CeVision.EDrawRegionEnum specifying how to draw the eVision.ERegion that may be associated with an eVision.EFoundPattern
 CeVision.EDrawableFeatureThe various features that can be drawn for coded elements
 CeVision.EDrawingModeAllowed modes to draw the bounding box of a symbol
 CeVision.EEditionModeThis enumeration is used to select which graphical interactions are allowed
 CeVision.EEncodingConnexityThe connexity mode for the encoding process
 CeVision.EErrorPossible eVision error codes
 CeVision.EFamilyAllowed values for the ECC symbol family in EasyMatrixCode
 CeVision.EFeatureThe various features that can be measured on the coded elements of a selection
 CeVision.EFilteringModeAllowed values for the filtering mode of EasyMatch
 CeVision.EFindContrastModeAllowed values for the contrast mode of EasyFind
 CeVision.EFlipAxisAxis for flipping
 CeVision.EFlippingAllowed values for the symbol flipping type in EasyMatrixCode
 CeVision.EFontStyleFont style
 CeVision.EFramePositionThis enumeration contains the possible values for the placement of the overlay frame edges that are drawn to highlight the position of an ROI
 CeVision.EFrameScalingScaling used to construct an eVision.EFrame from other objects
 CeVision.EFrequentialDomainFormatThis enumeration represents the supported data formats for frequential domain images
 CeVision.EGrayscaleSingleThresholdThe modes that are available to segment a grayscale image using a single threshold
 CeVision.EHarrisThresholdingModeThe thresholding modes for the Harris corner detector
 CeVision.EHistogramFeatureThe various parameters that can be extracted from a histogram
 CeVision.EHitAndMissValueThe allowed values for the elements of a hit-and-miss kernel
 CeVision.EImageFileTypeEnum representing the file types supported by eVision
 CeVision.EImageTypeImage type
 CeVision.EInterpolationModeEstimation function to apply when resizing an image
 CeVision.EKernelRectifierPossible values for the rectification mode of a kernel
 CeVision.EKernelRotationPossible values for rotating a convolution kernel
 CeVision.EKernelTypeThe types of convolution kernels that are supported by eVision
 CeVision.ELearnParamAllowed values for the kind of parameters that can be learnt by EasyMatrixCode
 CeVision.ELearningModeAllowed values for the learning mode in EasyOCV
 CeVision.ELegacyFeatureThe various parameters that can be extracted from a histogram
 CeVision.ELineSpacingModeAllowed values for the line spacing mode of EasyOCR
 CeVision.ELocalSearchModeAllowed values for the local search mode of EasyFind
 CeVision.ELocationModeAllowed values for the kind of pre-processing to be applied to the sample image in EasyOCV
 CeVision.ELogicalSizeAllowed values for the logical size of Data Matrix codes in EasyMatrixCode
 CeVision.EMailBarcodeOrientationThe orientations supported by EMailBarcode
 CeVision.EMailBarcodeSymbologiesThe symbologies supported by EMailBarcode
 CeVision.EMatchContrastModeAllowed values for the contrast mode of EasyMatch
 CeVision.EMatchingModeAllowed values for the matching mode of EasyOCR
 CeVision.EMatrixCodeContrastModeEnum representing the contrast mode of an EMatrixCode
 CeVision.EMergerTypeType of merger algorithm to use
 CeVision.ENormalizationModeAllowed values for the gray-level normalization mode in EChecker and EasyOCV
 CeVision.EOCR2ClassifierThis enumeration contains the different types of classifier for character recognition in eVision.EOCR2
 CeVision.EOCR2DetectionMethodThis enumeration contains the possible methods for text detection in eVision.EOCR2
 CeVision.EOCR2SegmentationMethodThis enumeration contains the possible methods for image segmentation in eVision.EOCR2
 CeVision.EOCRClassAllowed values for the class of pattern in EasyOCR
 CeVision.EOCRColorAllowed values for the text color in EasyOCR
 CeVision.EObjectTemplateMatcherAlignmentThe type of alignment perform by eVision.EObjectTemplateMatcher priori to matching the objects
 CeVision.EPathVectorDrawOptionEnum representing the drawing options of an eVision.EPathVector
 CeVision.EPatternStyleAllowed values for the nature of the pattern in EasyFind
 CeVision.EPatternTypeAllowed values for the type of patterns in EasyFind
 CeVision.EPenStylePen style
 CeVision.EPlotItemDefines how the profile is drawed across a gauge
 CeVision.EPolygonMeasurementModePolygonGauge measurement mode
 CeVision.EQRCodeCodingModeThis enumeration contains the possible values for the coding mode of a QR code
 CeVision.EQRCodeEncodingThis enumeration contains the possible values for the encoding used for parts of the bit stream of a QR code, contained by the eVision.EQRCodeDecodedStreamPart object
 CeVision.EQRCodeLevelThis enumeration contains the possible values for the level of error correction of a QR code
 CeVision.EQRCodeModelThis enumeration contains the possible values for a QR code model
 CeVision.EQRCodePerspectiveModeThis enumeration contains the possible values for the scanning precision of an eVision.EQRCodeReader object
 CeVision.EQRCodeScanPrecisionThis enumeration contains the possible values for the scanning precision used by an eVision.EQRCodeReader object
 CeVision.EQRDetectionMethodThis enumeration contains the possible detection methods the eVision.EQRCodeReader can use to detect QR codes
 CeVision.EQRDetectionTradeOffThis enumeration contains several settings for the trade-off between detection speed and reliability of the EasyQRCode methods
 CeVision.EQualityIndicatorAllowed values for the quality indicators in EasyOCV
 CeVision.ERectangleGaugeEdgeEdges that can be measured by a eVision.ERectangleGauge
 CeVision.ERectangleModeThe modes that specify how the selection of coded elements with a rectangle behaves
 CeVision.EReductionModeThe reduction mode to be used when learning a Consistent Edges model
 CeVision.EReferenceNoiseEnumeration for specifying how a reference image is affected by noise in EasyImage
 CeVision.ERgbStandardAllowed values for the RGB standard in EasyColor
 CeVision.ERoiHitDescribes the ROI that was hit by the mouse cursor
 CeVision.ERotationRightAnglesClockwise Right angles for rotation
 CeVision.ESegmentationMethodThe segmentation methods that are available to the image encoder
 CeVision.ESegmentationModeAllowed values for the segmentation mode in EasyOCR
 CeVision.ESelectionFlagSpecifies to which subset of a selection an operation should be applied in EasyObject and EasyOCV
 CeVision.ESerializerFileWriterModeCreation mode of the file
 CeVision.ESerializerModeThe mode of an eVision.ESerializer object
 CeVision.EShapeBehaviorAllowed values for conditions on the behavior of a shape
 CeVision.EShapeTypeShape type
 CeVision.EShiftingModeAllowed values for the shifting mode of EasyOCR
 CeVision.ESingleThresholdModeThe single threshold mode for the selection of coded elements with respect to a given feature
 CeVision.ESortDirectionThe sorting mode for selections of coded elements based on their features
 CeVision.ESpotPolarityThe possible polarities of an eVision.ESpot
 CeVision.ESpotTypeThe possible types of an eVision.ESpot
 CeVision.EStitchingAlgorithmAlgorithm used by the eVision.EImageStitcher
 CeVision.EStitchingGridStartingCornerDefines which corner of the grid is considered the starting corner for the traversal
 CeVision.EStitchingGridTraversalDefines how images are ordered (mapped) into a 2D grid when stitching in grid mode
 CeVision.ESymbolPolarityAllowed values for the polarity of a code
 CeVision.ESymbologiesThe symbologies supported by EasyBarCode
 CeVision.ETextSizeConstraintModeDifferent modes to resize or modify texts before drawing them
 CeVision.EThinStructureModeAllowed values for the type of thin structures in EasyFind
 CeVision.EThresholdModeThe various modes for thresholding that are supported by eVision
 CeVision.EToneMapperTypeType of tone-mapper algorithm to use
 CeVision.ETopologyFormatTypeFormat types supported for the specification of an eVision.ETopology
 CeVision.ETrainingModeAllowed values for the training mode in EChecker
 CeVision.ETransitionChoiceThe transition selection method applied by the gauge measurement
 CeVision.ETransitionTypeThe type of transition to be retained by the gauge measurement
 CeVision.EVerbosityThe verbosity level of a Memento message
 CeVision.EWedgeGaugeEdgeEdges that can be measured by a eVision.EWedgeGauge
 CeVision.Easy3D.E3DAttributeThis enumeration contains the possible attributes of the eVision.Easy3D.EPointCloud in addition to the eVision.Easy3D.E3DPoint
 CeVision.Easy3D.E3DObjectFeatureThe list of possible extracted features for eVision.Easy3D.E3DObject
 CeVision.Easy3D.E3DPlaneNormalOrientationOrient the normal of the plane such that normal.X/Y/Z is positive/negative
 CeVision.Easy3D.EAlignmentPolarityPolarity of an alignment, used in eVision.Easy3D.EFeaturesAligner
 CeVision.Easy3D.EAlignmentTypeType of alignment to perform by eVision.Easy3D.EFeaturesAligner
 CeVision.Easy3D.EAttributeTypeThis enumeration contains the possible types for the eVision.Easy3D.E3DAttribute
 CeVision.Easy3D.EAxisOriginModeThis enumeration contains the possible values for the parameter of eVision.Easy3D.E3DViewer.AxisOrigin method
 CeVision.Easy3D.EAxisSystemTypeAxis type used in a eVision.Easy3D.EZMap or eVision.Easy3D.EDepthMap
 CeVision.Easy3D.ECalibrationTypeThe Easy3D calibration type
 CeVision.Easy3D.EColorRampModeThis enumeration contains the possible values for the parameter of eVision.Easy3D.E3DViewer.GenerateColors method
 CeVision.Easy3D.EComparisonDistanceModeThis enumeration specifies the distance mode for the 3D comparison
 CeVision.Easy3D.EFillUndefinedPixelsDirectionDirection in which the undefined pixels are filled in a depthmap
 CeVision.Easy3D.EFillUndefinedPixelsMethodMethod to fill the undefined pixels in a depthmap
 CeVision.Easy3D.EMapConversionModeConversion modes to use in eVision.Easy3D.EConverter
 CeVision.Easy3D.EMaximumAnalysisModeThis enumeration contains the possible values for the analysis mode of the eVision.Easy3D.ELaserLineExtractor object
 CeVision.Easy3D.ENoiseRemovalMethodType of filter used in method eVision.Easy3D.EFilters.RemoveNoise
 CeVision.Easy3D.EObjectBasedCalibrationPrecisionVsSpeedTradeOffThe precision vs speed trade-off
 CeVision.Easy3D.EObjectBasedCalibrationTypeThe type of the calibration object
 CeVision.Easy3D.EPhotometricStereoContrastThis enumeration contains the possible ways to handle the contrast when retrieving Albedos, Gaussian curvatures or Mean curvatures
 CeVision.Easy3D.EPlaneCropperTypeType of crop to use in eVision.Easy3D.EPlaneCropper
 CeVision.Easy3D.EPointCloudFilteringMethodType of filtering method to use in eVision.Easy3D.EPointCloudFilter
 CeVision.Easy3D.EPreservationModeEnum defining what quantities related to the X, Y and Z axes are preserved by eVision.Easy3D.EZMapLeveler
 CeVision.Easy3D.EProjectionTypeThis enumeration contains the possible values for the parameter of eVision.Easy3D.E3DViewer.ProjectionType method
 CeVision.Easy3D.ESourceColorModeThis enumeration contains the modes for the display of the point cloud colors
 CeVision.Easy3D.ETextLabelAlignmentThis enumeration contains the alignment of the text labels
 CeVision.Easy3D.EUIAPIThis enumeration contains the various User Interface API supported by eVision.Easy3D.E3DViewer
 CeVision.Easy3D.EViewDirectionThis enumeration contains the axis aligned view directions
 CeVision.Easy3D.EZMapGeneratorResolutionXYModeMode used to specify the resolution of the ZMap generated on the x and y axes
 CeVision.Easy3D.EZMapGeneratorZResolutionFailureHandlerMode used to specify what to do when the Z Resolution set is too small to represent all the data
 CeVision.Easy3D.EZMapImageToWorldKernelRepresents the kernel to use to compute the Z coordinate of the worldPoint in eVision.Easy3D.EZMap.ImageToWorld
 CeVision.Easy3D.EZMapOrientationVectorModeThe eVision.Easy3D.EZMap orientation, it's the direction of the X (width) axis of the ZMap
 CeVision.Easy3D.EZMapReferencePlaneModeThe 3D reference plane used to build the eVision.Easy3D.EZMap
 CeVision.EasyBarCode2.EBarCodeSymbologiesEnum representing the different symbologies of barcodes that can be read by an eVision.EasyBarCode2.EBarCodeReader
 CeVision.EasyBarCode2.EReadingOrientationRepresents the orientation to assume when decoding a barcode without start/stop patterns, for example those of eVision.EasyBarCode2.EBarCodeSymbologies.PharmacodeOneTrack
 CeVision.EasyDeepLearning.EClassifierCapacityThe capacity of the classifier network
 CeVision.EasyDeepLearning.EConfusionMatrixElementThe various elements representing the cases of the 2x2 confusion matrix used in eVision.EasyDeepLearning.EDeepLearningDefectDetectionMetrics
 CeVision.EasyDeepLearning.EDLDataAugmentationTypeThis enum represents how the data augmentation transformation are generated
 CeVision.EasyDeepLearning.EDatasetTypeType of dataset split
 CeVision.EasyDeepLearning.EDeepLearningDeviceTypeDifferent types of Deep Learning device
 CeVision.EasyDeepLearning.EDeepLearningInferencePrecisionPrecisions supported by a Deep Learning device
 CeVision.EasyDeepLearning.EDeepLearningLearningRateTypeThe type of learning rate indicates how the learning rate changes during training
 CeVision.EasyDeepLearning.EDeepLearningToolTypeType of EasyDeepLearning tool
 CeVision.EasyDeepLearning.EDeepOCRModelEasyDeepOCR models that are trainable with eVision.EasyDeepLearning.EDeepOCRTool
 CeVision.EasyDeepLearning.EHeatmapColormapColor maps for visualizing the heatmap
 CeVision.EasyDeepLearning.EImageAnnotationFormatSupported formats of annotation files for image file
 CeVision.EasyDeepLearning.ELocatorCapacityThe capacity of the locator deep learning network
 CeVision.EasyDeepLearning.ELocatorFeatureFeatures supported by the eVision.EasyDeepLearning.ELocator or eVision.EasyDeepLearning.ELocatorObject
 CeVision.EasyDeepLearning.ESupervisedSegmenterCapacityThe capacity of the supervised segmentation network
 CeVision.EasyDeepLearning.EUnsupervisedSegmenterCapacityThe capacity of the unsupervised network
 CeVision.EasyMatrixCode2.ECC000FamilyFamily of error corrections used
 CeVision.EasyMatrixCode2.EReadModeThis enumeration contains the possible operation modes for the eVision.EasyMatrixCode2.EMatrixCodeReader.Read method
 CeVision.EasyOCR2CharSpacingBiasThis enumeration contains the possible biases for the optimized character spacing in the detection phase of eVision.EOCR2
 CeVision.EasyOCR2CharWidthBiasThis enumeration contains the possible biases for the optimized character width in the detection phase of eVision.EOCR2
 CeVision.EasyOCR2CharacterFilterThis enumeration contains the possible filters for loading fonts in eVision.EOCR2
 CeVision.EasyOCR2CharacterType
 CeVision.EasyOCR2DrawDetectionStyleThis enumeration contains the possible drawing styles for the detection results in eVision.EOCR2
 CeVision.EasyOCR2DrawRecognitionStyleThis enumeration contains the possible drawing styles for the recognition results in eVision.EOCR2
 CeVision.EasyOCR2DrawSegmentationStyleThis enumeration contains the possible drawing styles for the segmentation results in eVision.EOCR2
 CeVision.EasyOCR2TextPolarityThis enumeration contains the possible polarities of text searched during segmentation in eVision.EOCR2
 CeVision.Legacy.EFiducialMatchingModeAllowed values for the fiducial finder mode in EChecker
 CeVision.Legacy.EPolygonMeasurementModePolygonGauge measurement mode
 CeVision.LicenseFeatures.FeaturesEVision Features
 CeVision.Easy3D.TextLabelA class representing a text label that can be displayed using eVision.Easy3D.E3DViewer