EasyOcrRead¶
Support |
|
|---|---|
Required licenses |
EasyOCR |
Recommended images |
Any image from the folder |
Location |
|
Purpose¶
This sample program demonstrates how to:
Read a text inside the ROI of an image using EasyOCR (superseded by EasyOCR2).
Use a configuration based on a OCR font file (
.ocr).
Code highlights¶
Load an EasyOCR font file.
// Load the font file EOCR m_Ocr; m_Ocr.Load(ToUtf8(LoadFont.GetPathName()).GetString());
Read the text.
// Set the threshold mode m_Ocr.SetThreshold(EThresholdMode_MinResidue); // Perform recognition #define NB_MAX_RECO_CHARS 256 m_szOCRRecoText = m_Ocr.Recognize(&m_SrcRoi1, NB_MAX_RECO_CHARS, EOCRClass_AllClasses);
Draw the image, the ROI and the characters bounding boxes
// Display the source image Src.Draw(drawAdapter); // Draw the roi frame with its handles Roi.DrawFrame(drawAdapter, TRUE); // Draw the character bounding boxes if needed if (GetDocument()->m_bRead) { const ERGBColor greenPen(0, 255, 0); Ocr.DrawChars(drawAdapter, greenPen); }