Computing and Using Image Statistics

EasyImage provides multiple ways of extracting and computing statistics from an image. These returned statistics can either be:

  • Another image, this is the case for statistics that are expressed through filtering.

  • One or more values, this is the case when computing the maximum or minimum pixel values for example.

Sliding Window

The average and standard deviation of gray-level values can be computed in a sliding window, that is, computed for every position of a rectangular window centered on every pixel. The window size is arbitrary.

Note

The computing time of these functions does not depend on the window size.

Sliding window average.

Sliding window standard deviation.

Histogram Computation and Analysis (and LUT Creation)

A histogram is a statistical summary of an image: it shows the number of occurrences for every gray-level value in an image, and its shape reveals characteristics of the image. For instance, peaks in the histogram curve correspond to dominant colors in the image. If the histogram is bi-modal, a large peak for the dark values corresponding to the background, and smaller peaks in the light values.

Typical image histogram.

Histogram Computation

Histogram Analysis

Histogram Equalization

  • EasyImage::Equalize .NET Python re-maps the gray levels so that the histogram fills in the whole dynamic range as uniformly as possible.

  • This may be useful to maximize image contrast, or to reveal details in dark parts of the image.

Input image and its histogram.

Equalized image and its histogram.

Set Up a Lookup Table

../../../_images/lookup_graph.webp

Equalization lookup table.

Image Focus

EasyImage::Focusing() .NET Python returns a measure of how well-focused an image is, by computing its total gradient energy. Calling it repeatedly on images captured at different focus positions gives you the basis of an auto-focus routine: the position that yields the highest value is the sharpest.

The measure relies on image gradients, which highlight the edges of structures in the image. A well-focused image has sharp edges and therefore strong gradient values; a poorly focused image has soft edges and weaker gradient values.

To compute the total gradient energy, eVision:

  1. Computes the horizontal and vertical gradient images, and squares their pixel values.

  2. Averages the squared pixel values, separately, over each gradient image.

  3. Sums the two averages.

  4. Takes the square root of the result.

Hint

The resulting value is highest when the image is well-focused, and decreases as focus quality drops.

../../../_images/easyimage_focusing_1.webp

A well-focused image, with its (absolute-valued) horizontal and vertical gradients. The gradients show the edges of the structures with strong values. The total gradient energy for this image is 17.9.

../../../_images/easyimage_focusing_2.webp

A badly focused image, with its (absolute-valued) horizontal and vertical gradients. The gradients show the edges of the structures with weak values. The total gradient energy for this image is 7.9.

EasyImage Statistics Functions

The class responsible for computing the statistics depends on the image type:

The next section explains the method using EImageStatisticsBW8 .NET Python to ease the reading. The target image and its optional region have to be set before calling the getters using EImageStatisticsBW8::SetImage() .NET Python.

Binary and Weighted Moments

EImageStatisticsBW8::GetBinaryMoments() .NET Python computes the binary moments of pixels above or equal to EImageStatisticsBW8::SetHighThreshold() .NET Python up to the requested order on the image.

Returns a vector containing the moments in the following order (up to the maxOrder given):

  • returnedArray[0] is the area (0th order moment).

  • returnedArray[1] is the sum of abscissas (1st order, uncentered moment).

  • returnedArray[2] is the sum of ordinates (1st order, uncentered moment).

  • returnedArray[3] is the sum of squared abscissas (2nd order, uncentered moment).

  • returnedArray[4] is the sum of product of abscissas and ordinates (2nd order, uncentered moment).

  • returnedArray[5] is the sum of squared ordinates (2nd order, uncentered moment).

Gravity Center (Average Pixel Coordinates Above/On Threshold)

EImageStatisticsBW8::GetGravityCenterOfPixelsAboveHighThreshold .NET Python computes the coordinates of the gravity center of an image. The gravity center is computed on the pixels whose value are above the set high threshold (set using EImageStatisticsBW8::SetHighThreshold()).

Pixel Count (Between 2 Thresholds)

High and low threshold can be set using EImageStatisticsBW8::SetLowThreshold() .NET Python and EImageStatisticsBW8::SetHighThreshold() .NET Python

Minimum, Maximum and Average Gray-Level Value

Warning

GetPixelMax and GetPixelMin are the only methods that aren’t implemented for EImageC24 .NET Python images. Therefore, they do not exist in EImageStatisticsC24 .NET Python.

Variance and Standard Deviation

Number of Different Pixels by Comparing 2 Images

Supported Types

Method

Supported Types

Sliding Window (LocalAverage, LocalDeviation)

BW8, BW16

Histogram (Histogram)

BW8, BW16, BW32

Histogram Equalization (Equalize)

BW8, BW16

Image Focus (Focusing)

BW8, BW16, C24

Image Statistics (moments, pixel count, min/max/avg, variance/stddev)

BW8, BW16, C24 (note: GetPixelMax/GetPixelMin not available for C24)

Pixel Compare (PixelCompare)

BW8, BW16, C24

See Also

Code Snippets

Easy to understand, ready to copy code snippets.

Statistics
Thresholding

Use computed histograms to select and apply thresholds to an image.

Thresholding