Unwarping an Image¶
Unwarping an image is the application of the calibration model to create a rectified, distortion free image.
To unwarp an image, use the method
ECameraCalibration::Unwarp.NET Python.If the calibration model is fixed, you can speed up the unwarping process by first computing a lookup table with
ECameraCalibration::SetupUnwarp.NET Python.Use
ECameraCalibration::GetUnwarpedCalibration.NET Python to get the calibration of the unwarped image.The calibration of an unwarped image is an affine transformation.
It has the modes
ECalibrationMode_Scaled.NET Python,ECalibrationMode_Anisotropic.NET Python,ECalibrationMode_Inverse.NET Python andECalibrationMode_Skewed.NET Python.