Overlay

EasyImage::Overlay .NET Python overlays an image on the top of a color image, at a given position.

  • If a color overlay image is used, all its pixels are copied to the destination image, except those that equal the reference color, allowing multicolored overlays.

  • If a grayscale overlay image is used, all the overlay image pixels are copied to the destination image, except those that equal the reference color, which are replaced by the background image pixels.

See Also

Code Snippets

Easy to understand, ready to copy code snippets.

Overlay