EasyDeepOCR Principles and Workflow

Scope

EasyDeepOCR is able to locate and read all texts in a given image, provided they adhere to the following specifications:

  • Printable ASCII characters: !"#$%&\'()*+,-./0123456789:;<=>?@ABCDEFGHIJKLMNOPQRSTUVWXYZ[\]^_`abcdefghijklmnopqrstuvwxyz{|}~

  • Industrial fonts

  • Minimum line height: 12 pixels

  • Line aspect ratio between 1:1 and 40:1

  • Maximum characters per line: 50

  • Gray scale (8-bit) or color (24-bit) images

  • Near planar images (limited perspective)

Structured Texts

When you specify a topology, the lines are gathered into texts that satisfy the following requirements:

  • The texts match the topology.

  • The texts are structured.

EasyDeepOCR only returns ‘structured texts’ (a concept specific to this tool: see eVision::EasyDeepOCR::ETextLine .NET Python) where the geometric arrangement of lines and words meets a particular definition:

  1. All the lines of a ‘structured text’:

    • Must be parallel.

    • Must have the same height.

    • Must be horizontally aligned:
      Two lines l₀ and l₁ are horizontally aligned if:

    \[l_0^{\text{begin}} \le l_1^{\text{begin}} \quad \text{and} \quad l_1^{\text{end}} \le l_0^{\text{end}}\]
  2. All the pairs of consecutive lines:

    • Must not overlap vertically.

    • Must not be separated by a vertical distance greater than the line height.

  3. All the words of a line:

  • Must not be separated by a horizontal distance greater than the line height.

Parallelism

Line height

Horizontal alignment

Vertical alignment

Word spacing

Optimization for Custom Use Cases

EasyDeepOCR also offers the possibility to optimize the reader for a custom use case.

  • When doing so, an additional constraint is added to the list:

    • The texts must belong to the same custom use case as the one used for the optimization.

    • This optimization offers two potential benefits:

      • Increasing the processing speed.

      • Improving the detection of challenging texts.

  • In the context of EasyDeepOCR, a custom use case is defined as follows:

    • It is a batch of images captured in the same conditions that depict a different instance of the same object.

    • For every image, you must designate a ‘text of interest’.

    • This ‘text of interest’ is the text that the ETextReader should retrieve.

    • From one image to another, all the ‘texts of interest’ must share some geometrical properties.
      Specifically, they must have:

      • The same line height (in pixels).

      • The same font.

      • The same appearance (such as printed, embossed, dotted).

    Note

    There can be several ‘texts of interest’ in a given image, but all texts must share the above-mentioned geometrical properties.

Basic Workflow

The full-featured EasyDeepOCR workflow consists of the following steps:

  1. Instantiate an ETextReader .NET Python

  2. (Optional) Set the EDeepLearningExecutionSettings .NET Python

  3. Initialize

  4. (Optional) Set the ETopology .NET Python

  5. (Optional) Optimize

  6. Read

  7. Extract the EasyDeepOCR::EText .NET Python results

This complete workflow is broken down and explained in the following sections:

Inputs

The reading method of an ETextReader, namely ETextReader::Read(), accepts 2 input arguments:

  • An ROI (EROIBW8 or EROIC24): the image to be searched for texts.

  • An ERegion (optionally) that defines a geometrical filter: any text whose 4 corners are not included in the region is filtered out.

Outputs

The method ETextReader::Read() returns a vector of EText that contains the following information:

  • An ERectangle representing the text position in the image

  • A text string

  • A vector of ETextLine

This vector of ETextLine represents the lines of the text and contains 2 pieces of information:

  • An ERectangle representing the line position in the image

  • A line string