Creating a Dataset and Training a Supervised Segmenter¶
This code snippet shows how to create a dataset, train a supervised segmenter and get the best performance metrics obtained during the training.
C++¶
#include <eVision/EasyDeepLearning/EasySegment/ESupervisedSegmenter.h>
using namespace eVision;
using namespace eVision::EasyDeepLearning;
// Creating dataset and segmenter objects
EDataset dataset;
EDataset trainingDataset;
EDataset validationDataset;
ESupervisedSegmenter segmenter;
// Example with adding a single image with a mask
// Add a segmentation label
int label_idx = dataset.AddSegmentationLabel("scratch");
// In this case, the mask must contain pixel who are either 0 or equal to `label_idx`
// If your image is a binary image, you can set all non-null pixel to `label_idx`
EImageBW16 mask;
mask.Load("mask.png");
// Image to segment
EImageBW8 image;
image.Load("image.png");
// Adding image and linking it to the loaded mask
int image_idx = dataset.AddImage(image);
dataset.SetSegmentationMap(image_idx, mask);
// Create data augmentation
EDataAugmentation augmentation;
// Rotation of up to 90
augmentation.SetMaxRotationAngle(90);
// Enabling horizontal flips
augmentation.SetEnableHorizontalFlip(true);
// Splitting the dataset with 80% of images for the training dataset
// and 20% for the validation dataset
dataset.SplitDataset(trainingDataset, validationDataset, 0.8f);
// Training the segmenter for 50 epochs
segmenter.Train(trainingDataset, validationDataset, augmentation, 50);
segmenter.WaitForTrainingCompletion();
// Get the best metrics obtained on the validation dataset
ESupervisedSegmenterMetrics bestMetrics = segmenter.GetValidationMetrics(segmenter.GetBestIteration());
C#¶
using eVision;
using eVision.EasyDeepLearning;
// Creating dataset and segmenter objects
EDataset dataset = new EDataset();
EDataset trainingDataset = new EDataset();
EDataset validationDataset = new EDataset();
ESupervisedSegmenter segmenter = new ESupervisedSegmenter();
// Example with adding a single image with a mask
// Add a segmentation label
int label_idx = dataset.AddSegmentationLabel("scratch");
// In this case, the mask must contain pixel who are either 0 or equal to `label_idx`
// If your image is a binary image, you can set all non-null pixel to `label_idx`
EImageBW16 mask = new EImageBW16();
mask.Load("mask.png");
// Image to segment
EImageBW8 image = new EImageBW8();
image.Load("image.png");
// Adding image and linking it to the loaded mask
int image_idx = dataset.AddImage(image);
dataset.SetSegmentationMap(image_idx, mask);
// Create data augmentation
EDataAugmentation augmentation = new EDataAugmentation();
// Rotation of up to 90°
augmentation.MaxRotationAngle = 90.0F;
// Enabling horizontal flips
augmentation.EnableHorizontalFlip = true;
// Splitting the dataset with 80% of images for the training dataset
// and 20% for the validation dataset
dataset.SplitDataset(trainingDataset, validationDataset, 0.8F);
// Training the segmenter for 50 epochs
segmenter.Train(trainingDataset, validationDataset, augmentation, 50);
segmenter.WaitForTrainingCompletion();
// Get the best metrics obtained on the validation dataset
ESupervisedSegmenterMetrics bestMetrics = segmenter.GetValidationMetrics(segmenter.BestIteration);
Python¶
import eVision
from eVision import EasyDeepLearning as edl
# Creating dataset and segmenter objects
dataset = edl.EDataset()
training_dataset = edl.EDataset()
validation_dataset = edl.EDataset()
segmenter = edl.ESupervisedSegmenter()
# Example with adding a single image with a mask
# Add a segmentation label
label_idx = dataset.AddSegmentationLabel("scratch")
# In this case, the mask must contain pixel who are either 0 or equal to `label_idx`
# If your image is a binary image, you can set all non-null pixel to `label_idx`
mask = eVision.EImageBW16()
mask.Load("mask.png")
# Image to segment
image = eVision.EImageBW8()
image.Load("image.png")
# Adding image and linking it to the loaded mask
image_idx = dataset.AddImage(image)
dataset.SetSegmentationMap(image_idx, mask)
# Create data augmentation
augmentation = edl.EDataAugmentation()
# Rotation of up to 90°
augmentation.MaxRotationAngle = 90.0
# Enabling horizontal flips
augmentation.EnableHorizontalFlip = True
# Splitting the dataset with 80% of images for the training dataset
# and 20% for the validation dataset
dataset.SplitDataset(training_dataset, validation_dataset, 0.8)
# Training the segmenter for 50 epochs
segmenter.Train(training_dataset, validation_dataset, augmentation, 50)
segmenter.WaitForTrainingCompletion()
# Get the best metrics obtained on the validation dataset
best_metrics = segmenter.GetValidationMetrics(segmenter.BestIteration)