EasySegment - Detecting and Segmenting Defects¶
EasySegment is the deep learning segmentation library of eVision.
It contains 2 different modes:
The unsupervised mode:
The tool is trained only with good images (
EUnsupervisedSegmenter.NET Python class).This mode does not require a ground truth segmentation and the creation of the dataset is thus much quicker than for the supervised mode.
This mode can detect unexpected defects while the supervised mode is only capable of detecting defects similar to those in the dataset.
The supervised mode:
The tool is trained using the ground truth segmentation defined for the images (
ESupervisedSegmenter.NET Python class).This mode can detect and segment more types of defects with better accuracy than the unsupervised mode. It directly builds a model for the defects while the unsupervised mode builds a model of the good images and tries to detect variations from this model.
You can also use this mode to segment other types of objects than defects.