Text and Code Reading¶ Sample The sample program demonstrates: Image C++ C# Qt CMake Vb Python EasyCodeReading Read a bar code, a data matrix and a QR code in an image with a single read call. ✓ ✓ ✓ EasyBarCodeRead Read a 1D bar code in an image. ✓ ✓ ✓ ✓ ✓ EasyBarCodeReadMail Read a mail bar code in an image. ✓ ✓ EasyMatrixCodeRead Read a data matrix code in an image. ✓ ✓ ✓ ✓ EasyQRCodeRead Read a QR code in an image. ✓ ✓ ✓ ✓ ✓ EasyOcrRead Read a text inside the ROI of an image using EasyOCR (superseded by EasyOCR2). Use a configuration based on a OCR font file (.ocr). ✓ EasyOcr2Read Read a text inside the ROI of an image. ✓ ✓ ✓ ✓ ✓ EasyDeepOCRRead Read all the texts in an image with a single read call. Load a model. ✓ ✓ ✓ EasyDeepOCRReadConsole Read all the texts in an image with a single read call. Load a model. Set a topology. ✓ ✓