Using EasyColor

Color Definition and Supported Systems

What is Color?

  • The human eye is sensitive to light:

    • Intensity, or achromatic sensation, captured by grayscale images.

    • Wavelength, or chromatic sensation, described in red, green, and blue primary colors.

../../../_images/color_gamut.svg

Visible color gamut in the XYZ color space

  • There are three color systems:

    • Mixture systems (RGB / XYZ) give the proportions of the three primaries to be combined.

    • YUV Luma/chroma systems (YUV / L*a*b* / L*u*v* / YCbCr) separate the achromatic (Y) and chromatic sensations (U & V). Used when a black and white image is required as well (television).

    • Intensity/saturation/hue systems (ISH / LSH / VSH / LCH / YSH) separate achromatic (black and white Intensity) from enhanced chromatic (color Saturation and Hue) sensations. Used to eliminate lighting effects, or to convert RGB images to another color system. More saturated colors are more vivid, less saturated ones are grayer.

  • In general:

    • RGB is used by monitors, cameras and other display devices.

    • YUV / YCbCr is used for efficient transmission of color images by compressing the chrominance information.

    • XYZ is used for device-independent color representation.

  • All image processing operations can use quantized coordinates: discrete values in the [0..255] interval, which use a byte representation to store images in a frame buffer.

  • Color system conversion operations can also use simpler unquantized coordinates: continuous values, often normalized to the [0..1] interval.

Color Image Processing

  • A color image is a vector field with three components per pixel. All three RGB components reflected by an object have amplitude proportional to the intensity of the light source. By considering the ratio of two color components, one obtains an illumination-independent image. With a clever combination of three pieces of information per pixel, one can extract better features.

  • There are 3 ways to process a color image:

    • Component extraction: you can extract the most relevant feature from the triple color information, to reduce the amount of data. For instance, objects may be distinguished by their hue, a pre-processing step could transform the image to a gray-level image containing only hue values.

    • De-coupled transformation: you can perform operations separately on each color component. For instance, adding two images together adds the red, green and blue components and stores the result, component by component, in a resulting color image.

    • Coupled transformation: you can combine all three color components to produce three derived components. For example, converting YIQ to RGB.

Supported Color Systems

  • EasyColor supports color systems RGB, XYZ, L*a*b*, L*u*v*, YUV, YCbCr, YIQ, LCH, ISH / LSH, VSH and YSH.

  • RGB is the preferred internal representation as it is compatible with 24-bit Windows Bitmaps.

RGB-based

XYZ-based

YUV-based

Mixture

RGB

XYZ

Luma/Chroma

L*a*b*
L*u*v*

YUV
YCbCr
YIQ

Intensity/Saturation/Hue

ISH
LSH
VSH

LCH

YSH

Transform Using LUTs (Lookup Tables)

Index Bits

Number of entries

Table size (bytes)

4

\(2^{(3 \times 4)} = 4,096\)

14,739

5

\(2^{(3 \times 5)} = 32,768\)

107,811

6

\(2^{(3 \times 6)} = 262,144\)

823,875

Discrete Quantized vs. Continuous Unquantized

Color coordinates in the classical systems are normally continuous values, often normalized to the [0..1] interval. Computations on such values, termed unquantized, are simpler.

However, storage of images in a frame buffer imposes a byte representation, corresponding to discrete values, in the [0..255] interval. Such values are termed quantized.

All image processing operations apply to quantized values, but conversion operations can also be specified using unquantized coordinates.

Transform YUV444 / YUV422

  • YUV images can be minimized without degrading visual quality using function EasyColor::Format444To422 .NET Python to convert from 4:4:4 to 4:2:2 format (or you can convert Format 422 to 444 (EasyColor::Format422To444 .NET Python)).

    • 4:4:4 uses 3 bytes of information per pixel.

    • 4:2:2 uses 2 bytes of information per pixel. It stores the even pixels of U and V chroma with the even and odd pixels of Y luma as follows:

\( Y_{[\text{even}]} U_{[\text{even}]} Y_{[\text{odd}]} V_{[\text{even}]} \)

Merge, Extract, and Color

  • A color image contains three color planes of continuous tone images.

  • A gray-level image can be a component of a color system.

Merge and Extract Components

Note

EasyColor functions perform the necessary interleaving / un-interleaving operations to support Windows bitmap format of interleaved color planes (blue, green and red pixels follow each other).

Pseudo-Color to Transform Gray-Level Images to Color

  • The trick is to define a regular gamut of 256 colors and each color will be assigned to pixels with a corresponding gray-level value.

  • To define pseudo-color shades, you specify a trajectory in the color space of an arbitrary system. You can then pseudo-color using the drawing functions color palette (see Image and Vector Drawing) then save and/or transform it like any other color image.

Gray-level and pseudo-colored image.

Separate Color Objects

  • This EasyColor process takes a set of distinct colors and associates each pixel with the closest color, using a layer index that can then be used in EasyObject with the labeled image segmenter to improve blob creation.

ColorSegmentationNone
ColorSegmentationThree

Raw image and segmented image (3 colors).

RGB and BGR Conversion

EasyColor allows you to convert an image brom RGB to BGR. This can be applied to EImageC24 .NET Python and EImageC24A .NET Python.

Please note that eVision uses BGR (A) images internally. Therefore, a color image loaded using EImageC24::Load .NET Python is in the BGR format. When getting a EC24 .NET Python pixel from an image: