EasyMatrixCode1 - Reading Matrix Codes (deprecated)¶
Warning
This library is deprecated, use EasyMatrixCode2 instead.
Why use EasyMatrixCode2 instead¶
Compared to EasyMatrixCode1, EasyMatrixCode2 offers the following benefits:
Ability to read multiple data matrix codes in an image.
Support for asynchronous processing.
Improved consistency of reading and grading results.
Improved consistency of processing time.
Improved handling of deformed data matrix codes.
Note
EasyMatrixCode2 does not support the ANSI/AIM BC11 grading standard that was supported in EasyMatrixCode1 as this standard is superseded by ISO 15415 that is supported by EasyMatrixCode2.
Usage¶
You can read the matrix code in an image by using the EMatrixCodeReader::Read .NET Python method.
This method returns an EMatrixCode .NET Python instance that contains the following information about the found data matrix code:
Contents¶
Specification of the data matrix
Symbols supported by EasyMatrixCode
Workflow of EasyMatrixCode
How to learn a Matrix Code model
How to compute the print quality of a Matrix Code.
How to reading and interpret GS1 Data Matrix Codes.
Quick Links¶
List of all Classes, Structs and Enumerations of the EasyMatrixCode library.
Code snippets for the EasyMatrixCode library.