Computing the Print Quality

Warning

This library is deprecated, use EasyMatrixCode2 instead.

To compute the print quality indicators as defined by BC11, ISO 15415, ISO/IEC TR 29158 (formerly known as AIM DPM-1-2006) and SEMI T10-0701 standards, retrieve the grades with the EMatrixCode::GetIso15415GradingParameters .NET Python, EMatrixCode::GetIso29158GradingParameters .NET Python and EMatrixCode::GetSemiT10GradingParameters .NET Python accessors of the EMatrixCode .NET Python class.

Note

The print quality of the matrix codes is computed during the EMatrixCodeReader::Read .NET Python operation, only if EMatrixCodeReader::SetComputeGrading .NET Python parameter was set to true.

Note

Our implementation of ISO 29158, a complement to ISO 15415, includes only those parameters that are unique or redefined in ISO 29158. For parameters common to both standards, please refer to the corresponding ISO 15415 struct fields.

See also

For more information concerning code grading, see Code Grading.