Using EasySpotDetector

Operating Principle

Warning

Please note that EasySpotDetector is deprecated and will be removed in release 27.6.

Introduction

EasySpotDetector uses local segmentation to extract salient objects from the background, then a deep learning classifier can sort them. It is applicable to many materials like films, coated surfaces, steel, battery foils, glass…

Specific parameters allow you to select the aspect and the size of the defect, as well as the sensitivity of the detection. The segmentation is robust to noise and doesn’t require context training or calibration.

The main features are:

  • Detection of faint defects and contamination, even in noisy images

  • Fast processing for in-line inspection

  • Compatible with acquisition from line-scan and 2D cameras

  • Optional pre-alignment of the region of interest on the part edges

  • Optional deep learning classification of the defects

  • Simple and comprehensive C++, C# and Python API

  • Full featured tool, with samples

General Principle

  1. EasySpotDetector performs a simple alignment of the Region of Interest (ROI) from an 8-bit gray scale image. This stage is optional.

  2. The spots are extracted inside the ROI. Two types of spots are supported:

    • “Particle” for compact objects

    Examples of “particles”

    • “Scratch” for elongated objects

    Examples of “scratches”

  3. Optionally, you can invoke a deep learning classifier for each detected spot at production time.

    • This classifier produces a label and a probability for each spot.

    • Using Deep Learning Studio, you can train your own classifier, dedicated to your specific use case.

  4. At development time, EasySpotDetector offers an API to easily populate a classification dataset with the detected spots.

    • You can open this dataset file in Deep Learning Studio for spot annotation and training.

    • EasySpotDetector uses the resulting model at production time to classify the detections.

Workflow

../../../_images/workflow.webp

Workflow diagram

The Alignment

The alignment feature in EasySpotDetector is an optional step, before the detection of the spots. It aims to locate the part to process inside the image.

Hint

To restrict the processing domain in a more flexible and generic way, use the parameter Region of the ESpotDetector::Detect .NET Python method.

  • The alignment works by fitting an axis aligned rectangle to the object edges.

    • The nominal rectangle is defined by a center (X, Y) and a size (width and height).

    • A tolerance (in pixels) sets the search area inside and outside the nominal rectangle.

../../../_images/alignment_11.webp

Explanation of the different terms related to the alignment.

../../../_images/alignment_21.webp

Explanation of the different terms related to the guard bands.

Detecting Particles and Scratches

EasySpotDetector detects particles and scratches by comparing the average local surroundings with the value of the center pixel. It performs this operation at various scales to segment large and small objects.

Note

The definition of the surroundings is different for particles detection and for scratches detection.

  • To operate the detection, use the method ESpotDetector::Detect .NET Python with a gray scale image or an EROIBW8 as parameter. You can also use an optional ERegion to restrict the domain.

  • The result is returned by ESpotDetector::GetSpots .NET Python as a vector of ESpot .NET Python.

  • An ESpot .NET Python stores all the data about a detected object: type (particle or scratch), polarity (black or white), position and size, area (in pixels), strength (representing the contrast between the object and its surroundings), the pixel region…

Particle Detection

Examples of “particles”

../../../_images/detecting_particle.webp

eVision Studio settings for the EasySpotDetector tool related to particle detection.

Scratch Detection

Examples of “scratches”

A scratch is an elongated object, with length largely greater than the width.

../../../_images/detecting_scratch.webp

eVision Studio settings for the EasySpotDetector tool related to scratch detection.

Using a Deep Learning Classifier

After the detection of spots, you can submit them to a custom deep learning classifier.

  • You must train this classifier specifically for the inspection task (inspection of battery foil or fabric will have different classifiers). The purpose of this process is to get a class that represents/qualifies the object, for example:

    • To confirm or discard the detection.

    • To evaluate the severity of the defect.

    • To classify objects based on their aspect.

  1. In the class ESpotDetector .NET Python, use the method ESpotDetector::SetDLClassifierPath .NET Python to configure a deep learning classifier.

    In EasySpotDetector, the typical workflow with a deep learning classifier is:

    1. Gather samples of detected objects in a deep learning project.

    2. Open the deep learning project in Deep Learning Studio to annotate the samples and train a new classifier.

    3. Use the trained classifier at production time in EasySpotDetector.

../../../_images/using_classifier_workflow.webp

Workflow on training a specific deep learning classifier to work with EasySpotDetector.

  1. After calling the method ESpotDetector::Detect .NET Python, use the method ESpotDetector::AddDetectedSpotsToDLProject .NET Python to fill a EDeepLearningProject .NET Python with the newly detected spots:

    • The image used by ESpotDetector::Detect .NET Python is copied to the subdirectory Images and linked in the project.

      Note

      • Automatic image names are generated unless you set the parameter imageName.

      • All images must have a different name.

    • All the detected spots are added to the project as ROIs of the image, with a label depending on the spot type (particle or scratch).

    • Use the optional parameter roiExtension to increase the ROI size by a pixel amount. It could help the deep learning inference to have a ‘context’ around the ROI.

    • Use the optional parameter noDefectSamples to set the number of extra ROIs added to the project and representing areas without defect. The label of these areas is given by the parameter noDefectLabel.

  2. After adding enough spots to the deep learning project (depending on the context, between 20 and 200 samples per class are recommended), you can open the project with Deep Learning Studio.

    Note

    To annotate and train a deep learning classifier, see:
    Deep Learning Tools - Inspecting Images with Deep Learning > Workflow.

  3. At production time, set the trained classifier tool with the method ESpotDetector::SetDLClassifierPath .NET Python.

See also