Using the Online Command Line

  • When you order a Neo License, Allied Vision sends you a Ticket ID required to activate the license on your system.

    • A Ticket ID is made of 5 groups of 5 alphanumeric characters separated by a dash. For example: TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ

    • You can activate your license either directly on the computer, as a software license, or on a Neo USB Dongle, that you can buy from Allied Vision.

  • In the case of the software container, the license is strongly linked to a single computer system, while with a dongle you can move it easily from computer to computer.

Select a container

  1. To select a license container, use the list-containers command of the Neo License Manager. All the containers compatible with Neo Licenses are listed:

    > NeoLicenseManagerCL.exe list-containers
    
    Container list:
      130-3613949292 (software)
    
    • A software container appears in the list with a serial number starting with 130-.

    • A dongle appears in the list with a serial number starting with 3-. This serial number is also written on the dongle itself.

  2. To create a software container, use the create-software-container command of the Neo License Manager.

    > NeoLicenseManagerCL.exe create-software-container
    
    Software container 130-3245488904 has been created.
    

    If you already have a software container on your system:

    • We highly recommend you to use that one.

    • Create a new software container only if the old one is broken for any reason. The old license container will become unavailable for activation purposes.

  3. Copy the serial number of the container you want to use for the next step.

Activate the license

  1. To activate the license, use the activate command of the Neo License Manager with the serial number of the container.

    > NeoLicenseManagerCL.exe activate -t TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ -s 130-3245488904
    
    Activation of ticket TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ has been done successfully.
    

    The command associates the Ticket ID to the container and activates the license.

Check the Neo License presence

  • To check the presence of the license, use the list-licenses command of the Neo License Manager.

    The new license appears under the serial number of the license container.

    > NeoLicenseManagerCL.exe list-licenses
    
    Licenses on container 130-3613949292 (software):
         Open eVision EasyOCR
    

Activating the OEM key feature

By default, the dongles come with the OEM key feature activated. Nevertheless, older dongles may have to be activated.

  • To check if this feature is activated use the check-dongle-OEM-key-readiness command:

    > NeoLicenseManagerCL.exe check-dongle-OEM-key-readiness –s 3-3613949292
    
  • If the feature is not activated on the dongle, use the prepare-dongle-for-OEM-key command to activate it:

    > NeoLicenseManagerCL.exe prepare-dongle-for-OEM-key –s 3-3613949292
    

Forcing more than one copy of the same license

  • By default, the license manager protects you against multiple activations of the same license in a container, refusing the subsequent activations:

  • If you want to bypass that protection, use the --force argument:

    > NeoLicenseManagerCL.exe activate --force -t TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ -s 130-3245488904
    

Troubleshooting

Command line help

  • To get help about the syntax and the usage of the command line, use the --help argument:

    > NeoLicenseManagerCL.exe --help
    
    Neo License Manager 2
    Usage: C:\Program Files\Euresys\NeoLicenseManager\NeoLicenseManagerCL.exe [OPTIONS] SUBCOMMAND
    
    Options:
    --console-log               Activates console log
    --file-log TEXT             Activates file log; a path to the desired log file must be specified as argument
    -h,--help
    
    Subcommands:
    list-containers
    Returns the list of containers
    Options:
        --filter TEXT:{dongle,software}
                                    Type of containers to be checked (dongle/software)
        -e,--expert                 Enables expert mode
    
    list-licenses
    Returns the list of licenses
    Options:
        -s,--serial-number TEXT     Serial number of a specific container to be checked
        -l,--list-empty-containers  List containers even if they contain no license
        -e,--expert                 Enables expert mode
    
    apply-license-file
    Applies the given activation file to the software container of your computer
    Options:
        -p,--path TEXT REQUIRED     Path of the license activation file
    
    create-software-container
    Creates a new software container on the computer. It will only work if none were present
    Options:
        -f,--force                  Additional argument to enforce container creation. For expert users only
    
    delete-software-container
    Deletes a software container on the computer, given its serial number
    Options:
        -s,--serial-number TEXT REQUIRED
                                    Serial number of the software container to be deleted
    
    get-container-fingerprint
    Saves the fingerprint file of the given container at the specified location
    Options:
        -s,--serial-number TEXT REQUIRED
                                    Serial number of the software container we want to retrieve the fingerprint from
        -p,--path TEXT REQUIRED     File path for the creation of fingerprint
    
    check-dongle-OEM-key-readiness
    Checks if the OEM key feature is available in the given container
    Options:
        -s,--serial-number TEXT REQUIRED
                                    Serial number of the dongle on which we want to check OEM key readiness
    
    prepare-dongle-for-OEM-key
    Prepares a given dongle for OEM key
    Options:
        -s,--serial-number TEXT REQUIRED
                                    Serial number of the dongle we want to prepare for OEM key
    
    check-neo-status
    Performs a global check-up of the Neo licensing system and print it
    Options:
        -p,--path TEXT              File path for the creation of report
    
    activity-log
    Prints the content of the log file
    
    activate
    Activates a Neo ticket ID on the given container
    Options:
        -t,--ticket TEXT REQUIRED   Id of the Neo ticket to be activated
        -s,--serial-number TEXT REQUIRED
                                    Serial number of the container on which ticket will be activated
        -f,--force                  Additional argument to enforce activation. For expert users only
    
    reactivate
    Reactivates a Neo ticket ID on the given container
    Options:
        -t,--ticket TEXT REQUIRED   Id of the Neo ticket to be reactivated
        -s,--serial-number TEXT REQUIRED
                                    Serial number of the container on which ticket will be reactivated
        -f,--force                  Additional argument to enforce reactivation. For expert users only
    
    request-activation-file
    Generates an activation file using the given Neo ticket ID and container fingerprint file. This file can then be used to proceed to an offline activation.
    Options:
        -f,--fingerprint-path TEXT REQUIRED
                                    Path to the fingerprint of a container
        -p,--output-path TEXT REQUIRED
                                    Path for the generated activation file
        -t,--ticket TEXT REQUIRED   Neo ticket Id
    
    request-reactivation-file
    Generates a reactivation file using the given Neo ticket ID and container fingerprint file. This file can then be used to proceed to an offline reactivation.
    Options:
        -f,--fingerprint-path TEXT REQUIRED
                                    Path to the fingerprint of a container
        -p,--output-path TEXT REQUIRED
                                    Path for the generated reactivation file
        -t,--ticket TEXT REQUIRED   Neo ticket Id
    
    apply-emergency-license
    Activates one of the three emergency licenses packages. It has a 8 days duration.
    
    version
    Prints the version of Neo License Manager
    
    
    End message of Neo License Manager CL
    

Emergency licenses

If you need a license for a limited time (for instance while waiting for some support), use an emergency license.

  1. To activate an emergency license , use the apply-emergency-license command:

    • These licenses activate all eVision products.

    • They are valid for 8 days.

    • You can repeat this a maximum of 3 times.

    • For security reasons, you cannot activate emergency licenses on virtual machines.

    > NeoLicenseManagerCL.exe apply-emergency-license
    

License recovery with a software container

If you have to reinstall the system and lost your licenses:

  1. Create a software container.

  2. Activate the license with the old Ticket ID to try to recover all the licenses associated to the container where you first activated this Ticket ID.

    This only works if:

    • It is done in a new, empty container.

    • The system is recognizable (the hardware is more or less the same).

  3. If this does not work, perform a reactivation.

Reactivation

If the recovery does not work or if you lost your licenses and the system has changed significantly (for instance after the failure and replacement of a hardware component), you need to perform a reactivation.

  • This transfers your lost license on a container on the new system.

  • By default, the reactivation is disabled.

  1. Contact the support to obtain a reactivation authorization for the corresponding Ticket ID.

  2. Once the reactivation is authorized, follow the license activation procedure described above but use the reactivate command instead of activate.

Error reporting

If anything fails, the Neo License Manager returns an error and information about it in stderr.

  1. To recover the stderr log from the command line, you can use -–file-log argument, followed by the path to a log file, as follows:

    NeoLicenseManagerCL.exe --file-log c:\tmp\error.log activate -t TT5YY-HYAGN-Q2PBU-U7K7J-DKJJQ -s 130-3245488904
    
  2. If you need more information, use the Memento tool from Euresys.

  3. To check the status of the licensing system on your computer at any time, use the check-neo-status command of the Neo License Manager.

    > NeoLicenseManagerCL.exe check-neo-status
    
    ** Starting List Product Item for box 130-3613949292 and firm code 6001261 **
    Found Productcode (Dependency: 0x7): 4305
        Text (#=20, Dependency 0x00):  "Open eVision EasyOCR"
        Extended Protected Data (#=16, Type 136, Dependency 0x07): 6c 63 64 63 00 01
    9b 05 00 00 00 00 00 00 01 00
    ** List Product Item finished without errors **
    
  4. To check the log of the licensing system on your computer at any time, use the activity-log command of the Neo License Manager.

    > NeoLicenseManagerCL.exe activity-log
    ** L.M version 23.08.0 09/07/23 14:25:02 : Emergency activation was requested.
    L.M version 23.08.0 09/07/23 14:25:03 : Emergency activation was successful. There is (are) 2 emergency license(s) remaining. **