Image Stitching¶
This code snippet shows how to stitch multiple images.
C++¶
#include <eVision/EasyImage/EImageStitcher.h>
using namespace eVision;
// Create the stitcher class
EImageStitcher stitcher;
// EImageC24 can be used instead of EImageBW8
// Patchs is a vector of image where each image is calibrated
std::vector<EImageBW8> patchs;
EImageBW8 output;
stitcher.Stitch(patchs, output);
C#¶
using eVision;
using System.Collections.Generic;
// Create the stitcher class
EImageStitcher stitcher = new EImageStitcher();
// EImageC24 can be used instead of EImageBW8
// Patchs is a vector of image where each image is calibrated
List<EImageBW8> patchs = new List<EImageBW8>();
EImageBW8 output = new EImageBW8();
stitcher.Stitch(patchs.ToArray(), output);
Python¶
import eVision
# Create the stitcher class
stitcher = eVision.EImageStitcher()
# EImageC24 can be used instead of EImageBW8
# Patchs is a vector of image where each image is calibrated
patchs = []
output = eVision.EImageBW8()
stitcher.Stitch(patchs, output)