ConsoleBasic

Support

Required licenses

Any, EasyImage for the processing part

Recommended images

Any

Location

Image Processing/Basic

Purpose

This sample program demonstrates:

  • Initialize and release the library.

  • Check for a specific license.

  • Load an image and perform a simple processing on it.

Code highlights

  1. Initializes the eVision library. This should be done before any other call to eVision.

    Easy::Initialize();
    
  2. Release the library or tool.

    Attention

    You must do this after all the other calls to eVision.

    Easy::Terminate();
    
  3. Check the presence of a license on the system.

    Easy::CheckLicense(...);
    
  4. Load an image file from the disk into an object EImage.

    img.Load(...);